Other Parts Discussed in Thread: UNIFLASH,
I have updated the firmware as per the instruction here: <e2e.ti.com/.../1612764>
Still The SmartRF Flash Programmer 2 is unable to identify the CC3200STK Sensor tag connected to the debug dev kit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have updated the firmware as per the instruction here: <e2e.ti.com/.../1612764>
Still The SmartRF Flash Programmer 2 is unable to identify the CC3200STK Sensor tag connected to the debug dev kit.
Hi Jan,
-I have updated the firmware as mentioned in this post <e2e.ti.com/.../1612764>
-I guess the above mentioned method is for upgrading the firmware on the dev kit and not the sensor tag
- Is there a way I can flash/program/read data from CC3200 STK SensorTag through SimpleLink SensorTag Debugger DevPack?
Hi,
CC3200STK use CC3200 chip inside. Any procedures for another types of SensorTag are not relevant for CC3200 SensorTag. This completely different hardware. You can't use firmware from another SensorTags into CC3200STK.
I don't know how looks SensorTag Debugger DevPack. But definitely is not possible upload firmware into CC3200 using JTAG. It is not important if CC3200 is embedded in SensorTag or any other hardware. But it looks that SensorTag Debugger DevPack also contains serial port interface and lines for control SOP0 and SOP2. From this reason I suppose that using SensorTag Debugger DevPack can be possible upload firmware using Uniflash software into CC3200STK.
My suggestion is use CC3200 LaunchPad or wait for official release CC3200STK.
Jan