Other Parts Discussed in Thread: WL1837
Dear TI support Team,
we are working with WL1837MOD module and we will need to put it in Bluetooth Test Mode in order to perform BT RF PHY Tests.
How can we set the module in Test Mode?
Will we need to flash the chip with a TI test software?
We have tried with the following commands
HCI_Enable_Device_Under_Test_Mode
HCI_Set_Event_Filter 0x02, 0x00, 0x03
HCI_Write_Scan_Enable 0x03
but the chip doesn't connect correctly to the Rohde-Schwarz instrument CBT. It seems that it remains in normal-BT mode.
Thank you for your support,
Maurizio
- Host platform (Sitara EVM, BeagleBone, etc.)
- If TI Sitara, which SDK version is being used?
- Operating system (Linux, Android, etc.)
- WiLink™ flavor (WL1837MOD, etc.)
- Module vendor, if any (TI, Jorjin, Murata, etc.)
- WiLink™ firmware version (click here for more information)
- WiLink software driver version (R8.5/6/7)
- Any applicable logs including Wireshark sniffer logs, WLAN firmware (gLogger), BT firmware (logger), kernel logs, wlconf dump, supplicant logs