This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: Channel 12/13 for FCC

Part Number: CC3200

Hi, 

In FCC specification, channel 12 and 13 are defined as below:

1. Wi-Fi Devices operating in Channels 12 and 13 In the U.S., Wi-Fi devices operating on channels 12 and 13 (in 2.4 GHz band under § 15.247 rules) must ensure that the maximum transmit power is properly adjusted to comply with the outof-band emission requirements.5  A Wi-Fi client device that relies on a network access point to determine if it can operate on channels 12 and 13 must ensure that its transmission will comply with the rules when operating in the U.S.6  If a Wi-Fi client device has the ability to operate at different power levels, it is not sufficient to use passive scanning alone, in order to meet the U.S. and non-U.S. requirements.  The client device must use a supplemental approach to ensure compliance while operating on these channels.  

As we know, channel 12 and 13 can be enabled if country code is EU.

Customer is asking whether they can set country code to be EU and then to pass FCC certification.

Regards,

Yonghua