This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1835MOD: Maximum conducted output power testing for Wi-FI

Part Number: WL1835MOD

Hi,

The calibrator wiki page states that the start_tx will send continuous transmission at 50% duty cycle. But the FCC regulations require atleast 98% duty cycle to do conducted power measurements.

How was this handled during the FCC certification of the module ?

Also I am using a spectrum analyzer (RSA306 with RBW, VBW limit of 20MHz) and dont have a power meter, Can you please suggest appropriate RBW and VBW settings for measuring 802.11b/g/n signals.

Also how to compoensate if my spectrum analyzer's bandwidth is not comparable to signal bandwidth ?

Thanks for the help.