Other Parts Discussed in Thread: WL1837MOD, WL1837
Hi,
I refer to the following of WL1837MOD datasheet.
Table 6-1. WLAN Performance Parameters
WL1837 MOD datasheet:
http://www.tij.co.jp/jp/lit/ds/symlink/wl1837mod.pdf
This list has the following definitions.
a)Sleep current: 160 µA Leakage, firmware retained Connected
b)IDLE: 750 µA No traffic IDLE connect
Please tell me when this measurement condition defines each.
1.Would I set WLAN_EN in low?
2.Is it time of the wait state in WOWLAN?
3.other ?
Best Regards,
Shigehiro Tsuda