This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100BOOST: Reg need of CC3100EMUBOOST

Part Number: CC3100BOOST
Other Parts Discussed in Thread: CC3100, CC3100MOD

Hello,

I am having a CC3100BOOST and MSP432p401r.

I wanted to know what are limitations that I would face for not having a CC3100EMUBOOST?

Can't the work of CC3100EMUBOOST be done by MSP432?

What is the role of SDK in CC3100BOOST?

By project consists of taking inputs from sensors connected to MSP432 and sending it to an online database via CC3100 and if the data is right according to the database, revert back to the MSP432 to signal an output.

Will I face a problem doing the above project using just CC3100BOOST and MSP432?

  • Hi Abhishek,

    The CC3100EMUBOOST gives you access to flashing the CC3100MOD serial flash. This is necessary for things such as updating to the latest service pack (which is always advised before troubleshooting or providing support on the forums) and adding user files such as HTML pages and certificates. You cannot flash the CC3100 through the MSP432 LaunchPad. I hope this helps.

    Best regards,
    Sarah