This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100BOOST: Connection of CC3100 with my wifi

Part Number: CC3100BOOST
Other Parts Discussed in Thread: CC3100, ENERGIA, CC3200

Hello,
I am having a problem with this cc3100and msp432.
I configured the cc3100 wifi and added my android wifi hotspot details into it.

Then uploaded the simplewebserverWifi example on energia, pressed the restart button but only line comes is Attempting to connect to Network named: abhi.matlotia  .

I think the code isn't working after Serial.print("Attempting to connect to Network named: "); this line.
Even if its not connecting to my wifi it should show not connected in serial port right?  
But the serial port just shows one line and nothing after that.
Kindly help on this.
The code used is -

#ifndef __CC3200R1M1RGC__
// Do not include SPI for CC3200 LaunchPad
#include <SPI.h>
#endif
#include <WiFi.h>

// your network name also called SSID
char ssid[] = "abhi.matlotia";
// your network password
char password[] = "supersecret";
// your network key Index number (needed only for WEP)
int keyIndex = 0;

WiFiServer server(80);

void setup() {
Serial.begin(115200); // initialize serial communication
pinMode(RED_LED, OUTPUT); // set the LED pin mode

// attempt to connect to Wifi network:
Serial.print("Attempting to connect to Network named: ");
// print the network name (SSID);
Serial.println(ssid);
// Connect to WPA/WPA2 network. Change this line if using open or WEP network:
WiFi.begin(ssid, password);
while ( WiFi.status() != WL_CONNECTED) {
// print dots while we wait to connect
Serial.print(".");
delay(300);
}

Serial.println("\nYou're connected to the network");
Serial.println("Waiting for an ip address");

while (WiFi.localIP() == INADDR_NONE) {
// print dots while we wait for an ip addresss
Serial.print(".");
delay(300);
}

Serial.println("\nIP Address obtained");

// you're connected now, so print out the status
printWifiStatus();

Serial.println("Starting webserver on port 80");
server.begin(); // start the web server on port 80
Serial.println("Webserver started!");
}

void loop() {
int i = 0;
WiFiClient client = server.available(); // listen for incoming clients

if (client) { // if you get a client,
Serial.println("new client"); // print a message out the serial port
char buffer[150] = {0}; // make a buffer to hold incoming data
while (client.connected()) { // loop while the client's connected
if (client.available()) { // if there's bytes to read from the client,
char c = client.read(); // read a byte, then
Serial.write(c); // print it out the serial monitor
if (c == '\n') { // if the byte is a newline character

// if the current line is blank, you got two newline characters in a row.
// that's the end of the client HTTP request, so send a response:
if (strlen(buffer) == 0) {
// HTTP headers always start with a response code (e.g. HTTP/1.1 200 OK)
// and a content-type so the client knows what's coming, then a blank line:
client.println("HTTP/1.1 200 OK");
client.println("Content-type:text/html");
client.println();

// the content of the HTTP response follows the header:
client.println("<html><head><title>Energia CC3200 WiFi Web Server</title></head><body align=center>");
client.println("<h1 align=center><font color=\"red\">Welcome to the CC3200 WiFi Web Server</font></h1>");
client.print("RED LED <button onclick=\"location.href='/H'\">HIGH</button>");
client.println(" <button onclick=\"location.href='/L'\">LOW</button><br>");

// The HTTP response ends with another blank line:
client.println();
// break out of the while loop:
break;
}
else { // if you got a newline, then clear the buffer:
memset(buffer, 0, 150);
i = 0;
}
}
else if (c != '\r') { // if you got anything else but a carriage return character,
buffer[i++] = c; // add it to the end of the currentLine
}

// Check to see if the client request was "GET /H" or "GET /L":
if (endsWith(buffer, "GET /H")) {
digitalWrite(RED_LED, HIGH); // GET /H turns the LED on
}
if (endsWith(buffer, "GET /L")) {
digitalWrite(RED_LED, LOW); // GET /L turns the LED off
}
}
}
// close the connection:
client.stop();
Serial.println("client disonnected");
}
}

//
//a way to check if one array ends with another array
//
boolean endsWith(char* inString, const char* compString) {
int compLength = strlen(compString);
int strLength = strlen(inString);

//compare the last "compLength" values of the inString
int i;
for (i = 0; i < compLength; i++) {
char a = inString[(strLength - 1) - i];
char b = compString[(compLength - 1) - i];
if (a != b) {
return false;
}
}
return true;
}

void printWifiStatus() {
// print the SSID of the network you're attached to:
Serial.print("SSID: ");
Serial.println(WiFi.SSID());

// print your WiFi IP address:
IPAddress ip = WiFi.localIP();
Serial.print("IP Address: ");
Serial.println(ip);

// print the received signal strength:
long rssi = WiFi.RSSI();
Serial.print("signal strength (RSSI):");
Serial.print(rssi);
Serial.println(" dBm");
// print where to go in a browser:
Serial.print("To see this page in action, open a browser to http://");
Serial.println(ip);
}