This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: BLE 4.2 support

Part Number: WL1837MOD
Other Parts Discussed in Thread: CC2650

Hi,

I was looking for a Wi-Fi + BLE4.2 solution and stumbled upon WL1837MOD. Initially I gave up on the module as the description states "Bluetooth 4.1 Compliance and CSA2 Support", however shortly after I have ran into TI Bluetooth 4.2 Stack Add-On link.

In the add-on description it is stated that it "Supports Bluetooth Core Specification v4.2" and it is intended for WL1837MOD. This is slightly confusing, could you please shed some light on it?

Ideally I am looking for FCC, CE certified Wi-Fi + BLE4.2 module, if WL1837OD does not support this is there another TI solution that does?

Thanks,
Nenad

  • Hi Nenad,

    Some of the Bluetooth 4.2 features (like LE secure connections and LE ping etc.) were added to the WL183x support through the TI Bluetooth 4.2 Stack add-on release that you referenced above. Also, the WL1837MOD is 4.2 certified as well : www.bluetooth.org/.../QLI_viewQDL.cfm

    The WL1837MOD is also FCC and CE certified.

    From your description above, it looks like the WL1837MOD fits the requirements. Are you looking for a specific BLE4.2 feature in your end product/use-case? Or the BT 4.2 certification stamp is all that is required?

    Best regards,
    Vihang
  • Hi Vihang,

    Indeed I am looking for a specific BLE4.2 feature, namely LE Data Packet Lenght Extension, as higher data throughputs are needed for the application.LE secure connections and LE Privacy are also nice to have. Is there a list of supported BLE4.2 features of the noted add-on?

    Essentially, radio I am looking for should communicate with CC2650 via BLE4.2 at data rates >200 kbps (plus Wi-Fi support I mentioned in previous post), and preferably the solution would come for TI. I can imagine this is a very specific requirement, nevertheless this is the situation.

    Best,
    Nenad