Other Parts Discussed in Thread: CC3100,
We are having trouble connecting to an enterprise network with the CC3120. This all works fine with the CC3100. Here is what I am seeing:
1) With a known good Server Root CA file, after I call sl_WlanConnect(), I get a SL_WLAN_EVENT_DISCONNECT event with reason code of 210 (SL_WLAN_DISCONNECT_CERTIFICATE_EXPIRED). The certificate we're using has an expiration of November 2017, and I verified that I set the date/time correctly.
2) I tried to disable server authentication just before the call to sl_WlanConnect(), but I still get the disconnect with reason of 210.
3) I tried reformatting the flash and not storing the Server Root CA file, and then connecting with server authentication disabled, but then I get a disconnect with reason of 209 (SL_WLAN_DISCONNECT_MISSING_CERT).
Any idea what could be going on here? I should also add that I am able to successfully perform a WPA2 connection, so the framework seems to be good.