This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1835MODCOM8B: WLAN/BLE continuous receiving mode

Part Number: WL1835MODCOM8B


Tool/software: Linux

Hi,


I have to checked the WLAN/BLE in continuous receiving mode and also tested it using random SOURCE/Destination MAC address.

WiFi continuous receiving : processors.wiki.ti.com/.../WL18xx_RX_Testing

BLE continuous receiving : http://processors.wiki.ti.com/index.php/WL18xx_Bluetopia_PM_Bluetooth_RF_Testing


But here in WiFi receiving mode, We have shown that to operate the WIFI in PLT mode , first need to down a wifi interface in board.

Because of that, in  continuous rx test our device is not connected to any outside device, so what do we fill in source MAC address and Destination MAC address fields of continuous RX mode because

we do not know the source MAC at that time.

Due to above mentioned issue, we got PER value near about 1 which is not suiatable for FCC certification of the custom device

Thanks,

Ankit