This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC3200: TI-RTOS uses fatfs on the _FS_REENTRANT reentrant function

Part Number: CC3200


Tool/software: TI-RTOS

CC3200 in the use of fatfs _FS_REENTRANT function, the following function I do not know how to amend (I can not find TI-RTOS mutex function), thanks

#if _FS_REENTRANT
/*------------------------------------------------------------------------*/
/* Create a Synchronization Object
/*------------------------------------------------------------------------*/
/* This function is called by f_mount() function to create a new
/  synchronization object, such as semaphore and mutex. When a 0 is
/  returned, the f_mount() function fails with FR_INT_ERR.
*/

int ff_cre_syncobj (	/* 1:Function succeeded, 0:Could not create due to any error */
	BYTE vol,			/* Corresponding logical drive being processed */
	_SYNC_t* sobj		/* Pointer to return the created sync object */
)
{
	int ret;


	*sobj = CreateMutex(NULL, FALSE, NULL);		/* Win32 */
	ret = (int)(*sobj != INVALID_HANDLE_VALUE);

//	*sobj = SyncObjects[vol];		/* uITRON (give a static created semaphore) */
//	ret = 1;

//	*sobj = OSMutexCreate(0, &err);	/* uC/OS-II */
//	ret = (int)(err == OS_NO_ERR);

//  *sobj = xSemaphoreCreateMutex();	/* FreeRTOS */
//	ret = (int)(*sobj != NULL);

	return ret;
}



/*------------------------------------------------------------------------*/
/* Delete a Synchronization Object                                        */
/*------------------------------------------------------------------------*/
/* This function is called in f_mount() function to delete a synchronization
/  object that created with ff_cre_syncobj() function. When a 0 is
/  returned, the f_mount() function fails with FR_INT_ERR.
*/

int ff_del_syncobj (	/* 1:Function succeeded, 0:Could not delete due to any error */
	_SYNC_t sobj		/* Sync object tied to the logical drive to be deleted */
)
{
	int ret;


	ret = CloseHandle(sobj);	/* Win32 */

//	ret = 1;					/* uITRON (nothing to do) */

//	OSMutexDel(sobj, OS_DEL_ALWAYS, &err);	/* uC/OS-II */
//	ret = (int)(err == OS_NO_ERR);

//  xSemaphoreDelete(sobj);		/* FreeRTOS */
//	ret = 1;

	return ret;
}



/*------------------------------------------------------------------------*/
/* Request Grant to Access the Volume                                     */
/*------------------------------------------------------------------------*/
/* This function is called on entering file functions to lock the volume.
/  When a FALSE is returned, the file function fails with FR_TIMEOUT.
*/

int ff_req_grant (	/* TRUE:Got a grant to access the volume, FALSE:Could not get a grant */
	_SYNC_t sobj	/* Sync object to wait */
)
{
	int ret;

	ret = (int)(WaitForSingleObject(sobj, _FS_TIMEOUT) == WAIT_OBJECT_0);	/* Win32 */

//	ret = (int)(wai_sem(sobj) == E_OK);			/* uITRON */

//	OSMutexPend(sobj, _FS_TIMEOUT, &err));		/* uC/OS-II */
//	ret = (int)(err == OS_NO_ERR);

//	ret = (int)(xSemaphoreTake(sobj, _FS_TIMEOUT) == pdTRUE);	/* FreeRTOS */

	return ret;
}



/*------------------------------------------------------------------------*/
/* Release Grant to Access the Volume                                     */
/*------------------------------------------------------------------------*/
/* This function is called on leaving file functions to unlock the volume.
*/

void ff_rel_grant (
	_SYNC_t sobj	/* Sync object to be signaled */
)
{
	ReleaseMutex(sobj);		/* Win32 */

//	sig_sem(sobj);			/* uITRON */

//	OSMutexPost(sobj);		/* uC/OS-II */

//	xSemaphoreGive(sobj);	/* FreeRTOS */
}

#endif