Other Parts Discussed in Thread: CC3200
Tool/software: Code Composer Studio
Ciao to everybody,
a ctm is almost finished his project (medical equipment) using a CC3200MOD.
They used Wi-Fi to remove the cable of an hand-held instrument, that normally is “sleeping” but it has to wake up and functioning as soon it is moved.
All their test are made with Win10 PC (they make also the PC side and/or they can choose the OS Windows version )
They use Wi-Fi Direct.
In this moment the connection is OK and well functioning, only when they use WLAN-Connect manual connection method.
So the time to be connected to the PC is about 30” (to much for a normal usage of the instrument).
Of course they know that if the “profile” is already saved, they can use an “Auto Connect” or even better a “Fast Connect”…..BUT it seams is not functioning. They have not found any reason why the faster way to connect are not functioning….
Do you have any suggestion or a functioning example (on the CC3200 EVB is 100% OK) ?
Feel free to ask any info you need to better understant the issue.
Thanks a lot in advance
Have a good day
Franco