Other Parts Discussed in Thread: CC3200SDK, CC3200
Hello,
In MQTT Application when i am going to change CLIENTID as NULL the all my code is freeze in CC3200SDK_1.3.0 but same works in older version of SDK i.e CC3200SDK_1.2.0
Why I'm going to make as NULL reason is - I've 2 CC3200 LP and both are running on the same server.If I allocate same CLIENTID i.e. "user1" to both then one will work and 2 one gets disconnected and vice versa because both client is having same ID. I want to make it dynamic or make it as null so both can work at same time on same server.
As above I mentioned as NULL ClientID is working well in old sdk but not working in new sdk .I don't want to change every time the CLIENTID in the code.
connect_config usr_connect_config[] =
{
{
{
{
SL_MQTT_NETCONN_URL,
SERVER_ADDRESS,
PORT_NUMBER,
0,
0,
0,
NULL
},
SERVER_MODE,
true,
},
NULL,
"user1",
NULL,
NULL,
true,
KEEP_ALIVE_TIMER,
{Mqtt_Recv, sl_MqttEvt, sl_MqttDisconnect},
TOPIC_COUNT,
{TOPIC1, TOPIC2, TOPIC3},
{QOS2, QOS2, QOS2},
{WILL_TOPIC,WILL_MSG,WILL_QOS,WILL_RETAIN},
false
}
};
Best Regards,
Shashank