Tool/software: Linux
Hello all,
I am interfacing Wl1271 with imx6quad processor and ODIN-W160 chip for wifi.
I have compiled my driver with Linux Kernel version-3.10.17
When i load the drivers and make interface up once in my board. the firmware is loading.
I am getting Wlan0 interface also, but unable to communicate with Wlan0.
The firmware files for Wireless LAN is wl1273-ODIN-W160.bin and it is renamed as wl127x-fw-5-sr.bin and installed at "/lib/firmware/ti-connectivity/".
When i give “iw wlan0 scan” , am not getting any results. Minicom log file is attached with this query forum. Please do check it and help me to solve this issue as soon a possible.
U-Boot 2013.04 (Oct 13 2016 - 10:47:01)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 43 C, calibration data: 0x5964dc7d
Reset cause: POR
Board: i.MX6Q iW-RAINBOW-G15M-MXM
Boot Device: UNKNOWN
DRAM: 4 GiB WARNING: Caches not enabled
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2, FSL_SDHC: 3
In: serial
Out: serial
Err: serial
Board Info:
BSP Version : iW-EMDO9-SC-01-R3.0-REL1.0-Linux3.10
SOM Version : iW-EMDO9-AP-01-R3.x
CPU Unique ID : 0x110e71d4df63c0a1
Net: PHY indentify @ 0x1 = 0x00221622
Configuring PHY skew timing for Micrel ksz9031
FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 1 0
mmc3 is current device
reading uImage
5342448 bytes read in 249 ms (20.5 MiB/s)
reading imx6qd-iwg15m-mxm_ldoactive.dtb
48288 bytes read in 23 ms (2 MiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.17
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5342384 Bytes = 5.1 MiB
Load Address: 10800000
Entry Point: 10800000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
OK
Using Device Tree in place at 18000000, end 1800ec9f
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.17 (root@aishwariya) (gcc version 4.8.4 (Ubuntu/Linaro 4.8.4-2ubuntu1~14.04.1) ) #131 SMP PREEMPT Wed Jul 5 17:38:44 IST 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: iW-RainboW-G15 platform based on i.MX6 (Device Tree), model: iWave RainboW-G15M-MXM Board based on Freescale i.MX6 Quad/Dual
cma: CMA: reserved 320 MiB at 6a000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @819e5000 s9088 r8192 d15488 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520720
Kernel command line: console=ttymxc3,115200n8 root=/dev/mmcblk0p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 2048MB = 2048MB total
Memory: 1740552k/1740552k available, 356600k reserved, 270336K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
lowmem : 0x80000000 - 0xef800000 (1784 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80885184 (8693 kB)
.init : 0x80886000 - 0x80907380 ( 517 kB)
.data : 0x80908000 - 0x80962f88 ( 364 kB)
.bss : 0x80962f88 - 0x809cb00c ( 417 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.5
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80636450 - 0x806364a8
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: Booted secondary processor
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: Booted secondary processor
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
reg-dummy reg-dummy: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
reg-dummy reg-dummy: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
anatop_regulator regulator-1p1.4: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-1p1.4: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
vdd1p1: 800 <--> 1375 mV at 1125 mV
anatop_regulator regulator-3p0.5: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-3p0.5: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
vdd3p0: 2800 <--> 3150 mV at 3000 mV
anatop_regulator regulator-2p5.6: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-2p5.6: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
vdd2p5: 2000 <--> 2750 mV at 2425 mV
anatop_regulator regulator-vddcore.7: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-vddcore.7: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
cpu: 725 <--> 1450 mV at 1150 mV
anatop_regulator regulator-vddpu.8: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-vddpu.8: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
vddpu: 725 <--> 1450 mV
anatop_regulator regulator-vddsoc.9: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
anatop_regulator regulator-vddsoc.9: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
vddsoc: 725 <--> 1450 mV at 1200 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
Board Info:
BSP Version : iW-EMDO9-SC-01-R3.0-REL1.0-Linux3.10
SOM Version : iW-EMDO9-AP-01-R3.x
CPU Unique ID : 0x110e71d4df63c0a1
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
reg-fixed-voltage fixedregulator.16:
######################################Gpio value is: 204######################################
reg-fixed-voltage fixedregulator.16:
###################################### after setting high gpio get value is: 0######################################
reg-fixed-voltage fixedregulator.16: ********************Inside else of enabled_at_boot and setting low*********************
reg-fixed-voltage fixedregulator.16: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
reg-fixed-voltage fixedregulator.16: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:204@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
wlan-en-regulator: ^^^^^^^^^^^^^^^ inside gpio valid if condition=:204 ^^^^^^^^^^^^^^^^
wlan-en-regulator: ########### else of Gpio high and gpio_flag=0 ###################
wlan-en-regulator: ########### else of Gpio invert ###################
wlan-en-regulator: 1800 mV
reg-fixed-voltage 2p5v.18:
######################################Gpio value is: -2######################################
reg-fixed-voltage 2p5v.18:
###################################### after setting high gpio get value is: 0######################################
reg-fixed-voltage 2p5v.18: ********************Inside else of enabled_at_boot and setting high*********************
reg-fixed-voltage 2p5v.18: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
reg-fixed-voltage 2p5v.18: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
2P5V: 2500 mV
reg-fixed-voltage 3p3v.19:
######################################Gpio value is: -2######################################
reg-fixed-voltage 3p3v.19:
###################################### after setting high gpio get value is: 0######################################
reg-fixed-voltage 3p3v.19: ********************Inside else of enabled_at_boot and setting high*********************
reg-fixed-voltage 3p3v.19: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
reg-fixed-voltage 3p3v.19: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
3P3V: 3300 mV
reg-fixed-voltage 0p0v.20:
######################################Gpio value is: -2######################################
reg-fixed-voltage 0p0v.20:
###################################### after setting high gpio get value is: 0######################################
reg-fixed-voltage 0p0v.20: ********************Inside else of enabled_at_boot and setting high*********************
reg-fixed-voltage 0p0v.20: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
reg-fixed-voltage 0p0v.20: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
0P0V: no parameters
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switching to clocksource mxc_timer1
PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
pci 0000:00:00.0: BAR 8: assigned [mem 0x01100000-0x011fffff]
pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]
pci 0000:00:00.0: BAR 7: assigned [io 0x1000-0x1fff]
pci 0000:01:00.0: BAR 0: assigned [mem 0x01100000-0x0117ffff]
pci 0000:01:00.0: BAR 3: assigned [mem 0x01180000-0x01183fff]
pci 0000:01:00.0: BAR 2: assigned [io 0x1000-0x101f]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
pci 0000:00:00.0: bridge window [mem 0x01100000-0x011fffff]
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP: reno registered
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx6_busfreq busfreq.14: DDR medium rate not supported.
Bus freq driver module loaded
bounce pool size: 64 pages
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 3511
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
pwm-backlight backlight.26: unable to request PWM, trying legacy API
pwm-backlight backlight.27: unable to request PWM, trying legacy API
pwm-backlight backlight.27: unable to request legacy PWM
pwm-backlight: probe of backlight.27 failed with error -16
mxc_sdc_fb fb.23: register mxc display driver hdmi
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 240x67
mxc_sdc_fb fb.24: register mxc display driver ldb
mxc_sdc_fb fb.24: NO mxc display driver found!
mxc_sdc_fb fb.25: register mxc display driver ldb
mxc_sdc_fb fb.25: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
Serial: IMX driver
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_CSI0_DAT10 already requested by 20e0000.iomuxc; cannot claim for 2020000.serial
imx6q-pinctrl 20e0000.iomuxc: pin-160 (2020000.serial) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 160 on device 20e0000.iomuxc
imx-uart 2020000.serial: Error applying setting, reverse things back
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_EIM_D27 already requested by 20e0000.iomuxc; cannot claim for 21e8000.serial
imx6q-pinctrl 20e0000.iomuxc: pin-48 (21e8000.serial) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 48 on device 20e0000.iomuxc
imx-uart 21e8000.serial: Error applying setting, reverse things back
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
console [ttymxc3] enabled
serial: Freescale lpuart driver
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
at24 2-0051: 8192 byte 24c64 EEPROM, writable, 32 bytes/write
Wait for CR ACK error!
sata phy RX_PLL is stable!
ahci: SSS flag set, parallel bus scan disabled
ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
m25p80 spi32766.0: found sst25vf016b, expected m25p32
m25p80 spi32766.0: sst25vf016b (2048 Kbytes)
spi_imx 2008000.ecspi: probed
m25p80 spi32765.0: found mr25h256, expected m25p32
m25p80 spi32765.0: mr25h256 (32 Kbytes)
spi_imx 2014000.ecspi: probed
CAN device driver interface
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: max11801_ts as /devices/soc0/soc.0/2100000.aips-bus/21a0000.i2c/i2c-0/0-0049/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
ov7725_read_reg:write reg error:reg=a
camera ov7725 is not found
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
Bluetooth: Virtual HCI driver ver 1.3
usbcore: registered new interface driver bfusb
usbcore: registered new interface driver btusb
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
mmc0: no vqmmc regulator found
wlan-en-regulator: ******************** inside regulator_enable*********************
wlan-en-regulator: ************************** Inside _regulator_enable ***************************
wlan-en-regulator: ******************regulator_enable's gpio value is= d81bda40****************
wlan-en-regulator: !!!!!!!!!!!!!!!!!!!!!!!!!!!!!return value is=0!!!!!!!!!!!!!!!!!!!!!!!!!!
wlan-en-regulator: ************************* INside _regulator_do_enable function ***************************
wlan-en-regulator: ******************regulator_get_enable_time***********************
wlan-en-regulator: ************************* INside _regulator_do_enable function AND Return value is=70000 ***************************
wlan-en-regulator: *************** INside _regulator_do_enable function AND Return value is greater than and equal to *****************
wlan-en-regulator: ****************** gpio value is= d81bda40****************
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable condition and gpio=204 $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable count condition and gpio=204 BEFORE $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable count condition and gpio=204 AFTER $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ gpio get value=0 $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
ata1: SATA link down (SStatus 0 SControl 300)
usb 1-1: new high-speed USB device number 2 using ci_hdrc
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing unknown CIS tuple 0x91 (3 bytes)
mmc0: new SDIO card at address 0001
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
mmc1: host does not support reading read-only switch. assuming write-enable.
mmc1: new high speed SDHC card at address 0007
mmcblk0: mmc1:0007 SS08G 7.21 GiB
mmc3: no vmmc regulator found
mmcblk0: p1 p2
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mmc2: host does not support reading read-only switch. assuming write-enable.
mmc2: new high speed SDHC card at address aaaa
mmcblk1: mmc2:aaaa SS08G 7.40 GiB
mmcblk1: p1 p2
mmc3: BKOPS_EN bit is not set
Galcore version 4.6.9.9754
mmc3: new high speed DDR MMC card at address 0001
mmcblk2: mmc3:0001 SEM32G 29.1 GiB
mmcblk2boot0: mmc3:0001 SEM32G partition 1 4.00 MiB
mmcblk2boot1: mmc3:0001 SEM32G partition 2 4.00 MiB
mmcblk2rpmb: mmc3:0001 SEM32G partition 3 4.00 MiB
vddpu: ******************** inside regulator_enable*********************
vddpu: ************************** Inside _regulator_enable ***************************
mmcblk2: p1 p2
vddpu: ******************regulator_enable's gpio value is= 0****************
vddpu: !!!!!!!!!!!!!!!!!!!!!!!!!!!!!return value is=0!!!!!!!!!!!!!!!!!!!!!!!!!!
vddpu: ************************* INside _regulator_do_enable function ***************************
vddpu: ******************regulator_get_enable_time***********************
mmcblk2boot1: unknown partition table
vddpu: ************************* INside _regulator_do_enable function AND Return value is=129 ***************************
vddpu: *************** INside _regulator_do_enable function AND Return value is greater than and equal to *****************
mmcblk2boot0: unknown partition table
vddpu: ****************** gpio value is= 0****************
vddpu: **************INside _regulator_do_enable function, if else condition ***************
vddpu: ******************** inside regulator_enable*********************
vddpu: ************************** Inside _regulator_enable ***************************
vddpu: ******************** inside regulator_enable*********************
vddpu: ************************** Inside _regulator_enable ***************************
vddpu: ********************** inside regulator_do_disabble****************************
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)
caam 2100000.caam: job rings = 2, qi = 0
caam 2100000.caam: authenc-hmac-md5-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-aes-caam
caam 2100000.caam: authenc-hmac-md5-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-md5-cbc-des-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-des-caam
caam 2100000.caam: ecb-des-caam
caam 2100000.caam: ecb-arc4-caam
caam 2100000.caam: ecb-aes-caam
caam 2100000.caam: ctr-aes-caam
caam 2100000.caam: cbc-aes-caam
caam 2100000.caam: ecb-des3-caam
caam 2100000.caam: cbc-3des-caam
caam 2100000.caam: cbc-des-caam
caam 2100000.caam: fsl,sec-v4.0 algorithms registered in /proc/crypto
platform 2101000.jr0: registering rng-caam
platform caam_sm: caam_sm_test: 8-byte key test match OK
platform caam_sm: caam_sm_test: 16-byte key test match OK
platform caam_sm: caam_sm_test: 32-byte key test match OK
platform caam_secvio.30: security violation service handlers armed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000 2-000a: sgtl5000 revision 0x11
sgtl5000 2-000a: @@@@@@@@@@@@@@@@@@@@@@@@@@@@Calling regulator register function@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
sgtl5000 2-000a: @@@@@@@@@@@@@@@@@@@@@@@@@@ begining gpio value is:0@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
2-000a: 1200 mV normal
sgtl5000 2-000a: Using internal LDO instead of VDDD
2-000a: ******************** inside regulator_enable*********************
2-000a: ************************** Inside _regulator_enable ***************************
2-000a: ******************regulator_enable's gpio value is= 0****************
2-000a: !!!!!!!!!!!!!!!!!!!!!!!!!!!!!return value is=0!!!!!!!!!!!!!!!!!!!!!!!!!!
2-000a: ************************* INside _regulator_do_enable function ***************************
2-000a: ******************regulator_get_enable_time***********************
2-000a: ************************* INside _regulator_do_enable function AND Return value is=0 ***************************
2-000a: *************** INside _regulator_do_enable function AND Return value is greater than and equal to *****************
2-000a: ****************** gpio value is= 0****************
2-000a: **************INside _regulator_do_enable function, if else condition ***************
2-000a: ******************** inside regulator_enable*********************
2-000a: ************************** Inside _regulator_enable ***************************
imx-sgtl5000 sound.22: sgtl5000 <-> 2028000.ssi mapping ok
imx-audio-hdmi sound-hdmi.21: hdmi-hifi <-> hdmi_audio.15 mapping ok
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Bridge firewalling registered
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
ALSA device list:
#0: imx6-audio-sgtl5000
#1: imx-hdmi-soc
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 516K (80886000 - 80907000)
INIT: version 2.88 booting
Starting udev
udevd[191]: starting version 182
Loading modules backported from Linux version R8.5-0-gcb51164
Backport generated by backports.git R8.4-0-g0d46f43
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: World regulatory domain updated:
cfg80211: DFS Master region: unset
cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
cfg80211: (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
wlan-en-regulator: ********************** inside regulator_do_disabble****************************
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable condition and gpio=204 $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: **************** disable condition and gpio=204 ******************************** r
wlcore: loaded
wlcore: driver version: R8.7_SP1
wlcore: compilation time: Tue Dec 20 09:17:25 2016
EXT4-fs (mmcblk2p2): recovery complete
EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)
FAT-fs (mmcblk2p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
EXT4-fs (mmcblk1p2): recovery complete
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
UIM SYSFS Node Not Found
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
ALSA: Restoring mixer settings...
Configuring network interfaces... ifup: ignoring unknown interface eth0
Starting rpcbind daemon...done.
net.ipv4.conf.default.rp_filter = 1
net.ipv4.conf.all.rp_filter = 1
Fri Jan 9 16:18:00 UTC 2015
INIT: Entering runlevel: 5
Starting Xserver
Starting system message bus: dbus.
Starting Connection Manager
Starting Dropbear SSH server: dropbear.
creating NFS state directory: fec 2188000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
done
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon
...done.
Starting Telephony daemon
Starting Linux NFC daemon
Starting OProfileUI server
Running local boot scripts (/etc/rc.local).
Stopping Bootlog daemon: bootlogd.
Rootfs Version : iW-EMDO9-SC-01-R3.0-REL1.0-YoctoPoky
Poky (Yocto Project Reference Distro) 1.5.1 iWave-G15M /dev/ttymxc3
iWave-G15M login: root
root@iWave-G15M:~# rfkill unblock all
root@iWave-G15M:~# iwconfig
wlan0 IEEE 802.11abgn ESSID:off/any
Mode:Managed Access Point: Not-Associated Tx-Power=0 dBm
Retry short limit:7 RTS thr:off Fragment thr:off
Encryption key:off
Power Management:on
sit0 no wireless extensions.
lo no wireless extensions.
eth0 no wireless extensions.
root@iWave-G15M:~# ifconfig wlan0 up
wlan-en-regulator: ******************** inside regulator_enable*********************
wlan-en-regulator: ************************** Inside _regulator_enable ***************************
wlan-en-regulator: ******************regulator_enable's gpio value is= d81bda40****************
wlan-en-regulator: !!!!!!!!!!!!!!!!!!!!!!!!!!!!!return value is=0!!!!!!!!!!!!!!!!!!!!!!!!!!
wlan-en-regulator: ************************* INside _regulator_do_enable function ***************************
wlan-en-regulator: ******************regulator_get_enable_time***********************
wlan-en-regulator: ************************* INside _regulator_do_enable function AND Return value is=70000 ***************************
wlan-en-regulator: *************** INside _regulator_do_enable function AND Return value is greater than and equal to *****************
wlan-en-regulator: ****************** gpio value is= d81bda40****************
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable condition and gpio=204 $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable count condition and gpio=204 BEFORE $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ enable count condition and gpio=204 AFTER $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlan-en-regulator: $$$$$$$$$$$$$$$$$$$$$$ gpio get value=0 $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
wlcore: firmware booted (Rev 6.3.10.100.135)
IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
root@iWave-G15M:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:01:02:03:04:05
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:2 errors:0 dropped:0 overruns:0 frame:0
TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:100 (100.0 B) TX bytes:100 (100.0 B)
wlan0 Link encap:Ethernet HWaddr D4:CA:6E:70:9E:F5
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@iWave-G15M:~# iw --debug iw wlan0 scan
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 20 <0x14>
.flags = 5 <REQUEST,ACK>
.seq = 1420820412
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 33
.version = 0
.unused = 0
[PAYLOAD] 16 octets
08 00 03 00 04 00 00 00 08 00 2d 00 04 00 01 00 ..........-.....
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820412
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 20 <0x14>
.flags = 5 <REQUEST,ACK>
.seq = 1420820412
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820413
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 1
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 116
.type = 16 <genl/family::nlctrl>
.flags = 0 <>
.seq = 1420820413
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 1
.version = 2
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
[ATTR 01] 2 octets
10 00 ..
[PADDING] 2 octets
00 00 ..
[ATTR 03] 4 octets
02 00 00 00 ....
[ATTR 04] 4 octets
00 00 00 00 ....
[ATTR 05] 4 octets
07 00 00 00 ....
[ATTR 06] 20 octets
14 00 01 00 08 00 01 00 03 00 00 00 08 00 02 00 ................
0e 00 00 00 ....
[ATTR 07] 24 octets
18 00 01 00 08 00 02 00 10 00 00 00 0b 00 01 00 ................
6e 6f 74 69 66 79 00 00 notify..
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820413
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 16 <0x10>
.flags = 5 <REQUEST,ACK>
.seq = 1420820413
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820414
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 0
.unused = 0
[ATTR 02] 8 octets
6e 6c 38 30 32 31 31 00 nl80211.
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820415
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 1
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 116
.type = 16 <genl/family::nlctrl>
.flags = 0 <>
.seq = 1420820415
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 1
.version = 2
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
[ATTR 01] 2 octets
10 00 ..
[PADDING] 2 octets
00 00 ..
[ATTR 03] 4 octets
02 00 00 00 ....
[ATTR 04] 4 octets
00 00 00 00 ....
[ATTR 05] 4 octets
07 00 00 00 ....
[ATTR 06] 20 octets
14 00 01 00 08 00 01 00 03 00 00 00 08 00 02 00 ................
0e 00 00 00 ....
[ATTR 07] 24 octets
18 00 01 00 08 00 02 00 10 00 00 00 0b 00 01 00 ................
6e 6f 74 69 66 79 00 00 notify..
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820415
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 16 <0x10>
.flags = 5 <REQUEST,ACK>
.seq = 1420820415
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820416
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 0
.unused = 0
[ATTR 02] 8 octets
6e 6c 38 30 32 31 31 00 nl80211.
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820417
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 1
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 116
.type = 16 <genl/family::nlctrl>
.flags = 0 <>
.seq = 1420820417
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 1
.version = 2
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
[ATTR 01] 2 octets
10 00 ..
[PADDING] 2 octets
00 00 ..
[ATTR 03] 4 octets
02 00 00 00 ....
[ATTR 04] 4 octets
00 00 00 00 ....
[ATTR 05] 4 octets
07 00 00 00 ....
[ATTR 06] 20 octets
14 00 01 00 08 00 01 00 03 00 00 00 08 00 02 00 ................
0e 00 00 00 ....
[ATTR 07] 24 octets
18 00 01 00 08 00 02 00 10 00 00 00 0b 00 01 00 ................
6e 6f 74 69 66 79 00 00 notify..
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820417
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 16 <0x10>
.flags = 5 <REQUEST,ACK>
.seq = 1420820417
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820418
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 0
.unused = 0
[ATTR 02] 8 octets
6e 6c 38 30 32 31 31 00 nl80211.
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820419
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 1
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 116
.type = 16 <genl/family::nlctrl>
.flags = 0 <>
.seq = 1420820419
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 1
.version = 2
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
[ATTR 01] 2 octets
10 00 ..
[PADDING] 2 octets
00 00 ..
[ATTR 03] 4 octets
02 00 00 00 ....
[ATTR 04] 4 octets
00 00 00 00 ....
[ATTR 05] 4 octets
07 00 00 00 ....
[ATTR 06] 20 octets
14 00 01 00 08 00 01 00 03 00 00 00 08 00 02 00 ................
0e 00 00 00 ....
[ATTR 07] 24 octets
18 00 01 00 08 00 02 00 10 00 00 00 0b 00 01 00 ................
6e 6f 74 69 66 79 00 00 notify..
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820419
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 16 <0x10>
.flags = 5 <REQUEST,ACK>
.seq = 1420820419
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820420
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 0
.unused = 0
[ATTR 02] 8 octets
6e 6c 38 30 32 31 31 00 nl80211.
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820421
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 1
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 116
.type = 16 <genl/family::nlctrl>
.flags = 0 <>
.seq = 1420820421
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 1
.version = 2
.unused = 0
[ATTR 02] 7 octets
6e 6c 63 74 72 6c 00 nlctrl.
[PADDING] 1 octets
00 .
[ATTR 01] 2 octets
10 00 ..
[PADDING] 2 octets
00 00 ..
[ATTR 03] 4 octets
02 00 00 00 ....
[ATTR 04] 4 octets
00 00 00 00 ....
[ATTR 05] 4 octets
07 00 00 00 ....
[ATTR 06] 20 octets
14 00 01 00 08 00 01 00 03 00 00 00 08 00 02 00 ................
0e 00 00 00 ....
[ATTR 07] 24 octets
18 00 01 00 08 00 02 00 10 00 00 00 0b 00 01 00 ................
6e 6f 74 69 66 79 00 00 notify..
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 36
.type = 2 <ERROR>
.flags = 0 <>
.seq = 1420820421
.port = 1207960325
[ERRORMSG] 20 octets
.error = 0 "Success"
[ORIGINAL MESSAGE] 16 octets
.nlmsg_len = 16
.type = 16 <0x10>
.flags = 5 <REQUEST,ACK>
.seq = 1420820421
.port = 1207960325
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 32
.type = 16 <genl/family::nlctrl>
.flags = 5 <REQUEST,ACK>
.seq = 1420820422
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 3
.version = 0
.unused = 0
[ATTR 02] 8 octets
6e 6c 38 30 32 31 31 00 nl80211.
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 388
.type = 20 <0x14>
.flags = 0 <>
.seq = 0
.port = 0
[GENERIC NETLINK HEADER] 4 octets
.cmd = 34
.version = 1
.unused = 0
[PAYLOAD] 368 octets
08 00 01 00 00 00 00 00 08 00 03 00 04 00 00 00 ................
0c 00 99 00 01 00 00 00 00 00 00 00 08 00 2d 00 ..............-.
04 00 00 00 4c 01 2c 00 08 00 00 00 6c 09 00 00 ....L.,.....l...
08 00 01 00 71 09 00 00 08 00 02 00 76 09 00 00 ....q.......v...
08 00 03 00 7b 09 00 00 08 00 04 00 80 09 00 00 ....{...........
08 00 05 00 85 09 00 00 08 00 06 00 8a 09 00 00 ................
08 00 07 00 8f 09 00 00 08 00 08 00 94 09 00 00 ................
08 00 09 00 99 09 00 00 08 00 0a 00 9e 09 00 00 ................
08 00 0b 00 a3 09 00 00 08 00 0c 00 a8 09 00 00 ................
08 00 0d 00 b4 09 00 00 08 00 0e 00 3c 14 00 00 ............<...
08 00 0f 00 46 14 00 00 08 00 10 00 50 14 00 00 ....F.......P...
08 00 11 00 5a 14 00 00 08 00 12 00 64 14 00 00 ....Z.......d...
08 00 13 00 6e 14 00 00 08 00 14 00 78 14 00 00 ....n.......x...
08 00 15 00 8c 14 00 00 08 00 16 00 a0 14 00 00 ................
08 00 17 00 b4 14 00 00 08 00 18 00 c8 14 00 00 ................
08 00 19 00 7c 15 00 00 08 00 1a 00 90 15 00 00 ....|...........
08 00 1b 00 a4 15 00 00 08 00 1c 00 b8 15 00 00 ................
08 00 1d 00 cc 15 00 00 08 00 1e 00 e0 15 00 00 ................
08 00 1f 00 f4 15 00 00 08 00 20 00 08 16 00 00 .......... .....
08 00 21 00 1c 16 00 00 08 00 22 00 30 16 00 00 ..!.......".0...
08 00 23 00 44 16 00 00 08 00 24 00 71 16 00 00 ..#.D.....$.q...
08 00 25 00 85 16 00 00 08 00 26 00 99 16 00 00 ..%.......&.....
08 00 27 00 ad 16 00 00 08 00 28 00 c1 16 00 00 ..'.......(.....
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Sent Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 28
.type = 20 <0x14>
.flags = 773 <REQUEST,ACK,ROOT,MATCH>
.seq = 1420820423
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 32
.version = 0
.unused = 0
[PAYLOAD] 8 octets
08 00 03 00 04 00 00 00 ........
--------------------------- END NETLINK MESSAGE ---------------------------
-- Debug: Received Message:
-------------------------- BEGIN NETLINK MESSAGE ---------------------------
[NETLINK HEADER] 16 octets
.nlmsg_len = 20
.type = 3 <DONE>
.flags = 2 <MULTI>
.seq = 1420820423
.port = 1207960325
[GENERIC NETLINK HEADER] 4 octets
.cmd = 0
.version = 0
.unused = 0
--------------------------- END NETLINK MESSAGE ---------------------------
root@iWave-G15M:~#
Thanks and Regards,
Aishwarya Bhat