Part Number: WL1831MOD
Tool/software: Linux
We are using the WL1831MOD device and want to configure the platform to provide multi BSSID functionality. From what I see the WL18XX device and driver rely on hostapd to provide this functionality.
Can the WL18XX device/driver work with the Linux Network Manager when the Network Manager has been used to bring up an AP?
I believe that the Network Manager does not work with Hostapd but instead uses wpa-supplicant when it is setup to start an AP. In fact I think the Network Manager cannot work with hostapd. It uses the AP functionality that is built into wpa-supplicant. Can this setup (Network Manager + wpa-supplicant) also be used to support multi BSSID functionality or is hostapd required.
Thanks,
Bruno