This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1835MODCOM8B: WL1835MODCOM8B WLAN not working with kernel 2.6.37 on Customized DM385 board with IPNC RDK 3.5 version

Part Number: WL1835MODCOM8B
Other Parts Discussed in Thread: DM385, WL1835, ADS7846, TSC2007, TSC2004, PCF8574, TPS65010, TPS65910, BQ24022, LP3971, LP3972, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS7303, TLV320AIC3110, DA8XX, LP3944, LP5521, LP5523, DAC124S085, WL1271

When following the build guide http://processors.wiki.ti.com/index.php/WL18xx_Platform_Integration_Guide  the CONFIG_WL12XX_PLATFORM_DATA  switch in the config file is not present so I am running the specified scripts in the guide.

I see see the following errors when running the scripts::

msmith@msmith-VirtualBox:~/qt/wilink8-wlan-build-utilites$ IP_TABLES=1 verify_kernel_config.sh /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel/arch/arm/configs/dm385_cbb_ubifs_defconfig

verify_kernel_config.sh: command not found

msmith@msmith-VirtualBox:~/qt/wilink8-wlan-build-utilites$ ./verify_kernel_config.sh /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel/arch/arm/configs/dm385_cbb_ubifs_defconfig

Validating kernel .config (base_config[@])

msmith@msmith-VirtualBox:~/qt/wilink8-wlan-build-utilites$

I have tried various combinations to execute the "IP_TABLES=1 verify_kernel_config.sh .config " with no luck. As per the build guide below:

Note: In case there are missing kernel switches like CONFIG_WL12XX_PLATFORM_DATA, then there probably is a missing part in the kernel that relates to the WL127x chipset, and patches should be applied.

Script usage

Usage: <option=1> verify_kernel_config.sh <kernel_config_file>

options:

IP_TABLES - add ip tables support

NO_DEVICE_TREE - add support for non device tree compilation

BT_HCI - add support for BT HCI

For example, for adding the IP_TABLES support use :

IP_TABLES=1 verify_kernel_config.sh .config

 

I have searched this error but so far can't find the solution.

Any ideas?

 

  • Hi ,
    We have assigned your query to relevant expert and will get back to you shortly .

    Thanks
    Saurabh
  • Thank You!
  • I'm making progress but getting this error when running ./build-ipnc-wifi.sh to install r8.4.
    I'm using r8.4 because it is ported for kernel 2.6.37.
    Below is my setup-env file:
    #========================oOO==(_)==OOo=======================
    # This file contains the exports needed for automating the
    # build process of WLAN components.
    # Place this file in the same directory with wl18xx_build.sh
    # build scripts. No need to run 'source setup-env', the build
    # scripts will perfom it internaly.
    #===========================================================
    # User specific environment settings - use full PATH


    # if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain.
    export TOOLCHAIN_PATH=${PATH__ROOT}/../../linux_devkit/bin

    # if DEFAULT path to root filesystem is set ./fs folder will be used.
    #export ROOTFS=${PATH__ROOT}/../../../ipnc_rdk/target/filesys
    export ROOTFS="/home/msmith/nfs-stuff/filesys"
    #if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version)
    #export KERNEL_PATH=${PATH__ROOT}/../../ipnc_psp_arago/kernel
    export KERNEL_PATH="/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel"
    export CROSS_COMPILE=arm-arago-linux-gnueabi-

    export ARCH=arm

    [ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH

    # Set this if the filesystem needs root access to install the build
    export ROOT_ACCESS_REQUIRED=n



    Below is the error in the error I am getting:
    CC /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore.mod.o
    LD [M] /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore.ko
    CC /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore_sdio.mod.o
    LD [M] /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore_sdio.ko
    CC /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/mac80211/mac80211.mod.o
    LD [M] /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/mac80211/mac80211.ko
    CC /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/wireless/cfg80211.mod.o
    LD [M] /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/wireless/cfg80211.ko
    ****** *******
    make: Entering directory '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel'
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/compat/compat.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wl12xx/wl12xx.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wl18xx/wl18xx.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/drivers/net/wireless/ti/wlcore/wlcore_sdio.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/mac80211/mac80211.ko
    INSTALL /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/compat_wireless/net/wireless/cfg80211.ko
    DEPMOD 2.6.37_DM385_CBB_1.50.50
    depmod: WARNING: could not open /home/msmith/nfs-stuff/filesys/lib/modules/2.6.37_DM385_CBB_1.50.50/modules.order: No such file or directory
    depmod: WARNING: /home/msmith/nfs-stuff/filesys/lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/mac80211/mac80211.ko needs unknown symbol unregister_inet6addr_notifier
    depmod: WARNING: /home/msmith/nfs-stuff/filesys/lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/mac80211/mac80211.ko needs unknown symbol register_inet6addr_notifier
    depmod: WARNING: could not open /home/msmith/nfs-stuff/filesys/lib/modules/2.6.37_DM385_CBB_1.50.50/modules.builtin: No such file or directory
    make: Leaving directory '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel'
    ****** *******
    make: *** No rule to make target 'clean'. Stop.
    ****** *******
    make: *** No targets specified and no makefile found. Stop.
    ****** ERROR 0 *******
    msmith@msmith-VirtualBox:~/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4$


    BTW, I do have the modules.order and modules.builtin located in my " /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/cbb_psp_04_04_00_02/kernel" folder
  • Still no luck....

    The build is failing  - cd: /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel: No such file or directory

    there is no kernel directory in /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src

    Should it be built here by the scripts?

    I have spent weeks trying to build the drivers for the TI wifi modules with no luck Every guide I follow has a road block...

    smith@msmith-VirtualBox:~/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites$ ./build_wl18xx-dm.sh kernel_modules
     Changing ROOTFS path to /home/msmith/nfs-stuff/filesys
     Using user defined kernel
    Makefile was found. Kernel version was set to 2.6.37.
       *****  building only Driver modules  *****  
    ./build_wl18xx-dm.sh: line 104: cd: /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel: No such file or directory
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/configuration/kernel_2.6.config': No such file or directory
    make: *** No rule to make target 'clean'.  Stop.
    ******  *******
    make: *** No rule to make target 'uImage'.  Stop.
    make: *** No rule to make target 'am335x-evm.dtb'.  Stop.
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel/arch/arm/boot/zImage': No such file or directory
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel/arch/arm/boot/dts/am335x-evm.dtb': No such file or directory
    ****** ERROR 0 *******
    msmith@msmith-VirtualBox:~/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites$ ./build_wl18xx-dm.sh kernel_modules
     Changing ROOTFS path to /home/msmith/nfs-stuff/filesys
     Using user defined kernel
    Makefile was found. Kernel version was set to 2.6.37.
       *****  building only Driver modules  *****  
    ./build_wl18xx-dm.sh: line 104: cd: /home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel: No such file or directory
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/configuration/kernel_2.6.config': No such file or directory
    make: *** No rule to make target 'clean'.  Stop.
    ******  *******
    make: *** No rule to make target 'uImage'.  Stop.
    make: *** No rule to make target 'am335x-evm.dtb'.  Stop.
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel/arch/arm/boot/zImage': No such file or directory
    cp: cannot stat '/home/msmith/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites/src/kernel/arch/arm/boot/dts/am335x-evm.dtb': No such file or directory
    ****** ERROR 0 *******
    msmith@msmith-VirtualBox:~/qt/carbb-rdk-dm385/Source/ti_tools/wifi-driver-files-r8-4/build-utilites$

  • My current switch settings :

    #
    # Generated by Mark Smith to enable TI wl1835 sdio driver for wireless communication.
    # Linux/arm 2.6.37 Kernel Configuration
    # Tue Aug 15 09:35:19 2017
    #
    CONFIG_ARM=y
    # CONFIG_HAVE_PWM is not set
    CONFIG_SYS_SUPPORTS_APM_EMULATION=y
    CONFIG_GENERIC_GPIO=y
    # CONFIG_ARCH_USES_GETTIMEOFFSET is not set
    CONFIG_GENERIC_CLOCKEVENTS=y
    CONFIG_HAVE_PROC_CPU=y
    CONFIG_GENERIC_HARDIRQS=y
    CONFIG_STACKTRACE_SUPPORT=y
    CONFIG_HAVE_LATENCYTOP_SUPPORT=y
    CONFIG_LOCKDEP_SUPPORT=y
    CONFIG_TRACE_IRQFLAGS_SUPPORT=y
    CONFIG_HARDIRQS_SW_RESEND=y
    CONFIG_GENERIC_IRQ_PROBE=y
    CONFIG_RWSEM_GENERIC_SPINLOCK=y
    CONFIG_ARCH_HAS_CPUFREQ=y
    CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
    CONFIG_GENERIC_HWEIGHT=y
    CONFIG_GENERIC_CALIBRATE_DELAY=y
    CONFIG_NEED_DMA_MAP_STATE=y
    CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
    CONFIG_ARM_L1_CACHE_SHIFT_6=y
    CONFIG_VECTORS_BASE=0xffff0000
    CONFIG_ARM_PATCH_PHYS_VIRT=y
    CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
    CONFIG_CONSTRUCTORS=y
    CONFIG_HAVE_IRQ_WORK=y

    #
    # General setup
    #
    CONFIG_EXPERIMENTAL=y
    CONFIG_BROKEN_ON_SMP=y
    CONFIG_INIT_ENV_ARG_LIMIT=32
    CONFIG_CROSS_COMPILE=""
    CONFIG_LOCALVERSION="_DM385_CBB_1.50.50"
    CONFIG_LOCALVERSION_AUTO=y
    CONFIG_HAVE_KERNEL_GZIP=y
    CONFIG_HAVE_KERNEL_LZMA=y
    CONFIG_HAVE_KERNEL_LZO=y
    CONFIG_KERNEL_GZIP=y
    # CONFIG_KERNEL_LZMA is not set
    # CONFIG_KERNEL_LZO is not set
    # CONFIG_SWAP is not set
    CONFIG_SYSVIPC=y
    CONFIG_SYSVIPC_SYSCTL=y
    CONFIG_POSIX_MQUEUE=y
    CONFIG_POSIX_MQUEUE_SYSCTL=y
    CONFIG_BSD_PROCESS_ACCT=y
    # CONFIG_BSD_PROCESS_ACCT_V3 is not set
    # CONFIG_TASKSTATS is not set
    # CONFIG_AUDIT is not set
    # CONFIG_HAVE_GENERIC_HARDIRQS is not set
    # CONFIG_SPARSE_IRQ is not set

    #
    # RCU Subsystem
    #
    CONFIG_TINY_RCU=y
    # CONFIG_PREEMPT_RCU is not set
    # CONFIG_TREE_RCU_TRACE is not set
    CONFIG_IKCONFIG=y
    CONFIG_IKCONFIG_PROC=y
    CONFIG_LOG_BUF_SHIFT=17
    # CONFIG_CGROUPS is not set
    CONFIG_NAMESPACES=y
    # CONFIG_UTS_NS is not set
    # CONFIG_IPC_NS is not set
    # CONFIG_USER_NS is not set
    # CONFIG_PID_NS is not set
    # CONFIG_NET_NS is not set
    # CONFIG_SYSFS_DEPRECATED is not set
    # CONFIG_RELAY is not set
    CONFIG_BLK_DEV_INITRD=y
    CONFIG_INITRAMFS_SOURCE=""
    CONFIG_RD_GZIP=y
    CONFIG_RD_BZIP2=y
    CONFIG_RD_LZMA=y
    CONFIG_RD_LZO=y
    CONFIG_CC_OPTIMIZE_FOR_SIZE=y
    CONFIG_SYSCTL=y
    CONFIG_ANON_INODES=y
    # CONFIG_EMBEDDED is not set
    CONFIG_UID16=y
    CONFIG_SYSCTL_SYSCALL=y
    CONFIG_KALLSYMS=y
    # CONFIG_KALLSYMS_ALL is not set
    CONFIG_KALLSYMS_EXTRA_PASS=y
    CONFIG_HOTPLUG=y
    CONFIG_PRINTK=y
    CONFIG_BUG=y
    CONFIG_ELF_CORE=y
    CONFIG_BASE_FULL=y
    CONFIG_FUTEX=y
    CONFIG_EPOLL=y
    CONFIG_SIGNALFD=y
    CONFIG_TIMERFD=y
    CONFIG_EVENTFD=y
    CONFIG_SHMEM=y
    CONFIG_AIO=y
    CONFIG_HAVE_PERF_EVENTS=y
    CONFIG_PERF_USE_VMALLOC=y

    #
    # Kernel Performance Events And Counters
    #
    # CONFIG_PERF_EVENTS is not set
    # CONFIG_PERF_COUNTERS is not set
    CONFIG_VM_EVENT_COUNTERS=y
    CONFIG_SLUB_DEBUG=y
    CONFIG_COMPAT_BRK=y
    # CONFIG_SLAB is not set
    CONFIG_SLUB=y
    # CONFIG_PROFILING is not set
    CONFIG_HAVE_OPROFILE=y
    CONFIG_KPROBES=y
    CONFIG_KRETPROBES=y
    CONFIG_HAVE_KPROBES=y
    CONFIG_HAVE_KRETPROBES=y
    CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
    CONFIG_HAVE_CLK=y

    #
    # GCOV-based kernel profiling
    #
    # CONFIG_GCOV_KERNEL is not set
    CONFIG_HAVE_GENERIC_DMA_COHERENT=y
    CONFIG_SLABINFO=y
    CONFIG_RT_MUTEXES=y
    CONFIG_BASE_SMALL=0
    CONFIG_MODULES=y
    # CONFIG_MODULE_FORCE_LOAD is not set
    CONFIG_MODULE_UNLOAD=y
    # CONFIG_MODULE_FORCE_UNLOAD is not set
    CONFIG_MODVERSIONS=y
    # CONFIG_MODULE_SRCVERSION_ALL is not set
    CONFIG_BLOCK=y
    # CONFIG_LBDAF is not set
    # CONFIG_BLK_DEV_BSG is not set
    # CONFIG_BLK_DEV_INTEGRITY is not set

    #
    # IO Schedulers
    #
    CONFIG_IOSCHED_NOOP=y
    CONFIG_IOSCHED_DEADLINE=y
    CONFIG_IOSCHED_CFQ=y
    # CONFIG_DEFAULT_DEADLINE is not set
    CONFIG_DEFAULT_CFQ=y
    # CONFIG_DEFAULT_NOOP is not set
    CONFIG_DEFAULT_IOSCHED="cfq"

    #
    # sbull Driver
    #
    CONFIG_SBULL=m
    # CONFIG_INLINE_SPIN_TRYLOCK is not set
    # CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK is not set
    # CONFIG_INLINE_SPIN_LOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQ is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
    CONFIG_INLINE_SPIN_UNLOCK=y
    # CONFIG_INLINE_SPIN_UNLOCK_BH is not set
    CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
    # CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_READ_TRYLOCK is not set
    # CONFIG_INLINE_READ_LOCK is not set
    # CONFIG_INLINE_READ_LOCK_BH is not set
    # CONFIG_INLINE_READ_LOCK_IRQ is not set
    # CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
    CONFIG_INLINE_READ_UNLOCK=y
    # CONFIG_INLINE_READ_UNLOCK_BH is not set
    CONFIG_INLINE_READ_UNLOCK_IRQ=y
    # CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_WRITE_TRYLOCK is not set
    # CONFIG_INLINE_WRITE_LOCK is not set
    # CONFIG_INLINE_WRITE_LOCK_BH is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQ is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
    CONFIG_INLINE_WRITE_UNLOCK=y
    # CONFIG_INLINE_WRITE_UNLOCK_BH is not set
    CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
    # CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
    # CONFIG_MUTEX_SPIN_ON_OWNER is not set
    CONFIG_FREEZER=y

    #
    # System Type
    #
    CONFIG_MMU=y
    # CONFIG_ARCH_AAEC2000 is not set
    # CONFIG_ARCH_INTEGRATOR is not set
    # CONFIG_ARCH_REALVIEW is not set
    # CONFIG_ARCH_VERSATILE is not set
    # CONFIG_ARCH_VEXPRESS is not set
    # CONFIG_ARCH_AT91 is not set
    # CONFIG_ARCH_BCMRING is not set
    # CONFIG_ARCH_CLPS711X is not set
    # CONFIG_ARCH_CNS3XXX is not set
    # CONFIG_ARCH_GEMINI is not set
    # CONFIG_ARCH_EBSA110 is not set
    # CONFIG_ARCH_EP93XX is not set
    # CONFIG_ARCH_FOOTBRIDGE is not set
    # CONFIG_ARCH_MXC is not set
    # CONFIG_ARCH_STMP3XXX is not set
    # CONFIG_ARCH_NETX is not set
    # CONFIG_ARCH_H720X is not set
    # CONFIG_ARCH_IOP13XX is not set
    # CONFIG_ARCH_IOP32X is not set
    # CONFIG_ARCH_IOP33X is not set
    # CONFIG_ARCH_IXP23XX is not set
    # CONFIG_ARCH_IXP2000 is not set
    # CONFIG_ARCH_IXP4XX is not set
    # CONFIG_ARCH_DOVE is not set
    # CONFIG_ARCH_KIRKWOOD is not set
    # CONFIG_ARCH_LOKI is not set
    # CONFIG_ARCH_LPC32XX is not set
    # CONFIG_ARCH_MV78XX0 is not set
    # CONFIG_ARCH_ORION5X is not set
    # CONFIG_ARCH_MMP is not set
    # CONFIG_ARCH_KS8695 is not set
    # CONFIG_ARCH_NS9XXX is not set
    # CONFIG_ARCH_W90X900 is not set
    # CONFIG_ARCH_NUC93X is not set
    # CONFIG_ARCH_TEGRA is not set
    # CONFIG_ARCH_PNX4008 is not set
    # CONFIG_ARCH_PXA is not set
    # CONFIG_ARCH_MSM is not set
    # CONFIG_ARCH_SHMOBILE is not set
    # CONFIG_ARCH_RPC is not set
    # CONFIG_ARCH_SA1100 is not set
    # CONFIG_ARCH_S3C2410 is not set
    # CONFIG_ARCH_S3C64XX is not set
    # CONFIG_ARCH_S5P64X0 is not set
    # CONFIG_ARCH_S5P6442 is not set
    # CONFIG_ARCH_S5PC100 is not set
    # CONFIG_ARCH_S5PV210 is not set
    # CONFIG_ARCH_S5PV310 is not set
    # CONFIG_ARCH_SHARK is not set
    # CONFIG_ARCH_TCC_926 is not set
    # CONFIG_ARCH_LH7A40X is not set
    # CONFIG_ARCH_U300 is not set
    # CONFIG_ARCH_U8500 is not set
    # CONFIG_ARCH_NOMADIK is not set
    # CONFIG_ARCH_DAVINCI is not set
    CONFIG_ARCH_OMAP=y
    # CONFIG_PLAT_SPEAR is not set

    #
    # TI OMAP Common Features
    #
    # CONFIG_ARCH_OMAP1 is not set
    CONFIG_ARCH_OMAP2PLUS=y

    #
    # OMAP Feature Selections
    #
    # CONFIG_OMAP_RESET_CLOCKS is not set
    CONFIG_OMAP_MUX=y
    # CONFIG_OMAP_MUX_DEBUG is not set
    CONFIG_OMAP_MUX_WARNINGS=y
    # CONFIG_OMAP_MCBSP is not set
    CONFIG_OMAP_MBOX_FWK=y
    CONFIG_OMAP_MBOX_KFIFO_SIZE=256
    CONFIG_OMAP_IOMMU=y
    # CONFIG_OMAP_IOMMU_DEBUG is not set
    CONFIG_OMAP_MPU_TIMER=y
    # CONFIG_OMAP_32K_TIMER is not set
    CONFIG_OMAP_DM_TIMER=y
    # CONFIG_OMAP_PM_NONE is not set
    CONFIG_OMAP_PM_NOOP=y

    #
    # TI OMAP2/3/4 Specific Features
    #
    CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
    # CONFIG_ARCH_OMAP2 is not set
    # CONFIG_ARCH_OMAP3 is not set
    # CONFIG_ARCH_OMAP4 is not set
    CONFIG_ARCH_TI81XX=y
    # CONFIG_ARCH_TI816X is not set
    CONFIG_ARCH_TI814X=y

    #
    # OMAP Board Type
    #

    #
    # TI81XX Board Type
    #
    # CONFIG_MACH_TI8148IPNC is not set
    CONFIG_MACH_TI8148EVM=y
    # CONFIG_MACH_DM385EVM is not set
    # CONFIG_MACH_TI811XEVM is not set
    # CONFIG_MACH_DM385IPNC is not set
    CONFIG_MACH_DM385CBB=y
    # CONFIG_TI8148_EVM_OPTIMIZED is not set

    #
    # Processor Type
    #
    CONFIG_CPU_32v6K=y
    CONFIG_CPU_V7=y
    CONFIG_CPU_32v7=y
    CONFIG_CPU_ABRT_EV7=y
    CONFIG_CPU_PABRT_V7=y
    CONFIG_CPU_CACHE_V7=y
    CONFIG_CPU_CACHE_VIPT=y
    CONFIG_CPU_COPY_V6=y
    CONFIG_CPU_TLB_V7=y
    CONFIG_CPU_HAS_ASID=y
    CONFIG_CPU_CP15=y
    CONFIG_CPU_CP15_MMU=y

    #
    # Processor Features
    #
    CONFIG_ARM_THUMB=y
    # CONFIG_ARM_THUMBEE is not set
    # CONFIG_CPU_ICACHE_DISABLE is not set
    # CONFIG_CPU_DCACHE_DISABLE is not set
    # CONFIG_CPU_BPREDICT_DISABLE is not set
    CONFIG_ARM_L1_CACHE_SHIFT=6
    CONFIG_ARM_DMA_MEM_BUFFERABLE=y
    CONFIG_CPU_HAS_PMU=y
    # CONFIG_ARM_ERRATA_430973 is not set
    # CONFIG_ARM_ERRATA_458693 is not set
    # CONFIG_ARM_ERRATA_460075 is not set
    # CONFIG_ARM_ERRATA_743622 is not set
    CONFIG_COMMON_CLKDEV=y

    #
    # Bus support
    #
    # CONFIG_PCI is not set
    # CONFIG_PCI_SYSCALL is not set
    CONFIG_ARCH_SUPPORTS_MSI=y
    # CONFIG_PCCARD is not set

    #
    # Kernel Features
    #
    CONFIG_TICK_ONESHOT=y
    CONFIG_NO_HZ=y
    CONFIG_HIGH_RES_TIMERS=y
    CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
    CONFIG_VMSPLIT_3G=y
    # CONFIG_VMSPLIT_2G is not set
    # CONFIG_VMSPLIT_1G is not set
    CONFIG_PAGE_OFFSET=0xC0000000
    CONFIG_PREEMPT_NONE=y
    # CONFIG_PREEMPT_VOLUNTARY is not set
    # CONFIG_PREEMPT is not set
    CONFIG_HZ=100
    # CONFIG_THUMB2_KERNEL is not set
    CONFIG_AEABI=y
    CONFIG_OABI_COMPAT=y
    CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
    # CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
    # CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
    CONFIG_HIGHMEM=y
    # CONFIG_HIGHPTE is not set
    CONFIG_SELECT_MEMORY_MODEL=y
    CONFIG_FLATMEM_MANUAL=y
    CONFIG_FLATMEM=y
    CONFIG_FLAT_NODE_MEM_MAP=y
    CONFIG_HAVE_MEMBLOCK=y
    CONFIG_PAGEFLAGS_EXTENDED=y
    CONFIG_SPLIT_PTLOCK_CPUS=4
    # CONFIG_PHYS_ADDR_T_64BIT is not set
    CONFIG_ZONE_DMA_FLAG=0
    CONFIG_BOUNCE=y
    CONFIG_VIRT_TO_BUS=y
    # CONFIG_KSM is not set
    CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
    CONFIG_NEED_PER_CPU_KM=y
    CONFIG_FORCE_MAX_ZONEORDER=11
    # CONFIG_LEDS is not set
    CONFIG_ALIGNMENT_TRAP=y
    # CONFIG_UACCESS_WITH_MEMCPY is not set
    # CONFIG_SECCOMP is not set
    # CONFIG_CC_STACKPROTECTOR is not set
    # CONFIG_DEPRECATED_PARAM_STRUCT is not set

    #
    # Boot options
    #
    CONFIG_ZBOOT_ROM_TEXT=0
    CONFIG_ZBOOT_ROM_BSS=0
    CONFIG_CMDLINE=""
    # CONFIG_XIP_KERNEL is not set
    # CONFIG_KEXEC is not set
    CONFIG_AUTO_ZRELADDR=y

    #
    # CPU Power Management
    #
    # CONFIG_CPU_FREQ is not set
    # CONFIG_CPU_IDLE is not set

    #
    # Floating point emulation
    #

    #
    # At least one emulation must be selected
    #
    CONFIG_FPE_NWFPE=y
    # CONFIG_FPE_NWFPE_XP is not set
    # CONFIG_FPE_FASTFPE is not set
    CONFIG_VFP=y
    CONFIG_VFPv3=y
    CONFIG_NEON=y

    #
    # Userspace binary formats
    #
    CONFIG_BINFMT_ELF=y
    # CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
    CONFIG_HAVE_AOUT=y
    # CONFIG_BINFMT_AOUT is not set
    CONFIG_BINFMT_MISC=y

    #
    # Power management options
    #
    CONFIG_PM=y
    CONFIG_PM_DEBUG=y
    # CONFIG_PM_ADVANCED_DEBUG is not set
    CONFIG_PM_VERBOSE=y
    CONFIG_CAN_PM_TRACE=y
    CONFIG_PM_SLEEP=y
    CONFIG_SUSPEND_NVS=y
    CONFIG_SUSPEND=y
    # CONFIG_PM_TEST_SUSPEND is not set
    CONFIG_SUSPEND_FREEZER=y
    # CONFIG_APM_EMULATION is not set
    CONFIG_PM_RUNTIME=y
    CONFIG_PM_OPS=y
    # CONFIG_ARCH_HAS_OPP is not set
    CONFIG_ARCH_SUSPEND_POSSIBLE=y
    CONFIG_NET=y

    #
    # Networking options
    #
    CONFIG_PACKET=y
    CONFIG_UNIX=y
    CONFIG_XFRM=y
    # CONFIG_XFRM_USER is not set
    # CONFIG_XFRM_SUB_POLICY is not set
    # CONFIG_XFRM_MIGRATE is not set
    # CONFIG_XFRM_STATISTICS is not set
    # CONFIG_NET_KEY is not set
    CONFIG_INET=y
    CONFIG_IP_MULTICAST=y
    # CONFIG_IP_ADVANCED_ROUTER is not set
    CONFIG_IP_FIB_HASH=y
    CONFIG_IP_PNP=y
    CONFIG_IP_PNP_DHCP=y
    CONFIG_IP_PNP_BOOTP=y
    CONFIG_IP_PNP_RARP=y
    # CONFIG_NET_IPIP is not set
    # CONFIG_NET_IPGRE_DEMUX is not set
    # CONFIG_IP_MROUTE is not set
    # CONFIG_ARPD is not set
    # CONFIG_SYN_COOKIES is not set
    # CONFIG_INET_AH is not set
    # CONFIG_INET_ESP is not set
    # CONFIG_INET_IPCOMP is not set
    # CONFIG_INET_XFRM_TUNNEL is not set
    CONFIG_INET_TUNNEL=m
    CONFIG_INET_XFRM_MODE_TRANSPORT=y
    CONFIG_INET_XFRM_MODE_TUNNEL=y
    CONFIG_INET_XFRM_MODE_BEET=y
    CONFIG_INET_LRO=y
    CONFIG_INET_DIAG=y
    CONFIG_INET_TCP_DIAG=y
    # CONFIG_TCP_CONG_ADVANCED is not set
    CONFIG_TCP_CONG_CUBIC=y
    CONFIG_DEFAULT_TCP_CONG="cubic"
    # CONFIG_TCP_MD5SIG is not set
    CONFIG_IPV6=m
    # CONFIG_IPV6_PRIVACY is not set
    # CONFIG_IPV6_ROUTER_PREF is not set
    # CONFIG_IPV6_OPTIMISTIC_DAD is not set
    # CONFIG_INET6_AH is not set
    # CONFIG_INET6_ESP is not set
    # CONFIG_INET6_IPCOMP is not set
    # CONFIG_IPV6_MIP6 is not set
    # CONFIG_INET6_XFRM_TUNNEL is not set
    # CONFIG_INET6_TUNNEL is not set
    CONFIG_INET6_XFRM_MODE_TRANSPORT=m
    CONFIG_INET6_XFRM_MODE_TUNNEL=m
    CONFIG_INET6_XFRM_MODE_BEET=m
    # CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set
    CONFIG_IPV6_SIT=m
    # CONFIG_IPV6_SIT_6RD is not set
    CONFIG_IPV6_NDISC_NODETYPE=y
    # CONFIG_IPV6_TUNNEL is not set
    # CONFIG_IPV6_MULTIPLE_TABLES is not set
    # CONFIG_IPV6_MROUTE is not set
    # CONFIG_NETLABEL is not set
    # CONFIG_NETWORK_SECMARK is not set
    # CONFIG_NETWORK_PHY_TIMESTAMPING is not set
    # CONFIG_NETFILTER is not set
    # CONFIG_IP_DCCP is not set
    # CONFIG_IP_SCTP is not set
    # CONFIG_RDS is not set
    # CONFIG_TIPC is not set
    # CONFIG_ATM is not set
    # CONFIG_L2TP is not set
    # CONFIG_BRIDGE is not set
    # CONFIG_NET_DSA is not set
    # CONFIG_VLAN_8021Q is not set
    # CONFIG_DECNET is not set
    # CONFIG_LLC2 is not set
    # CONFIG_IPX is not set
    # CONFIG_ATALK is not set
    # CONFIG_X25 is not set
    # CONFIG_LAPB is not set
    # CONFIG_ECONET is not set
    # CONFIG_WAN_ROUTER is not set
    # CONFIG_PHONET is not set
    # CONFIG_IEEE802154 is not set
    # CONFIG_NET_SCHED is not set
    # CONFIG_DCB is not set
    CONFIG_DNS_RESOLVER=y

    #
    # Network testing
    #
    # CONFIG_NET_PKTGEN is not set
    # CONFIG_NET_TCPPROBE is not set
    # CONFIG_HAMRADIO is not set
    # CONFIG_CAN is not set
    # CONFIG_IRDA is not set
    # CONFIG_BT is not set
    # CONFIG_AF_RXRPC is not set
    CONFIG_WIRELESS=y
    CONFIG_WEXT_CORE=y
    CONFIG_WEXT_PROC=y
    CONFIG_CFG80211=m
    # CONFIG_NL80211_TESTMODE is not set
    # CONFIG_CFG80211_DEVELOPER_WARNINGS is not set
    # CONFIG_CFG80211_REG_DEBUG is not set
    CONFIG_CFG80211_DEFAULT_PS=y
    # CONFIG_CFG80211_DEBUGFS is not set
    # CONFIG_CFG80211_INTERNAL_REGDB is not set
    CONFIG_CFG80211_WEXT=y
    CONFIG_WIRELESS_EXT_SYSFS=y
    # CONFIG_LIB80211 is not set
    CONFIG_MAC80211=m
    CONFIG_MAC80211_HAS_RC=y
    CONFIG_MAC80211_RC_MINSTREL=y
    CONFIG_MAC80211_RC_MINSTREL_HT=y
    CONFIG_MAC80211_RC_DEFAULT_MINSTREL=y
    CONFIG_MAC80211_RC_DEFAULT="minstrel_ht"
    # CONFIG_MAC80211_MESH is not set
    # CONFIG_MAC80211_LEDS is not set
    # CONFIG_MAC80211_DEBUGFS is not set
    # CONFIG_MAC80211_DEBUG_MENU is not set
    # CONFIG_WIMAX is not set
    CONFIG_RFKILL=y
    # CONFIG_NET_9P is not set
    # CONFIG_CAIF is not set
    # CONFIG_CEPH_LIB is not set

    #
    # Device Drivers
    #

    #
    # Generic Driver Options
    #
    CONFIG_UEVENT_HELPER_PATH=""
    CONFIG_DEVTMPFS=y
    CONFIG_DEVTMPFS_MOUNT=y
    CONFIG_STANDALONE=y
    CONFIG_PREVENT_FIRMWARE_BUILD=y
    CONFIG_FW_LOADER=y
    CONFIG_FIRMWARE_IN_KERNEL=y
    CONFIG_EXTRA_FIRMWARE=""
    # CONFIG_DEBUG_DRIVER is not set
    # CONFIG_DEBUG_DEVRES is not set
    # CONFIG_SYS_HYPERVISOR is not set
    # CONFIG_CONNECTOR is not set
    CONFIG_MTD=y
    # CONFIG_MTD_DEBUG is not set
    # CONFIG_MTD_TESTS is not set
    CONFIG_MTD_CONCAT=y
    CONFIG_MTD_PARTITIONS=y
    # CONFIG_MTD_REDBOOT_PARTS is not set
    CONFIG_MTD_CMDLINE_PARTS=y
    # CONFIG_MTD_AFS_PARTS is not set
    # CONFIG_MTD_AR7_PARTS is not set

    #
    # User Modules And Translation Layers
    #
    CONFIG_MTD_CHAR=y
    CONFIG_MTD_BLKDEVS=y
    CONFIG_MTD_BLOCK=y
    # CONFIG_FTL is not set
    # CONFIG_NFTL is not set
    # CONFIG_INFTL is not set
    # CONFIG_RFD_FTL is not set
    # CONFIG_SSFDC is not set
    # CONFIG_SM_FTL is not set
    # CONFIG_MTD_OOPS is not set

    #
    # RAM/ROM/Flash chip drivers
    #
    # CONFIG_MTD_CFI is not set
    # CONFIG_MTD_JEDECPROBE is not set
    CONFIG_MTD_MAP_BANK_WIDTH_1=y
    CONFIG_MTD_MAP_BANK_WIDTH_2=y
    CONFIG_MTD_MAP_BANK_WIDTH_4=y
    # CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
    CONFIG_MTD_CFI_I1=y
    CONFIG_MTD_CFI_I2=y
    # CONFIG_MTD_CFI_I4 is not set
    # CONFIG_MTD_CFI_I8 is not set
    # CONFIG_MTD_RAM is not set
    # CONFIG_MTD_ROM is not set
    # CONFIG_MTD_ABSENT is not set

    #
    # Mapping drivers for chip access
    #
    # CONFIG_MTD_COMPLEX_MAPPINGS is not set
    # CONFIG_MTD_PLATRAM is not set

    #
    # Self-contained MTD device drivers
    #
    # CONFIG_MTD_DATAFLASH is not set
    # CONFIG_MTD_M25P80 is not set
    # CONFIG_MTD_SST25L is not set
    # CONFIG_MTD_SLRAM is not set
    # CONFIG_MTD_PHRAM is not set
    # CONFIG_MTD_MTDRAM is not set
    # CONFIG_MTD_BLOCK2MTD is not set

    #
    # Disk-On-Chip Device Drivers
    #
    # CONFIG_MTD_DOC2000 is not set
    # CONFIG_MTD_DOC2001 is not set
    # CONFIG_MTD_DOC2001PLUS is not set
    CONFIG_MTD_NAND_ECC=y
    # CONFIG_MTD_NAND_ECC_SMC is not set
    CONFIG_MTD_NAND=y
    # CONFIG_MTD_NAND_VERIFY_WRITE is not set
    # CONFIG_ECC_BCH8_OFF is not set
    # CONFIG_MTD_SM_COMMON is not set
    # CONFIG_MTD_NAND_MUSEUM_IDS is not set
    # CONFIG_MTD_NAND_GPIO is not set
    CONFIG_MTD_NAND_OMAP2=y
    # CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW is not set
    CONFIG_MTD_NAND_OMAP_ECC_BCH8_CODE_HW=y
    # CONFIG_MTD_NAND_OMAP_ECC_BCH4_CODE_HW is not set
    # CONFIG_MTD_NAND_OMAP_ECC_HAMMING_CODE_HW is not set
    # CONFIG_MTD_NAND_OMAP_ECC_HAMMING_CODE_SW is not set
    CONFIG_MTD_NAND_IDS=y
    # CONFIG_MTD_NAND_DISKONCHIP is not set
    # CONFIG_MTD_NAND_NANDSIM is not set
    # CONFIG_MTD_NAND_PLATFORM is not set
    # CONFIG_MTD_ONENAND is not set

    #
    # LPDDR flash memory drivers
    #
    # CONFIG_MTD_LPDDR is not set
    CONFIG_MTD_UBI=y
    CONFIG_MTD_UBI_WL_THRESHOLD=4096
    CONFIG_MTD_UBI_BEB_RESERVE=1
    # CONFIG_MTD_UBI_GLUEBI is not set
    # CONFIG_MTD_UBI_DEBUG is not set
    # CONFIG_PARPORT is not set
    CONFIG_BLK_DEV=y
    # CONFIG_BLK_DEV_COW_COMMON is not set
    CONFIG_BLK_DEV_LOOP=y
    # CONFIG_BLK_DEV_CRYPTOLOOP is not set

    #
    # DRBD disabled because PROC_FS, INET or CONNECTOR not selected
    #
    # CONFIG_BLK_DEV_NBD is not set
    CONFIG_BLK_DEV_RAM=y
    CONFIG_BLK_DEV_RAM_COUNT=16
    CONFIG_BLK_DEV_RAM_SIZE=32768
    # CONFIG_BLK_DEV_XIP is not set
    # CONFIG_CDROM_PKTCDVD is not set
    # CONFIG_ATA_OVER_ETH is not set
    # CONFIG_MG_DISK is not set
    # CONFIG_BLK_DEV_RBD is not set
    # CONFIG_MISC_DEVICES is not set
    CONFIG_HAVE_IDE=y
    # CONFIG_IDE is not set

    #
    # SCSI device support
    #
    CONFIG_SCSI_MOD=y
    # CONFIG_RAID_ATTRS is not set
    CONFIG_SCSI=y
    CONFIG_SCSI_DMA=y
    # CONFIG_SCSI_TGT is not set
    # CONFIG_SCSI_NETLINK is not set
    CONFIG_SCSI_PROC_FS=y

    #
    # SCSI support type (disk, tape, CD-ROM)
    #
    CONFIG_BLK_DEV_SD=y
    # CONFIG_CHR_DEV_ST is not set
    # CONFIG_CHR_DEV_OSST is not set
    # CONFIG_BLK_DEV_SR is not set
    CONFIG_CHR_DEV_SG=y
    # CONFIG_CHR_DEV_SCH is not set
    # CONFIG_SCSI_MULTI_LUN is not set
    # CONFIG_SCSI_CONSTANTS is not set
    # CONFIG_SCSI_LOGGING is not set
    # CONFIG_SCSI_SCAN_ASYNC is not set
    CONFIG_SCSI_WAIT_SCAN=m

    #
    # SCSI Transports
    #
    # CONFIG_SCSI_SPI_ATTRS is not set
    # CONFIG_SCSI_FC_ATTRS is not set
    # CONFIG_SCSI_ISCSI_ATTRS is not set
    # CONFIG_SCSI_SAS_ATTRS is not set
    # CONFIG_SCSI_SAS_LIBSAS is not set
    # CONFIG_SCSI_SRP_ATTRS is not set
    # CONFIG_SCSI_LOWLEVEL is not set
    # CONFIG_SCSI_DH is not set
    # CONFIG_SCSI_OSD_INITIATOR is not set
    # CONFIG_ATA is not set
    # CONFIG_MD is not set
    CONFIG_NETDEVICES=y
    # CONFIG_DUMMY is not set
    # CONFIG_BONDING is not set
    # CONFIG_MACVLAN is not set
    # CONFIG_EQUALIZER is not set
    # CONFIG_TUN is not set
    # CONFIG_VETH is not set
    CONFIG_MII=y
    CONFIG_PHYLIB=y

    #
    # MII PHY device drivers
    #
    # CONFIG_MARVELL_PHY is not set
    # CONFIG_DAVICOM_PHY is not set
    # CONFIG_QSEMI_PHY is not set
    # CONFIG_LXT_PHY is not set
    # CONFIG_CICADA_PHY is not set
    # CONFIG_VITESSE_PHY is not set
    # CONFIG_SMSC_PHY is not set
    # CONFIG_BROADCOM_PHY is not set
    # CONFIG_BCM63XX_PHY is not set
    # CONFIG_ICPLUS_PHY is not set
    # CONFIG_REALTEK_PHY is not set
    # CONFIG_NATIONAL_PHY is not set
    # CONFIG_STE10XP is not set
    # CONFIG_LSI_ET1011C_PHY is not set
    # CONFIG_MICREL_PHY is not set
    # CONFIG_FIXED_PHY is not set
    # CONFIG_MDIO_BITBANG is not set
    # CONFIG_NET_ETHERNET is not set
    CONFIG_NETDEV_1000=y
    CONFIG_TI_DAVINCI_MDIO=y
    CONFIG_TI_DAVINCI_CPDMA=y
    CONFIG_TI_CPSW=y
    # CONFIG_TI_CPSW_DUAL_EMAC is not set
    # CONFIG_STMMAC_ETH is not set
    # CONFIG_NETDEV_10000 is not set
    CONFIG_WLAN=y
    # CONFIG_LIBERTAS_THINFIRM is not set
    # CONFIG_MAC80211_HWSIM is not set
    # CONFIG_ATH_COMMON is not set
    # CONFIG_B43 is not set
    # CONFIG_B43LEGACY is not set
    # CONFIG_HOSTAP is not set
    # CONFIG_IWM is not set
    # CONFIG_LIBERTAS is not set
    # CONFIG_P54_COMMON is not set
    # CONFIG_RT2X00 is not set

    CONFIG_WL_TI=y
    CONFIG_WL12XX=m
    CONFIG_WL18XX=m
    CONFIG_WLCORE=m
    # CONFIG_WLCORE_SPI is not set
    CONFIG_WLCORE_SDIO=m
    CONFIG_WILINK_PLATFORM_DATA=y

    #
    # Enable WiMAX (Networking options) to see the WiMAX drivers
    #
    # CONFIG_WAN is not set

    #
    # CAIF transport drivers
    #
    # CONFIG_PPP is not set
    # CONFIG_SLIP is not set
    # CONFIG_NETCONSOLE is not set
    # CONFIG_NETPOLL is not set
    # CONFIG_NET_POLL_CONTROLLER is not set
    # CONFIG_ISDN is not set
    # CONFIG_PHONE is not set

    #
    # Input device support
    #
    CONFIG_INPUT=y
    # CONFIG_INPUT_FF_MEMLESS is not set
    # CONFIG_INPUT_POLLDEV is not set
    # CONFIG_INPUT_SPARSEKMAP is not set

    #
    # Userland interfaces
    #
    CONFIG_INPUT_MOUSEDEV=y
    # CONFIG_INPUT_MOUSEDEV_PSAUX is not set
    CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
    CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
    # CONFIG_INPUT_JOYDEV is not set
    CONFIG_INPUT_EVDEV=y
    # CONFIG_INPUT_EVBUG is not set

    #
    # Input Device Drivers
    #
    # CONFIG_INPUT_KEYBOARD is not set
    # CONFIG_INPUT_MOUSE is not set
    # CONFIG_INPUT_JOYSTICK is not set
    # CONFIG_INPUT_TABLET is not set
    CONFIG_INPUT_TOUCHSCREEN=y
    # CONFIG_TOUCHSCREEN_ADS7846 is not set
    # CONFIG_TOUCHSCREEN_AD7877 is not set
    # CONFIG_TOUCHSCREEN_AD7879 is not set
    # CONFIG_TOUCHSCREEN_BU21013 is not set
    # CONFIG_TOUCHSCREEN_CY8CTMG110 is not set
    # CONFIG_TOUCHSCREEN_DYNAPRO is not set
    # CONFIG_TOUCHSCREEN_HAMPSHIRE is not set
    # CONFIG_TOUCHSCREEN_EETI is not set
    # CONFIG_TOUCHSCREEN_FUJITSU is not set
    # CONFIG_TOUCHSCREEN_GUNZE is not set
    # CONFIG_TOUCHSCREEN_ELO is not set
    # CONFIG_TOUCHSCREEN_WACOM_W8001 is not set
    # CONFIG_TOUCHSCREEN_MCS5000 is not set
    # CONFIG_TOUCHSCREEN_MTOUCH is not set
    # CONFIG_TOUCHSCREEN_INEXIO is not set
    # CONFIG_TOUCHSCREEN_MK712 is not set
    # CONFIG_TOUCHSCREEN_PENMOUNT is not set
    # CONFIG_TOUCHSCREEN_QT602240 is not set
    # CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set
    # CONFIG_TOUCHSCREEN_TOUCHWIN is not set
    # CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set
    # CONFIG_TOUCHSCREEN_TOUCHIT213 is not set
    # CONFIG_TOUCHSCREEN_TSC2007 is not set
    CONFIG_TOUCHSCREEN_TSC2004=y
    # CONFIG_TOUCHSCREEN_W90X900 is not set
    # CONFIG_TOUCHSCREEN_TPS6507X is not set
    CONFIG_INPUT_MISC=y
    # CONFIG_INPUT_AD714X is not set
    # CONFIG_INPUT_ATI_REMOTE is not set
    # CONFIG_INPUT_ATI_REMOTE2 is not set
    # CONFIG_INPUT_KEYSPAN_REMOTE is not set
    # CONFIG_INPUT_POWERMATE is not set
    # CONFIG_INPUT_YEALINK is not set
    # CONFIG_INPUT_CM109 is not set
    # CONFIG_INPUT_UINPUT is not set
    # CONFIG_INPUT_PCF8574 is not set
    # CONFIG_INPUT_GPIO_ROTARY_ENCODER is not set
    # CONFIG_INPUT_ADXL34X is not set
    CONFIG_INPUT_BMA250=y
    CONFIG_INPUT_ISL29023=y
    CONFIG_INPUT_MCU_BRIDGE=y

    #
    # Hardware I/O ports
    #
    CONFIG_SERIO=y
    CONFIG_SERIO_SERPORT=y
    # CONFIG_SERIO_RAW is not set
    # CONFIG_SERIO_ALTERA_PS2 is not set
    # CONFIG_SERIO_PS2MULT is not set
    # CONFIG_GAMEPORT is not set

    #
    # Character devices
    #
    CONFIG_VT=y
    CONFIG_CONSOLE_TRANSLATIONS=y
    CONFIG_VT_CONSOLE=y
    CONFIG_HW_CONSOLE=y
    # CONFIG_VT_HW_CONSOLE_BINDING is not set
    CONFIG_DEVKMEM=y
    CONFIG_SERIAL_NONSTANDARD=y
    # CONFIG_N_HDLC is not set
    # CONFIG_N_GSM is not set
    # CONFIG_RISCOM8 is not set
    # CONFIG_SPECIALIX is not set
    # CONFIG_STALDRV is not set

    #
    # Serial drivers
    #
    CONFIG_SERIAL_8250=y
    CONFIG_SERIAL_8250_CONSOLE=y
    CONFIG_SERIAL_8250_NR_UARTS=64
    CONFIG_SERIAL_8250_RUNTIME_UARTS=4
    CONFIG_SERIAL_8250_EXTENDED=y
    # CONFIG_SERIAL_8250_MANY_PORTS is not set
    CONFIG_SERIAL_8250_SHARE_IRQ=y
    CONFIG_SERIAL_8250_DETECT_IRQ=y
    CONFIG_SERIAL_8250_RSA=y

    #
    # Non-8250 serial port support
    #
    # CONFIG_SERIAL_MAX3100 is not set
    # CONFIG_SERIAL_MAX3107 is not set
    CONFIG_SERIAL_CORE=y
    CONFIG_SERIAL_CORE_CONSOLE=y
    CONFIG_SERIAL_OMAP=y
    CONFIG_SERIAL_OMAP_CONSOLE=y
    # CONFIG_SERIAL_TIMBERDALE is not set
    # CONFIG_SERIAL_ALTERA_JTAGUART is not set
    # CONFIG_SERIAL_ALTERA_UART is not set
    CONFIG_UNIX98_PTYS=y
    # CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
    # CONFIG_LEGACY_PTYS is not set
    # CONFIG_IPMI_HANDLER is not set
    # CONFIG_HW_RANDOM is not set
    # CONFIG_R3964 is not set
    # CONFIG_RAW_DRIVER is not set
    # CONFIG_TCG_TPM is not set
    # CONFIG_TI81XX_PCIE_EPDRV is not set
    # CONFIG_RAMOOPS is not set
    CONFIG_I2C=y
    CONFIG_I2C_BOARDINFO=y
    CONFIG_I2C_COMPAT=y
    CONFIG_I2C_CHARDEV=y
    # CONFIG_I2C_MUX is not set
    CONFIG_I2C_HELPER_AUTO=y

    #
    # I2C Hardware Bus support
    #

    #
    # I2C system bus drivers (mostly embedded / system-on-chip)
    #
    # CONFIG_I2C_DESIGNWARE is not set
    # CONFIG_I2C_GPIO is not set
    # CONFIG_I2C_OCORES is not set
    CONFIG_I2C_OMAP=y
    # CONFIG_I2C_PCA_PLATFORM is not set
    # CONFIG_I2C_SIMTEC is not set
    # CONFIG_I2C_XILINX is not set

    #
    # External I2C/SMBus adapter drivers
    #
    # CONFIG_I2C_PARPORT_LIGHT is not set
    # CONFIG_I2C_TAOS_EVM is not set

    #
    # Other I2C/SMBus bus drivers
    #
    # CONFIG_I2C_STUB is not set
    # CONFIG_I2C_DEBUG_CORE is not set
    # CONFIG_I2C_DEBUG_ALGO is not set
    # CONFIG_I2C_DEBUG_BUS is not set
    CONFIG_SPI=y
    # CONFIG_SPI_DEBUG is not set
    CONFIG_SPI_MASTER=y

    #
    # SPI Master Controller Drivers
    #
    # CONFIG_SPI_BITBANG is not set
    # CONFIG_SPI_GPIO is not set
    CONFIG_SPI_OMAP24XX=y
    # CONFIG_SPI_XILINX is not set
    # CONFIG_SPI_DESIGNWARE is not set

    #
    # SPI Protocol Masters
    #
    # CONFIG_SPI_SPIDEV is not set
    # CONFIG_SPI_TLE62X0 is not set

    #
    # PPS support
    #
    # CONFIG_PPS is not set

    #
    # PTP clock support
    #

    #
    # Enable Device Drivers -> PPS to see the PTP clock options.
    #
    CONFIG_ARCH_REQUIRE_GPIOLIB=y
    CONFIG_GPIOLIB=y
    # CONFIG_DEBUG_GPIO is not set
    CONFIG_GPIO_SYSFS=y

    #
    # Memory mapped GPIO expanders:
    #
    # CONFIG_GPIO_BASIC_MMIO is not set
    # CONFIG_GPIO_IT8761E is not set
    # CONFIG_GPIO_VX855 is not set

    #
    # I2C GPIO expanders:
    #
    # CONFIG_GPIO_MAX7300 is not set
    # CONFIG_GPIO_MAX732X is not set
    # CONFIG_GPIO_PCA953X is not set
    # CONFIG_GPIO_PCF857X is not set
    # CONFIG_GPIO_SX150X is not set
    # CONFIG_GPIO_ADP5588 is not set

    #
    # PCI GPIO expanders:
    #

    #
    # SPI GPIO expanders:
    #
    # CONFIG_GPIO_MAX7301 is not set
    # CONFIG_GPIO_MCP23S08 is not set
    # CONFIG_GPIO_MC33880 is not set
    # CONFIG_GPIO_74X164 is not set

    #
    # AC97 GPIO expanders:
    #

    #
    # MODULbus GPIO expanders:
    #
    # CONFIG_W1 is not set
    # CONFIG_POWER_SUPPLY is not set
    # CONFIG_HWMON is not set
    # CONFIG_THERMAL is not set
    CONFIG_WATCHDOG=y
    # CONFIG_WATCHDOG_NOWAYOUT is not set

    #
    # Watchdog Device Drivers
    #
    # CONFIG_SOFT_WATCHDOG is not set
    CONFIG_OMAP_WATCHDOG=y
    # CONFIG_MAX63XX_WATCHDOG is not set
    CONFIG_SSB_POSSIBLE=y

    #
    # Sonics Silicon Backplane
    #
    CONFIG_SSB=m
    CONFIG_SSB_SDIOHOST_POSSIBLE=y
    # CONFIG_SSB_SDIOHOST is not set
    # CONFIG_SSB_DEBUG is not set
    CONFIG_MFD_SUPPORT=y
    # CONFIG_MFD_CORE is not set
    # CONFIG_MFD_88PM860X is not set
    # CONFIG_MFD_SM501 is not set
    # CONFIG_MFD_ASIC3 is not set
    # CONFIG_HTC_EGPIO is not set
    # CONFIG_HTC_PASIC3 is not set
    # CONFIG_HTC_I2CPLD is not set
    # CONFIG_TPS65010 is not set
    # CONFIG_TPS6507X is not set
    # CONFIG_MFD_STMPE is not set
    # CONFIG_MFD_TC35892 is not set
    # CONFIG_MFD_TMIO is not set
    # CONFIG_MFD_T7L66XB is not set
    # CONFIG_MFD_TC6387XB is not set
    # CONFIG_MFD_TC6393XB is not set
    # CONFIG_PMIC_DA903X is not set
    # CONFIG_PMIC_ADP5520 is not set
    # CONFIG_MFD_MAX8925 is not set
    # CONFIG_MFD_MAX8998 is not set
    # CONFIG_MFD_WM8400 is not set
    # CONFIG_MFD_WM831X_I2C is not set
    # CONFIG_MFD_WM831X_SPI is not set
    # CONFIG_MFD_WM8350_I2C is not set
    # CONFIG_MFD_WM8994 is not set
    # CONFIG_MFD_PCF50633 is not set
    # CONFIG_MFD_MC13XXX is not set
    # CONFIG_ABX500_CORE is not set
    # CONFIG_EZX_PCAP is not set
    # CONFIG_MFD_TPS6586X is not set
    # CONFIG_MFD_TPS65910 is not set
    CONFIG_REGULATOR=y
    # CONFIG_REGULATOR_DEBUG is not set
    # CONFIG_REGULATOR_DUMMY is not set
    CONFIG_REGULATOR_FIXED_VOLTAGE=y
    # CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
    # CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
    # CONFIG_REGULATOR_BQ24022 is not set
    # CONFIG_REGULATOR_MAX1586 is not set
    # CONFIG_REGULATOR_MAX8649 is not set
    # CONFIG_REGULATOR_MAX8660 is not set
    # CONFIG_REGULATOR_MAX8952 is not set
    # CONFIG_REGULATOR_LP3971 is not set
    # CONFIG_REGULATOR_LP3972 is not set
    # CONFIG_REGULATOR_TPS65023 is not set
    # CONFIG_REGULATOR_TPS6507X is not set
    # CONFIG_REGULATOR_ISL6271A is not set
    # CONFIG_REGULATOR_AD5398 is not set
    CONFIG_MEDIA_SUPPORT=y

    #
    # Multimedia core support
    #
    # CONFIG_MEDIA_CONTROLLER is not set
    CONFIG_VIDEO_DEV=y
    CONFIG_VIDEO_V4L2_COMMON=y
    CONFIG_VIDEO_ALLOW_V4L1=y
    CONFIG_VIDEO_V4L1_COMPAT=y
    # CONFIG_DVB_CORE is not set
    CONFIG_VIDEO_MEDIA=y

    #
    # Multimedia drivers
    #
    # CONFIG_IR_CORE is not set
    # CONFIG_MEDIA_ATTACH is not set
    CONFIG_MEDIA_TUNER=y
    # CONFIG_MEDIA_TUNER_CUSTOMISE is not set
    CONFIG_MEDIA_TUNER_SIMPLE=y
    CONFIG_MEDIA_TUNER_TDA8290=y
    CONFIG_MEDIA_TUNER_TDA827X=y
    CONFIG_MEDIA_TUNER_TDA18271=y
    CONFIG_MEDIA_TUNER_TDA9887=y
    CONFIG_MEDIA_TUNER_TEA5761=y
    CONFIG_MEDIA_TUNER_TEA5767=y
    CONFIG_MEDIA_TUNER_MT20XX=y
    CONFIG_MEDIA_TUNER_XC2028=y
    CONFIG_MEDIA_TUNER_XC5000=y
    CONFIG_MEDIA_TUNER_MC44S803=y
    CONFIG_VIDEO_V4L2=y
    CONFIG_VIDEO_V4L1=y
    CONFIG_VIDEOBUF_GEN=y
    CONFIG_VIDEOBUF_DMA_SG=y
    CONFIG_VIDEOBUF_DMA_CONTIG=y
    CONFIG_VIDEO_CAPTURE_DRIVERS=y
    # CONFIG_VIDEO_ADV_DEBUG is not set
    # CONFIG_VIDEO_FIXED_MINOR_RANGES is not set
    # CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set

    #
    # Encoders/decoders and other helper chips
    #

    #
    # Audio decoders
    #
    # CONFIG_VIDEO_TVAUDIO is not set
    # CONFIG_VIDEO_TDA7432 is not set
    # CONFIG_VIDEO_TDA9840 is not set
    # CONFIG_VIDEO_TDA9875 is not set
    # CONFIG_VIDEO_TEA6415C is not set
    # CONFIG_VIDEO_TEA6420 is not set
    # CONFIG_VIDEO_MSP3400 is not set
    # CONFIG_VIDEO_CS5345 is not set
    # CONFIG_VIDEO_CS53L32A is not set
    # CONFIG_VIDEO_M52790 is not set
    # CONFIG_VIDEO_TLV320AIC23B is not set
    # CONFIG_VIDEO_WM8775 is not set
    # CONFIG_VIDEO_WM8739 is not set
    # CONFIG_VIDEO_VP27SMPX is not set

    #
    # RDS decoders
    #
    # CONFIG_VIDEO_SAA6588 is not set

    #
    # Video decoders
    #
    # CONFIG_VIDEO_ADV7180 is not set
    # CONFIG_VIDEO_BT819 is not set
    # CONFIG_VIDEO_BT856 is not set
    # CONFIG_VIDEO_BT866 is not set
    # CONFIG_VIDEO_KS0127 is not set
    # CONFIG_VIDEO_OV7670 is not set
    # CONFIG_VIDEO_MT9T001 is not set
    # CONFIG_VIDEO_MT9V011 is not set
    # CONFIG_VIDEO_MT9V113 is not set
    # CONFIG_VIDEO_MT9T111 is not set
    # CONFIG_VIDEO_TCM825X is not set
    # CONFIG_VIDEO_SAA7110 is not set
    # CONFIG_VIDEO_SAA711X is not set
    # CONFIG_VIDEO_SAA717X is not set
    # CONFIG_VIDEO_SAA7191 is not set
    # CONFIG_VIDEO_TVP514X is not set
    # CONFIG_VIDEO_TVP5150 is not set
    # CONFIG_VIDEO_TVP7002 is not set
    # CONFIG_VIDEO_VPX3220 is not set

    #
    # Video and audio decoders
    #
    # CONFIG_VIDEO_CX25840 is not set

    #
    # MPEG video encoders
    #
    # CONFIG_VIDEO_CX2341X is not set

    #
    # Video encoders
    #
    # CONFIG_VIDEO_SAA7127 is not set
    # CONFIG_VIDEO_SAA7185 is not set
    # CONFIG_VIDEO_ADV7170 is not set
    # CONFIG_VIDEO_ADV7175 is not set
    # CONFIG_VIDEO_THS7303 is not set
    # CONFIG_VIDEO_ADV7343 is not set
    # CONFIG_VIDEO_AK881X is not set

    #
    # Video improvement chips
    #
    # CONFIG_VIDEO_UPD64031A is not set
    # CONFIG_VIDEO_UPD64083 is not set
    CONFIG_VIDEO_TI81XX_VIDOUT=m
    # CONFIG_VIDEO_TI81XX_VIDIN is not set
    # CONFIG_VIDEO_SR030PC30 is not set
    # CONFIG_SOC_CAMERA is not set
    # CONFIG_V4L_MEM2MEM_DRIVERS is not set
    # CONFIG_RADIO_ADAPTERS is not set
    # CONFIG_DAB is not set
    CONFIG_HAVE_TI_TILER=y
    # CONFIG_TI_TILER is not set

    #
    # Graphics support
    #
    # CONFIG_DRM is not set
    # CONFIG_VGASTATE is not set
    CONFIG_VIDEO_OUTPUT_CONTROL=y
    CONFIG_FB=y
    # CONFIG_FIRMWARE_EDID is not set
    # CONFIG_FB_DDC is not set
    # CONFIG_FB_BOOT_VESA_SUPPORT is not set
    CONFIG_FB_CFB_FILLRECT=y
    CONFIG_FB_CFB_COPYAREA=y
    CONFIG_FB_CFB_IMAGEBLIT=y
    # CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
    # CONFIG_FB_SYS_FILLRECT is not set
    # CONFIG_FB_SYS_COPYAREA is not set
    # CONFIG_FB_SYS_IMAGEBLIT is not set
    # CONFIG_FB_FOREIGN_ENDIAN is not set
    # CONFIG_FB_SYS_FOPS is not set
    # CONFIG_FB_SVGALIB is not set
    # CONFIG_FB_MACMODES is not set
    # CONFIG_FB_BACKLIGHT is not set
    # CONFIG_FB_MODE_HELPERS is not set
    # CONFIG_FB_TILEBLITTING is not set

    #
    # Frame buffer hardware drivers
    #
    # CONFIG_FB_S1D13XXX is not set
    # CONFIG_FB_VIRTUAL is not set
    # CONFIG_FB_METRONOME is not set
    # CONFIG_FB_MB862XX is not set
    # CONFIG_FB_BROADSHEET is not set
    CONFIG_TI81XX_VPSS=m
    CONFIG_TI81XX_VPSS_VRAM_SIZE=4
    CONFIG_TI81XX_VPSS_DEBUG_SUPPORT=y
    CONFIG_FB_TI81XX=m
    CONFIG_FB_TI81XX_DEBUG_SUPPORT=y
    CONFIG_FB_TI81XX_NUM_FBS=3
    CONFIG_TI81XX_HDMI=m
    # CONFIG_TI81XX_HDMI_HDCP is not set
    # CONFIG_SII9022a is not set
    # CONFIG_BACKLIGHT_LCD_SUPPORT is not set

    #
    # Display device support
    #
    # CONFIG_DISPLAY_SUPPORT is not set

    #
    # Console display driver support
    #
    CONFIG_DUMMY_CONSOLE=y
    # CONFIG_FRAMEBUFFER_CONSOLE is not set
    # CONFIG_LOGO is not set
    CONFIG_SOUND=y
    # CONFIG_SOUND_OSS_CORE is not set
    CONFIG_SND=y
    CONFIG_SND_TIMER=y
    CONFIG_SND_PCM=y
    CONFIG_SND_JACK=y
    # CONFIG_SND_SEQUENCER is not set
    # CONFIG_SND_MIXER_OSS is not set
    # CONFIG_SND_PCM_OSS is not set
    # CONFIG_SND_HRTIMER is not set
    # CONFIG_SND_DYNAMIC_MINORS is not set
    CONFIG_SND_SUPPORT_OLD_API=y
    CONFIG_SND_VERBOSE_PROCFS=y
    # CONFIG_SND_VERBOSE_PRINTK is not set
    # CONFIG_SND_DEBUG is not set
    # CONFIG_SND_RAWMIDI_SEQ is not set
    # CONFIG_SND_OPL3_LIB_SEQ is not set
    # CONFIG_SND_OPL4_LIB_SEQ is not set
    # CONFIG_SND_SBAWE_SEQ is not set
    # CONFIG_SND_EMU10K1_SEQ is not set
    # CONFIG_SND_DRIVERS is not set
    # CONFIG_SND_ARM is not set
    # CONFIG_SND_SPI is not set
    CONFIG_SND_SOC=y
    CONFIG_SND_TI81XX_SOC=y
    CONFIG_SND_DAVINCI_SOC_MCASP=y
    CONFIG_SND_TI81XX_SOC_EVM=y
    # CONFIG_SND_SOC_TI81XX_HDMI is not set
    # CONFIG_SND_OMAP_SOC is not set
    CONFIG_SND_SOC_I2C_AND_SPI=y
    # CONFIG_SND_SOC_ALL_CODECS is not set
    CONFIG_SND_SOC_TLV320AIC3110=y
    # CONFIG_SOUND_PRIME is not set
    # CONFIG_HID_SUPPORT is not set
    CONFIG_USB_SUPPORT=y
    CONFIG_USB_ARCH_HAS_HCD=y
    CONFIG_USB_ARCH_HAS_OHCI=y
    # CONFIG_USB_ARCH_HAS_EHCI is not set
    # CONFIG_USB is not set
    CONFIG_USB_MUSB_HDRC=y

    #
    # Platform Glue Layer
    #
    # CONFIG_USB_MUSB_TUSB6010_GLUE is not set
    # CONFIG_USB_MUSB_OMAP2PLUS_GLUE is not set
    # CONFIG_USB_MUSB_AM35X_GLUE is not set
    CONFIG_USB_MUSB_TI81XX_GLUE=y
    # CONFIG_USB_MUSB_DAVINCI is not set
    # CONFIG_USB_MUSB_DA8XX is not set
    # CONFIG_USB_MUSB_TUSB6010 is not set
    # CONFIG_USB_MUSB_OMAP2PLUS is not set
    # CONFIG_USB_MUSB_AM35X is not set
    CONFIG_USB_MUSB_TI81XX=y
    # CONFIG_USB_MUSB_BLACKFIN is not set
    # CONFIG_USB_MUSB_UX500 is not set
    CONFIG_USB_TI81XX_USBID_CTRL_SW=y
    # CONFIG_USB_TI81XX_USBID_CTRL_HW is not set
    CONFIG_USB_MUSB_PERIPHERAL=y
    CONFIG_USB_GADGET_MUSB_HDRC=y
    # CONFIG_MUSB_PIO_ONLY is not set
    # CONFIG_USB_INVENTRA_DMA_HW is not set
    # CONFIG_USB_TI_CPPI_DMA_HW is not set
    CONFIG_USB_TI_CPPI41_DMA_HW=y
    # CONFIG_USB_INVENTRA_DMA is not set
    # CONFIG_USB_TI_CPPI_DMA is not set
    CONFIG_USB_TI_CPPI41_DMA=y
    # CONFIG_USB_TUSB_OMAP_DMA is not set
    CONFIG_USB_MUSB_DEBUG=y

    #
    # NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
    #
    CONFIG_USB_GADGET=y
    # CONFIG_USB_GADGET_DEBUG is not set
    # CONFIG_USB_GADGET_DEBUG_FILES is not set
    # CONFIG_USB_GADGET_DEBUG_FS is not set
    CONFIG_USB_GADGET_VBUS_DRAW=2
    CONFIG_USB_GADGET_SELECTED=y
    # CONFIG_USB_GADGET_OMAP is not set
    # CONFIG_USB_GADGET_R8A66597 is not set
    # CONFIG_USB_GADGET_M66592 is not set
    CONFIG_USB_GADGET_DUALSPEED=y
    # CONFIG_USB_ZERO is not set
    # CONFIG_USB_AUDIO is not set
    # CONFIG_USB_ETH is not set
    # CONFIG_USB_GADGETFS is not set
    # CONFIG_USB_FUNCTIONFS is not set
    CONFIG_USB_FILE_STORAGE=m
    CONFIG_USB_FILE_STORAGE_TEST=y
    # CONFIG_USB_MASS_STORAGE is not set
    # CONFIG_USB_G_SERIAL is not set
    # CONFIG_USB_MIDI_GADGET is not set
    # CONFIG_USB_G_PRINTER is not set
    # CONFIG_USB_CDC_COMPOSITE is not set
    # CONFIG_USB_G_MULTI is not set
    # CONFIG_USB_G_HID is not set
    # CONFIG_USB_G_DBGP is not set
    # CONFIG_USB_G_WEBCAM is not set

    #
    # OTG and related infrastructure
    #
    CONFIG_USB_OTG_UTILS=y
    # CONFIG_USB_GPIO_VBUS is not set
    # CONFIG_USB_ULPI is not set
    CONFIG_NOP_USB_XCEIV=y
    CONFIG_MMC=y
    # CONFIG_MMC_DEBUG is not set
    # CONFIG_MMC_UNSAFE_RESUME is not set

    #
    # MMC/SD/SDIO Card Drivers
    #
    CONFIG_MMC_BLOCK=y
    CONFIG_MMC_BLOCK_MINORS=8
    CONFIG_MMC_BLOCK_BOUNCE=y
    # CONFIG_SDIO_UART is not set
    # CONFIG_MMC_TEST is not set

    #
    # MMC/SD/SDIO Host Controller Drivers
    #
    # CONFIG_MMC_SDHCI is not set
    # CONFIG_MMC_OMAP is not set
    CONFIG_MMC_OMAP_HS=y
    # CONFIG_MMC_DM385_EMMC is not set
    # CONFIG_MEMSTICK is not set
    CONFIG_NEW_LEDS=y
    CONFIG_LEDS_CLASS=y

    #
    # LED drivers
    #
    # CONFIG_LEDS_PCA9532 is not set
    CONFIG_LEDS_GPIO=y
    CONFIG_LEDS_CARBB=y
    CONFIG_LEDS_GPIO_PLATFORM=y
    # CONFIG_LEDS_LP3944 is not set
    # CONFIG_LEDS_LP5521 is not set
    # CONFIG_LEDS_LP5523 is not set
    # CONFIG_LEDS_PCA955X is not set
    # CONFIG_LEDS_DAC124S085 is not set
    # CONFIG_LEDS_REGULATOR is not set
    # CONFIG_LEDS_BD2802 is not set
    # CONFIG_LEDS_LT3593 is not set
    CONFIG_LEDS_TRIGGERS=y

    #
    # LED Triggers
    #
    CONFIG_LEDS_TRIGGER_TIMER=y
    CONFIG_LEDS_TRIGGER_HEARTBEAT=y
    # CONFIG_LEDS_TRIGGER_BACKLIGHT is not set
    # CONFIG_LEDS_TRIGGER_GPIO is not set
    # CONFIG_LEDS_TRIGGER_DEFAULT_ON is not set

    #
    # iptables trigger is under Netfilter config (LED target)
    #
    # CONFIG_ACCESSIBILITY is not set
    CONFIG_RTC_LIB=y
    CONFIG_RTC_CLASS=y
    CONFIG_RTC_HCTOSYS=y
    CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
    # CONFIG_RTC_DEBUG is not set

    #
    # RTC interfaces
    #
    CONFIG_RTC_INTF_SYSFS=y
    CONFIG_RTC_INTF_PROC=y
    CONFIG_RTC_INTF_DEV=y
    # CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
    # CONFIG_RTC_DRV_TEST is not set

    #
    # I2C RTC drivers
    #
    # CONFIG_RTC_DRV_DS1307 is not set
    # CONFIG_RTC_DRV_DS1374 is not set
    # CONFIG_RTC_DRV_DS1672 is not set
    # CONFIG_RTC_DRV_DS3232 is not set
    # CONFIG_RTC_DRV_MAX6900 is not set
    # CONFIG_RTC_DRV_RS5C372 is not set
    # CONFIG_RTC_DRV_ISL1208 is not set
    # CONFIG_RTC_DRV_ISL12022 is not set
    # CONFIG_RTC_DRV_X1205 is not set
    # CONFIG_RTC_DRV_PCF8563 is not set
    # CONFIG_RTC_DRV_PCF8583 is not set
    # CONFIG_RTC_DRV_M41T80 is not set
    CONFIG_RTC_DRV_BQ32K=y
    # CONFIG_RTC_DRV_S35390A is not set
    # CONFIG_RTC_DRV_FM3130 is not set
    # CONFIG_RTC_DRV_RX8581 is not set
    # CONFIG_RTC_DRV_RX8025 is not set

    #
    # SPI RTC drivers
    #
    # CONFIG_RTC_DRV_M41T94 is not set
    # CONFIG_RTC_DRV_DS1305 is not set
    # CONFIG_RTC_DRV_DS1390 is not set
    # CONFIG_RTC_DRV_MAX6902 is not set
    # CONFIG_RTC_DRV_R9701 is not set
    # CONFIG_RTC_DRV_RS5C348 is not set
    # CONFIG_RTC_DRV_DS3234 is not set
    # CONFIG_RTC_DRV_PCF2123 is not set

    #
    # Platform RTC drivers
    #
    # CONFIG_RTC_DRV_CMOS is not set
    # CONFIG_RTC_DRV_DS1286 is not set
    # CONFIG_RTC_DRV_DS1511 is not set
    # CONFIG_RTC_DRV_DS1553 is not set
    # CONFIG_RTC_DRV_DS1742 is not set
    # CONFIG_RTC_DRV_STK17TA8 is not set
    # CONFIG_RTC_DRV_M48T86 is not set
    # CONFIG_RTC_DRV_M48T35 is not set
    # CONFIG_RTC_DRV_M48T59 is not set
    # CONFIG_RTC_DRV_MSM6242 is not set
    # CONFIG_RTC_DRV_BQ4802 is not set
    # CONFIG_RTC_DRV_RP5C01 is not set
    # CONFIG_RTC_DRV_V3020 is not set

    #
    # on-CPU RTC drivers
    #
    # CONFIG_RTC_DRV_OMAP is not set
    # CONFIG_DMADEVICES is not set
    # CONFIG_AUXDISPLAY is not set
    CONFIG_UIO=y
    # CONFIG_UIO_PDRV is not set
    CONFIG_UIO_PDRV_GENIRQ=y
    # CONFIG_STAGING is not set
    CONFIG_Sys_Link=y
    CONFIG_SYSLINK_MULTIPROC=y
    CONFIG_SYSLINK_NOTIFY=y

    #
    # File systems
    #
    CONFIG_EXT2_FS=y
    CONFIG_EXT2_FS_XATTR=y
    CONFIG_EXT2_FS_POSIX_ACL=y
    CONFIG_EXT2_FS_SECURITY=y
    # CONFIG_EXT2_FS_XIP is not set
    CONFIG_EXT3_FS=y
    # CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
    CONFIG_EXT3_FS_XATTR=y
    CONFIG_EXT3_FS_POSIX_ACL=y
    CONFIG_EXT3_FS_SECURITY=y
    # CONFIG_EXT4_FS is not set
    CONFIG_JBD=y
    # CONFIG_JBD_DEBUG is not set
    CONFIG_FS_MBCACHE=y
    # CONFIG_REISERFS_FS is not set
    # CONFIG_JFS_FS is not set
    CONFIG_FS_POSIX_ACL=y
    # CONFIG_XFS_FS is not set
    # CONFIG_OCFS2_FS is not set
    # CONFIG_BTRFS_FS is not set
    # CONFIG_NILFS2_FS is not set
    CONFIG_FILE_LOCKING=y
    # CONFIG_FSNOTIFY is not set
    # CONFIG_DNOTIFY is not set
    # CONFIG_INOTIFY_USER is not set
    # CONFIG_FANOTIFY is not set
    # CONFIG_QUOTA is not set
    # CONFIG_QUOTACTL is not set
    # CONFIG_AUTOFS4_FS is not set
    # CONFIG_FUSE_FS is not set

    #
    # Caches
    #
    # CONFIG_FSCACHE is not set

    #
    # CD-ROM/DVD Filesystems
    #
    # CONFIG_ISO9660_FS is not set
    # CONFIG_UDF_FS is not set

    #
    # DOS/FAT/NT Filesystems
    #
    CONFIG_FAT_FS=y
    CONFIG_MSDOS_FS=y
    CONFIG_VFAT_FS=y
    CONFIG_FAT_DEFAULT_CODEPAGE=437
    CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
    # CONFIG_NTFS_FS is not set

    #
    # Pseudo filesystems
    #
    CONFIG_PROC_FS=y
    CONFIG_PROC_SYSCTL=y
    CONFIG_PROC_PAGE_MONITOR=y
    CONFIG_SYSFS=y
    CONFIG_TMPFS=y
    # CONFIG_TMPFS_POSIX_ACL is not set
    # CONFIG_HUGETLB_PAGE is not set
    # CONFIG_CONFIGFS_FS is not set
    CONFIG_MISC_FILESYSTEMS=y
    # CONFIG_ADFS_FS is not set
    # CONFIG_AFFS_FS is not set
    # CONFIG_ECRYPT_FS is not set
    # CONFIG_HFS_FS is not set
    # CONFIG_HFSPLUS_FS is not set
    # CONFIG_BEFS_FS is not set
    # CONFIG_BFS_FS is not set
    # CONFIG_EFS_FS is not set
    CONFIG_JFFS2_FS=y
    CONFIG_JFFS2_FS_DEBUG=0
    CONFIG_JFFS2_FS_WRITEBUFFER=y
    CONFIG_JFFS2_FS_WBUF_VERIFY=y
    # CONFIG_JFFS2_SUMMARY is not set
    # CONFIG_JFFS2_FS_XATTR is not set
    # CONFIG_JFFS2_COMPRESSION_OPTIONS is not set
    CONFIG_JFFS2_ZLIB=y
    # CONFIG_JFFS2_LZO is not set
    CONFIG_JFFS2_RTIME=y
    # CONFIG_JFFS2_RUBIN is not set
    CONFIG_UBIFS_FS=y
    # CONFIG_UBIFS_FS_XATTR is not set
    # CONFIG_UBIFS_FS_ADVANCED_COMPR is not set
    CONFIG_UBIFS_FS_LZO=y
    CONFIG_UBIFS_FS_ZLIB=y
    # CONFIG_UBIFS_FS_DEBUG is not set
    # CONFIG_LOGFS is not set
    # CONFIG_CRAMFS is not set
    # CONFIG_SQUASHFS is not set
    # CONFIG_VXFS_FS is not set
    # CONFIG_MINIX_FS is not set
    # CONFIG_OMFS_FS is not set
    # CONFIG_HPFS_FS is not set
    # CONFIG_QNX4FS_FS is not set
    # CONFIG_ROMFS_FS is not set
    # CONFIG_SYSV_FS is not set
    # CONFIG_UFS_FS is not set
    CONFIG_NETWORK_FILESYSTEMS=y
    CONFIG_NFS_FS=y
    CONFIG_NFS_V3=y
    # CONFIG_NFS_V3_ACL is not set
    CONFIG_NFS_V4=y
    # CONFIG_NFS_V4_1 is not set
    CONFIG_ROOT_NFS=y
    # CONFIG_NFS_USE_LEGACY_DNS is not set
    CONFIG_NFS_USE_KERNEL_DNS=y
    # CONFIG_NFS_USE_NEW_IDMAPPER is not set
    # CONFIG_NFSD is not set
    CONFIG_LOCKD=y
    CONFIG_LOCKD_V4=y
    CONFIG_NFS_COMMON=y
    CONFIG_SUNRPC=y
    CONFIG_SUNRPC_GSS=y
    CONFIG_RPCSEC_GSS_KRB5=y
    # CONFIG_CEPH_FS is not set
    # CONFIG_CIFS is not set
    # CONFIG_NCP_FS is not set
    # CONFIG_CODA_FS is not set
    # CONFIG_AFS_FS is not set

    #
    # Partition Types
    #
    # CONFIG_PARTITION_ADVANCED is not set
    CONFIG_MSDOS_PARTITION=y
    CONFIG_NLS=y
    CONFIG_NLS_DEFAULT="utf8"
    CONFIG_NLS_CODEPAGE_437=y
    # CONFIG_NLS_CODEPAGE_737 is not set
    # CONFIG_NLS_CODEPAGE_775 is not set
    # CONFIG_NLS_CODEPAGE_850 is not set
    # CONFIG_NLS_CODEPAGE_852 is not set
    # CONFIG_NLS_CODEPAGE_855 is not set
    # CONFIG_NLS_CODEPAGE_857 is not set
    # CONFIG_NLS_CODEPAGE_860 is not set
    # CONFIG_NLS_CODEPAGE_861 is not set
    # CONFIG_NLS_CODEPAGE_862 is not set
    # CONFIG_NLS_CODEPAGE_863 is not set
    # CONFIG_NLS_CODEPAGE_864 is not set
    # CONFIG_NLS_CODEPAGE_865 is not set
    # CONFIG_NLS_CODEPAGE_866 is not set
    # CONFIG_NLS_CODEPAGE_869 is not set
    # CONFIG_NLS_CODEPAGE_936 is not set
    # CONFIG_NLS_CODEPAGE_950 is not set
    # CONFIG_NLS_CODEPAGE_932 is not set
    # CONFIG_NLS_CODEPAGE_949 is not set
    # CONFIG_NLS_CODEPAGE_874 is not set
    # CONFIG_NLS_ISO8859_8 is not set
    # CONFIG_NLS_CODEPAGE_1250 is not set
    # CONFIG_NLS_CODEPAGE_1251 is not set
    CONFIG_NLS_ASCII=y
    CONFIG_NLS_ISO8859_1=y
    # CONFIG_NLS_ISO8859_2 is not set
    # CONFIG_NLS_ISO8859_3 is not set
    # CONFIG_NLS_ISO8859_4 is not set
    # CONFIG_NLS_ISO8859_5 is not set
    # CONFIG_NLS_ISO8859_6 is not set
    # CONFIG_NLS_ISO8859_7 is not set
    # CONFIG_NLS_ISO8859_9 is not set
    # CONFIG_NLS_ISO8859_13 is not set
    # CONFIG_NLS_ISO8859_14 is not set
    # CONFIG_NLS_ISO8859_15 is not set
    # CONFIG_NLS_KOI8_R is not set
    # CONFIG_NLS_KOI8_U is not set
    CONFIG_NLS_UTF8=y
    # CONFIG_DLM is not set

    #
    # Kernel hacking
    #
    # CONFIG_PRINTK_TIME is not set
    CONFIG_ENABLE_WARN_DEPRECATED=y
    CONFIG_ENABLE_MUST_CHECK=y
    CONFIG_FRAME_WARN=1024
    CONFIG_MAGIC_SYSRQ=y
    # CONFIG_STRIP_ASM_SYMS is not set
    # CONFIG_UNUSED_SYMBOLS is not set
    CONFIG_DEBUG_FS=y
    # CONFIG_HEADERS_CHECK is not set
    CONFIG_DEBUG_KERNEL=y
    # CONFIG_DEBUG_SHIRQ is not set
    # CONFIG_LOCKUP_DETECTOR is not set
    # CONFIG_HARDLOCKUP_DETECTOR is not set
    # CONFIG_DETECT_HUNG_TASK is not set
    # CONFIG_SCHED_DEBUG is not set
    # CONFIG_SCHEDSTATS is not set
    # CONFIG_TIMER_STATS is not set
    # CONFIG_DEBUG_OBJECTS is not set
    # CONFIG_SLUB_DEBUG_ON is not set
    # CONFIG_SLUB_STATS is not set
    # CONFIG_DEBUG_KMEMLEAK is not set
    # CONFIG_DEBUG_RT_MUTEXES is not set
    # CONFIG_RT_MUTEX_TESTER is not set
    # CONFIG_DEBUG_SPINLOCK is not set
    # CONFIG_DEBUG_MUTEXES is not set
    CONFIG_BKL=y
    # CONFIG_DEBUG_LOCK_ALLOC is not set
    # CONFIG_PROVE_LOCKING is not set
    # CONFIG_SPARSE_RCU_POINTER is not set
    # CONFIG_LOCK_STAT is not set
    # CONFIG_DEBUG_SPINLOCK_SLEEP is not set
    # CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
    # CONFIG_DEBUG_KOBJECT is not set
    # CONFIG_DEBUG_HIGHMEM is not set
    CONFIG_DEBUG_BUGVERBOSE=y
    # CONFIG_DEBUG_INFO is not set
    # CONFIG_DEBUG_VM is not set
    # CONFIG_DEBUG_WRITECOUNT is not set
    CONFIG_DEBUG_MEMORY_INIT=y
    # CONFIG_DEBUG_LIST is not set
    # CONFIG_TEST_LIST_SORT is not set
    # CONFIG_DEBUG_SG is not set
    # CONFIG_DEBUG_NOTIFIERS is not set
    # CONFIG_DEBUG_CREDENTIALS is not set
    CONFIG_FRAME_POINTER=y
    # CONFIG_BOOT_PRINTK_DELAY is not set
    # CONFIG_RCU_TORTURE_TEST is not set
    # CONFIG_KPROBES_SANITY_TEST is not set
    # CONFIG_BACKTRACE_SELF_TEST is not set
    # CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
    # CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
    # CONFIG_LKDTM is not set
    # CONFIG_FAULT_INJECTION is not set
    # CONFIG_LATENCYTOP is not set
    # CONFIG_SYSCTL_SYSCALL_CHECK is not set
    # CONFIG_PAGE_POISONING is not set
    CONFIG_HAVE_FUNCTION_TRACER=y
    CONFIG_HAVE_DYNAMIC_FTRACE=y
    CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
    CONFIG_TRACING_SUPPORT=y
    # CONFIG_FTRACE is not set
    # CONFIG_DYNAMIC_DEBUG is not set
    # CONFIG_ATOMIC64_SELFTEST is not set
    # CONFIG_SAMPLES is not set
    CONFIG_HAVE_ARCH_KGDB=y
    # CONFIG_KGDB is not set
    # CONFIG_STRICT_DEVMEM is not set
    # CONFIG_ARM_UNWIND is not set
    # CONFIG_DEBUG_USER is not set
    # CONFIG_DEBUG_ERRORS is not set
    # CONFIG_DEBUG_STACK_USAGE is not set
    CONFIG_DEBUG_LL=y
    CONFIG_EARLY_PRINTK=y
    # CONFIG_DEBUG_ICEDCC is not set
    # CONFIG_OC_ETM is not set

    #
    # Security options
    #
    CONFIG_KEYS=y
    CONFIG_KEYS_DEBUG_PROC_KEYS=y
    # CONFIG_SECURITY_DMESG_RESTRICT is not set
    CONFIG_SECURITY=y
    # CONFIG_SECURITYFS is not set
    CONFIG_SECURITY_NETWORK=y
    # CONFIG_SECURITY_NETWORK_XFRM is not set
    # CONFIG_SECURITY_PATH is not set
    # CONFIG_SECURITY_TOMOYO is not set
    # CONFIG_SECURITY_APPARMOR is not set
    # CONFIG_IMA is not set
    CONFIG_DEFAULT_SECURITY_DAC=y
    CONFIG_DEFAULT_SECURITY=""
    CONFIG_CRYPTO=y

    #
    # Crypto core or helper
    #
    CONFIG_CRYPTO_ALGAPI=y
    CONFIG_CRYPTO_ALGAPI2=y
    CONFIG_CRYPTO_AEAD2=y
    CONFIG_CRYPTO_BLKCIPHER=y
    CONFIG_CRYPTO_BLKCIPHER2=y
    CONFIG_CRYPTO_HASH=y
    CONFIG_CRYPTO_HASH2=y
    CONFIG_CRYPTO_RNG2=y
    CONFIG_CRYPTO_PCOMP2=y
    CONFIG_CRYPTO_MANAGER=y
    CONFIG_CRYPTO_MANAGER2=y
    CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
    # CONFIG_CRYPTO_GF128MUL is not set
    # CONFIG_CRYPTO_NULL is not set
    CONFIG_CRYPTO_WORKQUEUE=y
    # CONFIG_CRYPTO_CRYPTD is not set
    # CONFIG_CRYPTO_AUTHENC is not set
    # CONFIG_CRYPTO_TEST is not set

    #
    # Authenticated Encryption with Associated Data
    #
    CONFIG_CRYPTO_CCM=m
    CONFIG_CRYPTO_GCM=m
    CONFIG_CRYPTO_SEQIV=m

    #
    # Block modes
    #
    CONFIG_CRYPTO_CBC=y
    # CONFIG_CRYPTO_CTR is not set
    # CONFIG_CRYPTO_CTS is not set
    CONFIG_CRYPTO_ECB=y
    # CONFIG_CRYPTO_LRW is not set
    # CONFIG_CRYPTO_PCBC is not set
    # CONFIG_CRYPTO_XTS is not set

    #
    # Hash modes
    #
    # CONFIG_CRYPTO_HMAC is not set
    # CONFIG_CRYPTO_XCBC is not set
    # CONFIG_CRYPTO_VMAC is not set

    #
    # Digest
    #
    # CONFIG_CRYPTO_CRC32C is not set
    # CONFIG_CRYPTO_GHASH is not set
    # CONFIG_CRYPTO_MD4 is not set
    CONFIG_CRYPTO_MD5=y
    CONFIG_CRYPTO_MICHAEL_MIC=y
    # CONFIG_CRYPTO_RMD128 is not set
    # CONFIG_CRYPTO_RMD160 is not set
    # CONFIG_CRYPTO_RMD256 is not set
    # CONFIG_CRYPTO_RMD320 is not set
    # CONFIG_CRYPTO_SHA1 is not set
    # CONFIG_CRYPTO_SHA256 is not set
    # CONFIG_CRYPTO_SHA512 is not set
    # CONFIG_CRYPTO_TGR192 is not set
    # CONFIG_CRYPTO_WP512 is not set

    #
    # Ciphers
    #
    CONFIG_CRYPTO_AES=y
    # CONFIG_CRYPTO_ANUBIS is not set
    CONFIG_CRYPTO_ARC4=y
    # CONFIG_CRYPTO_BLOWFISH is not set
    # CONFIG_CRYPTO_CAMELLIA is not set
    # CONFIG_CRYPTO_CAST5 is not set
    # CONFIG_CRYPTO_CAST6 is not set
    CONFIG_CRYPTO_DES=y
    # CONFIG_CRYPTO_FCRYPT is not set
    # CONFIG_CRYPTO_KHAZAD is not set
    # CONFIG_CRYPTO_SALSA20 is not set
    # CONFIG_CRYPTO_SEED is not set
    # CONFIG_CRYPTO_SERPENT is not set
    # CONFIG_CRYPTO_TEA is not set
    # CONFIG_CRYPTO_TWOFISH is not set

    #
    # Compression
    #
    CONFIG_CRYPTO_DEFLATE=y
    # CONFIG_CRYPTO_ZLIB is not set
    CONFIG_CRYPTO_LZO=y

    #
    # Random Number Generation
    #
    # CONFIG_CRYPTO_ANSI_CPRNG is not set
    # CONFIG_CRYPTO_HW is not set
    # CONFIG_BINARY_PRINTF is not set

    #
    # Library routines
    #
    CONFIG_BITREVERSE=y
    CONFIG_GENERIC_FIND_LAST_BIT=y
    # CONFIG_CRC_CCITT is not set
    CONFIG_CRC16=y
    # CONFIG_CRC_T10DIF is not set
    # CONFIG_CRC_ITU_T is not set
    CONFIG_CRC32=y
    CONFIG_CRC7=y
    # CONFIG_LIBCRC32C is not set
    CONFIG_ZLIB_INFLATE=y
    CONFIG_ZLIB_DEFLATE=y
    CONFIG_LZO_COMPRESS=y
    CONFIG_LZO_DECOMPRESS=y
    CONFIG_DECOMPRESS_GZIP=y
    CONFIG_DECOMPRESS_BZIP2=y
    CONFIG_DECOMPRESS_LZMA=y
    CONFIG_DECOMPRESS_LZO=y
    CONFIG_HAS_IOMEM=y
    CONFIG_HAS_IOPORT=y
    CONFIG_HAS_DMA=y
    CONFIG_NLATTR=y

  • Still no luck, all wl18xx modules have been built and when I try to manually load them, I get the following:
    insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/wirele
    ss/cfg80211.ko
    cfg80211: Calling CRDA to update world regulatory domain
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/mac802
    11/mac80211.ko
    mac80211: Unknown symbol unregister_inet6addr_notifier (err 0)
    mac80211: Unknown symbol register_inet6addr_notifier (err 0)
    insmod: error inserting '/lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/mac80211/mac80211.ko': -1 Unknown symbol in module
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/ne
    t/wireless/ti/wlcore/wlcore.ko
    wlcore: Unknown symbol ieee80211_connection_loss (err 0)
    wlcore: Unknown symbol ieee80211_sched_scan_stopped (err 0)
    wlcore: Unknown symbol ieee80211_chswitch_done (err 0)
    wlcore: Unknown symbol ieee80211_free_hw (err 0)
    wlcore: Unknown symbol ieee80211_probereq_get (err 0)
    wlcore: Unknown symbol ieee80211_ap_probereq_get (err 0)
    wlcore: Unknown symbol ieee80211_alloc_hw (err 0)
    wlcore: Unknown symbol ieee80211_nullfunc_get (err 0)
    wlcore: Unknown symbol ieee80211_pspoll_get (err 0)
    wlcore: Unknown symbol ieee80211_register_hw (err 0)
    wlcore: Unknown symbol ieee80211_restart_hw (err 0)
    wlcore: Unknown symbol ieee80211_stop_rx_ba_session (err 0)
    wlcore: Unknown symbol ieee80211_wake_queue (err 0)
    wlcore: Unknown symbol ieee80211_find_sta (err 0)
    wlcore: Unknown symbol wiphy_to_ieee80211_hw (err 0)
    wlcore: Unknown symbol ieee80211_queue_delayed_work (err 0)
    wlcore: Unknown symbol ieee80211_proberesp_get (err 0)
    wlcore: Unknown symbol ieee80211_remain_on_channel_expired (err 0)
    wlcore: Unknown symbol ieee80211_wake_queues (err 0)
    wlcore: Unknown symbol ieee80211_report_low_ack (err 0)
    wlcore: Unknown symbol ieee80211_iterate_active_interfaces (err 0)
    wlcore: Unknown symbol ieee80211_free_txskb (err 0)
    wlcore: Unknown symbol ieee80211_tx_status (err 0)
    wlcore: Unknown symbol ieee80211_stop_queue (err 0)
    wlcore: Unknown symbol ieee80211_ready_on_channel (err 0)
    wlcore: Unknown symbol ieee80211_stop_queues (err 0)
    wlcore: Unknown symbol ieee80211_sched_scan_results (err 0)
    wlcore: Unknown symbol ieee80211_scan_completed (err 0)
    wlcore: Unknown symbol ieee80211_iterate_active_interfaces_atomic (err 0)
    wlcore: Unknown symbol ieee80211_unregister_hw (err 0)
    wlcore: Unknown symbol ieee80211_beacon_get_tim (err 0)
    wlcore: Unknown symbol ieee80211_cqm_rssi_notify (err 0)
    wlcore: Unknown symbol ieee80211_queue_work (err 0)
    wlcore: Unknown symbol ieee80211_sta_ps_transition (err 0)
    wlcore: Unknown symbol ieee80211_csa_finish (err 0)
    wlcore: Unknown symbol mac80211_ieee80211_rx (err 0)
    insmod: error inserting '/lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/net/wireless/ti/wlcore/wlcore.ko': -1 Unknown symbol in module
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/ne
    t/wireless/ti/wl18xx/wl18xx.ko
    wl18xx: Unknown symbol ieee80211_connection_loss (err 0)
    wl18xx: Unknown symbol wl1271_cmd_send (err 0)
    wl18xx: Unknown symbol wl12xx_is_dummy_packet (err 0)
    wl18xx: Unknown symbol wlcore_event_roc_complete (err 0)
    wl18xx: Unknown symbol wlcore_scan_sched_scan_ssid_list (err 0)
    wl18xx: Unknown symbol wlcore_translate_addr (err 0)
    wl18xx: Unknown symbol wlcore_boot_run_firmware (err 0)
    wl18xx: Unknown symbol wlcore_set_scan_chan_params (err 0)
    wl18xx: Unknown symbol wl1271_debugfs_update_stats (err 0)
    wl18xx: Unknown symbol wl1271_format_buffer (err 0)
    wl18xx: Unknown symbol wlcore_free_hw (err 0)
    wl18xx: Unknown symbol wlcore_scan_sched_scan_results (err 0)
    wl18xx: Unknown symbol wl1271_free_tx_id (err 0)
    wl18xx: Unknown symbol wlcore_event_max_tx_failure (err 0)
    wl18xx: Unknown symbol wlcore_remove (err 0)
    wl18xx: Unknown symbol wlcore_disable_interrupts (err 0)
    wl18xx: Unknown symbol wlcore_event_channel_switch (err 0)
    wl18xx: Unknown symbol ieee80211_queue_delayed_work (err 0)
    wl18xx: Unknown symbol wl1271_ps_elp_sleep (err 0)
    wl18xx: Unknown symbol wlcore_enable_interrupts (err 0)
    wl18xx: Unknown symbol wlcore_set_partition (err 0)
    wl18xx: Unknown symbol wlcore_boot_upload_firmware (err 0)
    wl18xx: Unknown symbol wlcore_event_sched_scan_completed (err 0)
    wl18xx: Unknown symbol wl1271_cmd_configure (err 0)
    wl18xx: Unknown symbol ieee80211_change_rx_ba_max_subframes (err 0)
    wl18xx: Unknown symbol wlcore_radar_detection_debug (err 0)
    wl18xx: Unknown symbol wlcore_alloc_hw (err 0)
    wl18xx: Unknown symbol wlcore_probe (err 0)
    wl18xx: Unknown symbol wlcore_cmd_wait_for_event_or_timeout (err 0)
    wl18xx: Unknown symbol wlcore_event_rssi_trigger (err 0)
    wl18xx: Unknown symbol wlcore_rx_ba_max_subframes (err 0)
    wl18xx: Unknown symbol ieee80211_radar_detected (err 0)
    wl18xx: Unknown symbol wlcore_event_ba_rx_constraint (err 0)
    wl18xx: Unknown symbol wlcore_event_inactive_sta (err 0)
    wl18xx: Unknown symbol wlcore_event_dummy_packet (err 0)
    wl18xx: Unknown symbol wlcore_event_beacon_loss (err 0)
    wl18xx: Unknown symbol wlcore_set_key (err 0)
    wl18xx: Unknown symbol wl12xx_debug_level (err 0)
    wl18xx: Unknown symbol wl1271_ps_elp_wakeup (err 0)
    wl18xx: Unknown symbol wl12xx_cmd_build_probe_req (err 0)
    insmod: error inserting '/lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/net/wireless/ti/wl18xx/wl18xx.ko': -1 Unknown symbol in module
  • Could this issue be caused by improper defconfig settings?
  • I now have the modules loading properly. The ipv6.ko module was required for the mac80211 module to load.
    I do not see wlan0 in my ifconfig:
    root@dm814x-evm:~# ifconfig
    eth0 Link encap:Ethernet HWaddr 20:CD:39:6C:D1:FC
    inet addr:192.168.1.240 Bcast:192.168.1.255 Mask:255.255.255.0
    inet6 addr: fe80::22cd:39ff:fe6c:d1fc/64 Scope:Link
    UP BROADCAST RUNNING ALLMULTI MULTICAST MTU:1500 Metric:1
    RX packets:7777 errors:0 dropped:23 overruns:0 frame:0
    TX packets:4870 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:8376548 (7.9 MiB) TX bytes:679270 (663.3 KiB)
    Interrupt:40

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    inet6 addr: ::1/128 Scope:Host
    UP LOOPBACK RUNNING MTU:16436 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    root@dm814x-evm:~#

    root@dm814x-evm:~# ifconfig wlan0 up
    ifconfig: SIOCGIFFLAGS: No such device
    root@dm814x-evm:~#



    root@dm814x-evm:~#
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/compat/com
    pat.ko
    insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/net/wireless/ti/wlcore/wlcore.ko
    insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/net/wireless/ti/wlcore/wlcore_sdio.ko
    insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/net/wireless/ti/wl18xx/wl18xx.koLoading modules backported from Linux version R8.4-0-gd03410c
    Backport generated by backports.git R8.4-0-g0d46f43
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/wirele
    ss/cfg80211.ko
    cfg80211: Calling CRDA to update world regulatory domain
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/ipv6/i
    pv6.ko
    NET: Registered protocol family 10
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/net/mac802
    11/mac80211.ko
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/ne
    t/wireless/ti/wlcore/wlcore.ko
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/ne
    t/wireless/ti/wlcore/wlcore_sdio.ko
    root@dm814x-evm:~# insmod /lib/modules/2.6.37_DM385_CBB_1.50.50/extra/drivers/ne
    t/wireless/ti/wl18xx/wl18xx.ko
    root@dm814x-evm:~#
    root@dm814x-evm:~# lsmod
    Module Size Used by
    wl18xx 79788 0
    wlcore_sdio 3218 0
    wlcore 164961 1 wl18xx
    mac80211 310010 2 wl18xx,wlcore
    ipv6 208597 9 mac80211
    cfg80211 176975 3 wl18xx,wlcore,mac80211
    compat 16095 5 wl18xx,wlcore_sdio,wlcore,mac80211,cfg80211
    syslink 772850 0
    root@dm814x-evm:~#
  • Hello,
    Do you know when I will be contacted? Is my issue posted in the correct forum? It appears this is a very difficult issue and there is no support. I switched to the wl18xx module as you recommended and spent weeks trying to implement it.
    Please let me know if there is some way to get support from TI on this issue.
  • You are trying to port to a pretty old kernel 2.6.37. Though some folks attempted and were successful with K2.6.37 back port for WL18xx, it is not actively supported from our side. Did, you check the instructions at the below for DM365 port?
    processors.wiki.ti.com/.../Using_WL18xx_with_DM365_EVM

    From, your above logs it seems like the modules are getting installed. Try putting some debug prints or trace with Debugger in 'wlcore' driver if the probe functions are getting invoked and where it is failing..

    Thanks
  • Yes, I did check the instructions for the DM365 with wl18xx and there were errors applying the scripts.
    I followed the processors.wiki.ti.com/.../WL18xx_to_DM3xx_porting_guide which states it can be specifically used to build against kernel 2.6.37 and now have the modules built and loading. The issue is there is no wlan0 listed when ifconfig command is issued.
    It appears we are close to resolving the issues on 2.6.37 but may be difficult if not supported on E2E.

    I am currently using the carbb kernel 2.6.37 cbb_psp_04_04_00_02
    using the DM385 CBB RDK from nSketch. Which kernel do you recommend we use?

    Is there a new kernel download available for the nSketch dm385cbb, carbb_rdk_GA_v1.1?

    Are the wl18xx drivers built into the latest kernel releases?
    How can I get support on 2.6.37 to complete this integration?

    Thanks for your assistance!

    Mark

  • Hello,

    I am currently using carbb-rdk-dm385_v1.5.7, cbb_psp_04_04_00_02 which is kernel version 2.6.37 and need to integrate the wl18xx wifi module. TI recommended I upgrade to the latest kernel to get support.

    Is there a newer version with wlan/wl18xx integrated , and if so, where can I get it?

    I have downloaded newer kernel versions but they are not specific to the CARBB. I need the latest wl18xx drivers and source integrated.

    Any help is appreciated.

    Mark
  • Hi,

    We understand you are attempting to upgrade the kernel (v4.4)
    using the ipnc-rdk--ipnc-ti-linux-kernel-ipnc-lsk-linux-4.4-dm38x-wlan.tar.gz

    Taking a look at this kernel it seems like wilink8 is supported as part of this .dts file:

    git.ti.com/.../dm38x-csk.dts

    Also based on the documentation:
    processors.wiki.ti.com/.../IPNC_RDK_DM38x_,_DM8127

    it seems like wilink8 wlan should be functional with this v4.4 kernel/release and you should be able to build the drivers in-tree.
    Please let us know in case you run into any issues.

    Best Regards,
    Eyal
  • Hi Eyal,

    Thanks for your reply and additional information. Is the dm38x-csk.dts specific to the dm385 carBB? I have not upgraded the kernel in the past and just want to be sure I am working with sources that will work with the nsketch DM385 Car BB.

    I assume my user applications should work as well, correct?

    Thanks, Mark