This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200MODLAUNCHXL: error #10010: errors encountered during linking "<projectname>.out"

Part Number: CC3200MODLAUNCHXL
Other Parts Discussed in Thread: CC3200SDK

Hello -

I made a new project using the spi_demo code as a reference.  When I try and build, I get the following error:


**** Build of configuration Debug for project spi_1553 ****

"C:\\TI\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: ARM Compiler'
"C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/bin/armcl" -mv4 --code_state=32 --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/inc" --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/driverlib" --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/example/common" --include_path="C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/include" -g --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="main.d"  "../main.c"
'Finished building: ../main.c'
' '
'Building file: ../pinmux.c'
'Invoking: ARM Compiler'
"C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/bin/armcl" -mv4 --code_state=32 --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/inc" --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/driverlib" --include_path="C:/TI/CC3200SDK_1.3.0/cc3200-sdk/example/common" --include_path="C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/include" -g --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="pinmux.d"  "../pinmux.c"
'Finished building: ../pinmux.c'
' '
'Building target: spi_1553.out'
'Invoking: ARM Linker'
"C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/bin/armcl" -mv4 --code_state=32 -g --diag_wrap=off --diag_warning=225 --display_error_number -z -m"spi_1553.map" -i"C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/lib" -i"C:/TI/CC3200SDK_1.3.0/cc3200-sdk/driverlib" -i"C:/TI/ccsv6/tools/compiler/arm_15.12.3.LTS/include" --reread_libs --diag_wrap=off --warn_sections --display_error_number --xml_link_info="spi_1553_linkInfo.xml" --rom_model -o "spi_1553.out" "./main.obj" "./pinmux.obj" "../cc3200v1p32.cmd"  -llibc.a
<Linking>
warning #10210-D: creating ".stack" section with default size of 0x800; use the -stack option to change the default size

 undefined               first referenced
  symbol                     in file    
 ---------               ----------------
 ClearTerm               ./main.obj     
 InitTerm                ./main.obj     
 IntEnable               ./main.obj     
 IntMasterEnable         ./main.obj     
 Message                 ./main.obj     
 PRCMCC3200MCUInit       ./main.obj     
 PRCMPeripheralClkEnable ./main.obj     
 PRCMPeripheralClockGet  ./main.obj     
 PRCMPeripheralReset     ./main.obj     
 PinTypeSPI              ./pinmux.obj   
 PinTypeUART             ./pinmux.obj   
 Report                  ./main.obj     
 SPICSDisable            ./main.obj     
 SPICSEnable             ./main.obj     
 SPIConfigSetExpClk      ./main.obj     
 SPIDataGet              ./main.obj     
 SPIDataGetNonBlocking   ./main.obj     
 SPIDataPut              ./main.obj     
 SPIEnable               ./main.obj     
 SPIIntClear             ./main.obj     
 SPIIntEnable            ./main.obj     
 SPIIntRegister          ./main.obj     
 SPIIntStatus            ./main.obj     
 SPIReset                ./main.obj     
 SPITransfer             ./main.obj     
 UARTCharGet             ./main.obj     
 UARTCharPut             ./main.obj     

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "spi_1553.out" not built

gmake: *** [spi_1553.out] Error 1
>> Compilation failure
makefile:141: recipe for target 'spi_1553.out' failed
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

Any help will do!

Thanks