This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1831MOD: Kernel Crash happening randomly / During long running of Wi-Fi module .

Part Number: WL1831MOD


Tool/software: Linux

Hi ,

In my project , i am using WL1831mod to communicate with cloud . Here i have configured Wl1831mod  as Client . I am facing kernel crash issue during long run or some time randomely (cant able to find the root cause) . After this crash i cant able to connect with any AP until i have reboot the board . I need immediate support and solution from Ti . Kindly look below the details of firmware and driver version ,

Kernel Crash Log:

wlcore: down
ieee80211 phy0: Hardware restart was requested
wlcore: PHY firmware version: Rev 8.2.0.0.237
wlcore: firmware booted (Rev 8.9.0.0.70)
wlcore: ERROR SW watchdog interrupt received! starting recovery.
------------[ cut here ]------------
WARNING: CPU: 0 PID: 378 at
/home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/build_elika76_92_dual/tmp/work/eliuaccs_dual-poky-linux-gnueabi/ti-compat-wl18xx/r8.a6.01-r0/ compat_wireless/drivers/net/wireless/ti/wlcore/main.c:806
wl12xx_queue_recovery_work.part.39+0x58/0x5c [wlcore]()
Modules linked in: wiegand_input snd_soc_microsemi_dac(O) zl380tw(O) v4l2loopback(O)
wl18xx(O) wlcore_sdio(O) wlcore(O) mac80211(O) cfg80211(O) compat(O) mxc_v4l2_capture
ipu_bg_overlay_sdc ipu_still ipu_prp_enc ov5640_camera_mipi ipu_csi_enc ipu_fg_overlay_sdc v4l2_int_device evbug
CPU: 0 PID: 378 Comm: irq/261-wl18xx Tainted: G W O 3.14.28_1.0.0_ga-eliuaccs #1
[<80014b10>] (unwind_backtrace) from [<800117ec>] (show_stack+0x10/0x14)
[<800117ec>] (show_stack) from [<806b3154>] (dump_stack+0x7c/0xbc)
[<806b3154>] (dump_stack) from [<8002ef34>] (warn_slowpath_common+0x70/0x8c)
[<8002ef34>] (warn_slowpath_common) from [<8002efec>] (warn_slowpath_null+0x1c/0x24)
[<8002efec>] (warn_slowpath_null) from [<7f127bd8>] (wl12xx_queue_recovery_work.part.39+0x58/0x5c [wlcore])
[<7f127bd8>] (wl12xx_queue_recovery_work.part.39 [wlcore]) from [<7f127e64>] (wlcore_irq+0x168/0x16c [wlcore])
[<7f127e64>] (wlcore_irq [wlcore]) from [<8006a5d8>] (irq_thread_fn+0x1c/0x40)
[<8006a5d8>] (irq_thread_fn) from [<8006a8d0>] (irq_thread+0x124/0x164)
[<8006a8d0>] (irq_thread) from [<80049a5c>] (kthread+0xcc/0xe4)
[<80049a5c>] (kthread) from [<8000e5f8>] (ret_from_fork+0x14/0x3c)
---[ end trace a0fb62a307cabee7 ]---

 

Firmware PHY version : Rev 8.2.0.0.237

Firmware Wlcore version : Rev 8.9.0.0.70

Backport version : R8.7_SP1-0

 

 

 

 

  • Ganesh , 

    What happens after recovery / crash ? In logs do you see WiLink8 firmware getting downloaded again ?

    Thanks

    Saurabh

  • Hi Saurabh ,

    After crash , Module is not connecting with AP 's and throwing some PSK IO error.
  • Hi, Can you pls share the logs

    Thanks
    Saurabh
  • Hi ,

    I have already shared the logs above ...
  • Hi ,

    Please find the attachment of crash , dmesg & kernel boot logs .

    root@eliuaccs-dual:~# Status: BTS Script successfully executed.
    DEVM_PowerOnDevice() Success: 0.
    Attempting to set Discoverability Mode: General.
    
    Device Powered On.
    DEVM_UpdateLocalDeviceProperties() Success: 0.
    
    Local Device Properties Changed.
    Disc. Mode:   TRUE , 0x00000001
    DEVM_QueryLocalDeviceProperties() Success: 0.
    BD Address - D0B5C2F1EE9E
    File is already there dont create
    GATM_RegisterEventCallback() Success: 1.
    DEVM_UpdateLocalDeviceProperties() Success: 0.
    ELIKA-D0B5C2F1EE9EAttempting to set Device Name to: "ELIKA-D0B5C2F1EE9E".
    
    Local Device Properties Changed.
    root@eliuaccs-dual:~# ------------[ cut here ]------------
    WARNING: CPU: 0 PID: 344 at /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/build_elika76_92_dual/tmp/work/eliuaccs_dual-poky-linux-gnueabi/t)
    Modules linked in: wiegand_input snd_soc_microsemi_dac(O) zl380tw(O) v4l2loopback(O) wl18xx(O) wlcore_sdio(O) wlcore(O) mac80211(O) cfg80211(Ot
    CPU: 0 PID: 344 Comm: irq/261-wl18xx Tainted: G           O 3.14.28_1.0.0_ga-eliuaccs #1
    [<80014b10>] (unwind_backtrace) from [<800117ec>] (show_stack+0x10/0x14)
    [<800117ec>] (show_stack) from [<806bed58>] (dump_stack+0x7c/0xbc)
    [<806bed58>] (dump_stack) from [<8002ef34>] (warn_slowpath_common+0x70/0x8c)
    [<8002ef34>] (warn_slowpath_common) from [<8002efec>] (warn_slowpath_null+0x1c/0x24)
    [<8002efec>] (warn_slowpath_null) from [<7f1821a4>] (wl12xx_sdio_raw_write+0xb0/0x138 [wlcore_sdio])
    [<7f1821a4>] (wl12xx_sdio_raw_write [wlcore_sdio]) from [<7f1553b8>] (wl1271_ps_elp_wakeup+0x130/0x1f4 [wlcore])
    [<7f1553b8>] (wl1271_ps_elp_wakeup [wlcore]) from [<7f148e04>] (wlcore_irq_locked+0x4c/0x6bc [wlcore])
    [<7f148e04>] (wlcore_irq_locked [wlcore]) from [<7f149dc8>] (wlcore_irq+0xcc/0x16c [wlcore])
    [<7f149dc8>] (wlcore_irq [wlcore]) from [<8006a5d8>] (irq_thread_fn+0x1c/0x40)
    [<8006a5d8>] (irq_thread_fn) from [<8006a8d0>] (irq_thread+0x124/0x164)
    [<8006a8d0>] (irq_thread) from [<80049a5c>] (kthread+0xcc/0xe4)
    [<80049a5c>] (kthread) from [<8000e5f8>] (ret_from_fork+0x14/0x3c)
    ---[ end trace ce4f09d43fb1920a ]---
    wl1271_sdio mmc1:0001:2: sdio write failed (-110)
    ------------[ cut here ]------------
    WARNING: CPU: 0 PID: 344 at /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/build_elika76_92_dual/tmp/work/eliuaccs_dual-poky-linux-gnueabi/t)
    Modules linked in: wiegand_input snd_soc_microsemi_dac(O) zl380tw(O) v4l2loopback(O) wl18xx(O) wlcore_sdio(O) wlcore(O) mac80211(O) cfg80211(Ot
    CPU: 0 PID: 344 Comm: irq/261-wl18xx Tainted: G        W  O 3.14.28_1.0.0_ga-eliuaccs #1
    [<80014b10>] (unwind_backtrace) from [<800117ec>] (show_stack+0x10/0x14)
    [<800117ec>] (show_stack) from [<806bed58>] (dump_stack+0x7c/0xbc)
    [<806bed58>] (dump_stack) from [<8002ef34>] (warn_slowpath_common+0x70/0x8c)
    [<8002ef34>] (warn_slowpath_common) from [<8002efec>] (warn_slowpath_null+0x1c/0x24)
    [<8002efec>] (warn_slowpath_null) from [<7f149bd8>] (wl12xx_queue_recovery_work.part.39+0x58/0x5c [wlcore])
    [<7f149bd8>] (wl12xx_queue_recovery_work.part.39 [wlcore]) from [<7f15536c>] (wl1271_ps_elp_wakeup+0xe4/0x1f4 [wlcore])
    [<7f15536c>] (wl1271_ps_elp_wakeup [wlcore]) from [<7f148e04>] (wlcore_irq_locked+0x4c/0x6bc [wlcore])
    [<7f148e04>] (wlcore_irq_locked [wlcore]) from [<7f149dc8>] (wlcore_irq+0xcc/0x16c [wlcore])
    [<7f149dc8>] (wlcore_irq [wlcore]) from [<8006a5d8>] (irq_thread_fn+0x1c/0x40)
    [<8006a5d8>] (irq_thread_fn) from [<8006a8d0>] (irq_thread+0x124/0x164)
    [<8006a8d0>] (irq_thread) from [<80049a5c>] (kthread+0xcc/0xe4)
    [<80049a5c>] (kthread) from [<8000e5f8>] (ret_from_fork+0x14/0x3c)
    ---[ end trace ce4f09d43fb1920b ]---
    wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.70
    wlcore: down
    ieee80211 phy0: Hardware restart was requested
    wlcore: ERROR firmware boot failed despite 3 retries
    ------------[ cut here ]------------
    WARNING: CPU: 0 PID: 466 at /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/build_elika76_92_dual/tmp/work/eliuaccs_dual-poky-linux-gnueabi/t)
    Modules linked in: wiegand_input snd_soc_microsemi_dac(O) zl380tw(O) v4l2loopback(O) wl18xx(O) wlcore_sdio(O) wlcore(O) mac80211(O) cfg80211(Ot
    CPU: 0 PID: 466 Comm: kworker/0:3 Tainted: G        W  O 3.14.28_1.0.0_ga-eliuaccs #1
    Workqueue: events_freezable ieee80211_restart_work [mac80211]
    [<80014b10>] (unwind_backtrace) from [<800117ec>] (show_stack+0x10/0x14)
    [<800117ec>] (show_stack) from [<806bed58>] (dump_stack+0x7c/0xbc)
    [<806bed58>] (dump_stack) from [<8002ef34>] (warn_slowpath_common+0x70/0x8c)
    [<8002ef34>] (warn_slowpath_common) from [<8002efec>] (warn_slowpath_null+0x1c/0x24)
    [<8002efec>] (warn_slowpath_null) from [<7f0dc414>] (ieee80211_reconfig+0x158/0xa18 [mac80211])
    [<7f0dc414>] (ieee80211_reconfig [mac80211]) from [<7f0b01d4>] (ieee80211_restart_work+0x60/0x8c [mac80211])
    [<7f0b01d4>] (ieee80211_restart_work [mac80211]) from [<800436ec>] (process_one_work+0xf4/0x35c)
    [<800436ec>] (process_one_work) from [<8004433c>] (worker_thread+0x130/0x3bc)
    [<8004433c>] (worker_thread) from [<80049a5c>] (kthread+0xcc/0xe4)
    [<80049a5c>] (kthread) from [<8000e5f8>] (ret_from_fork+0x14/0x3c)
    ---[ end trace ce4f09d43fb1920c ]---
    ------------[ cut here ]------------
    WARNING: CPU: 0 PID: 466 at /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/build_elika76_92_dual/tmp/work/eliuaccs_dual-poky-linux-gnueabi/t)
    wlan0:  Failed check-sdata-in-driver check, flags: 0x0
    Modules linked in: wiegand_input snd_soc_microsemi_dac(O) zl380tw(O) v4l2loopback(O) wl18xx(O) wlcore_sdio(O) wlcore(O) mac80211(O) cfg80211(Ot
    CPU: 0 PID: 466 Comm: kworker/0:3 Tainted: G        W  O 3.14.28_1.0.0_ga-eliuaccs #1
    Workqueue: events_freezable ieee80211_restart_work [mac80211]
    [<80014b10>] (unwind_backtrace) from [<800117ec>] (show_stack+0x10/0x14)
    [<800117ec>] (show_stack) from [<806bed58>] (dump_stack+0x7c/0xbc)
    [<806bed58>] (dump_stack) from [<8002ef34>] (warn_slowpath_common+0x70/0x8c)
    [<8002ef34>] (warn_slowpath_common) from [<8002ef80>] (warn_slowpath_fmt+0x30/0x40)
    [<8002ef80>] (warn_slowpath_fmt) from [<7f0b308c>] (drv_remove_interface+0x68/0x70 [mac80211])
    [<7f0b308c>] (drv_remove_interface [mac80211]) from [<7f0c3894>] (ieee80211_do_stop+0x4a4/0x7a0 [mac80211])
    [<7f0c3894>] (ieee80211_do_stop [mac80211]) from [<7f0c3ba0>] (ieee80211_stop+0x10/0x18 [mac80211])
    [<7f0c3ba0>] (ieee80211_stop [mac80211]) from [<8057cda8>] (__dev_close_many+0x88/0xd0)
    [<8057cda8>] (__dev_close_many) from [<8057ce58>] (dev_close_many+0x68/0xe0)
    [<8057ce58>] (dev_close_many) from [<8057f8bc>] (dev_close+0x38/0x50)
    [<8057f8bc>] (dev_close) from [<7f069550>] (cfg80211_shutdown_all_interfaces+0x38/0xa4 [cfg80211])
    [<7f069550>] (cfg80211_shutdown_all_interfaces [cfg80211]) from [<7f0dc45c>] (ieee80211_reconfig+0x1a0/0xa18 [mac80211])
    [<7f0dc45c>] (ieee80211_reconfig [mac80211]) from [<7f0b01d4>] (ieee80211_restart_work+0x60/0x8c [mac80211])
    [<7f0b01d4>] (ieee80211_restart_work [mac80211]) from [<800436ec>] (process_one_work+0xf4/0x35c)
    [<800436ec>] (process_one_work) from [<8004433c>] (worker_thread+0x130/0x3bc)
    [<8004433c>] (worker_thread) from [<80049a5c>] (kthread+0xcc/0xe4)
    [<80049a5c>] (kthread) from [<8000e5f8>] (ret_from_fork+0x14/0x3c)
    ---[ end trace ce4f09d43fb1920d ]---
    
    

    root@eliuaccs-dual:~# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 3.14.28_1.0.0_ga-eliuaccs (vvdnlt230@vvdnlt230-Latitude-3540) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Fri Sep 27
    [    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine model: Wandboard i.MX6 Dual Lite Board
    [    0.000000] cma: CMA: reserved 320 MiB at 1c000000
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] On node 0 totalpages: 131072
    [    0.000000] free_area_init_node: node 0, pgdat 80dc1e00, node_mem_map 8bb57000
    [    0.000000]   DMA zone: 1024 pages used for memmap
    [    0.000000]   DMA zone: 0 pages reserved
    [    0.000000]   DMA zone: 131072 pages, LIFO batch:31
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] PERCPU: Embedded 8 pages/cpu @8bb33000 s8896 r8192 d15680 u32768
    [    0.000000] pcpu-alloc: s8896 r8192 d15680 u32768 alloc=8*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    [    0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw
    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 176748K/524288K available (7115K kernel code, 404K rwdata, 6192K rodata, 336K init, 431K bss, 347540K reserved, 0K high)
    [    0.000000] Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
        lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
        pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
        modules : 0x7f000000 - 0x7fe00000   (  14 MB)
          .text : 0x80008000 - 0x80d07150   (13309 kB)
          .init : 0x80d08000 - 0x80d5c2c0   ( 337 kB)
          .data : 0x80d5e000 - 0x80dc31a0   ( 405 kB)
           .bss : 0x80dc31fc - 0x80e2f1a4   ( 432 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] L310 cache controller enabled
    [    0.000000] l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32450000, Cache size: 512 kB
    [    0.000000] failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22
    [    0.000000] Switching to timer-based delay loop
    [    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
    [    0.001030] Console: colour dummy device 80x30
    [    0.001047] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
    [    0.001059] pid_max: default: 32768 minimum: 301
    [    0.001222] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.001233] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.008857] CPU: Testing write buffer coherency: ok
    [    0.009172] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.009217] Setting up static identity map for 0x106c4360 - 0x106c43b8
    [    0.060384] CPU1: failed to boot: -38
    [    0.060417] Brought up 1 CPUs
    [    0.060423] SMP: Total of 1 processors activated.
    [    0.060429] CPU: All CPU(s) started in SVC mode.
    [    0.060950] devtmpfs: initialized
    [    0.064603] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    [    0.064963] pinctrl core: initialized pinctrl subsystem
    [    0.065275] regulator-dummy: no parameters
    [    0.081932] NET: Registered protocol family 16
    [    0.089212] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.089816] cpuidle: using governor ladder
    [    0.089825] cpuidle: using governor menu
    [    0.089919] CPU identified as i.MX6DL, silicon rev 1.3
    [    0.090015] Use WDOG1 as reset source
    [    0.099100] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
    [    0.099391] vdd1p1: 800 <--> 1375 mV at 1100 mV 
    [    0.099761] vdd3p0: 2800 <--> 3150 mV at 3000 mV 
    [    0.100093] vdd2p5: 2000 <--> 2750 mV at 2400 mV 
    [    0.100478] vddarm: 725 <--> 1450 mV at 1150 mV 
    [    0.110357] vddpu: 725 <--> 1450 mV at 1150 mV 
    [    0.110729] vddsoc: 725 <--> 1450 mV at 1175 mV 
    [    0.112681] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
    [    0.115570] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
    [    0.120072] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    [    0.120080] hw-breakpoint: maximum watchpoint size is 4 bytes.
    [    0.122185] imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
    [    0.134179] bio: create slab <bio-0> at 0
    [    0.136445] mxs-dma 110000.dma-apbh: initialized
    [    0.137156] wilink_wl_en: 1800 mV 
    [    0.137394] 1P8V: 1800 mV 
    [    0.137599] 2P5V: 2500 mV 
    [    0.137810] 3P3V: 3300 mV 
    [    0.138038] usb_h1_vbus: 5000 mV 
    [    0.138271] usb_otg_vbus: 5000 mV 
    [    0.138884] i2c-core: driver [max17135] using legacy suspend method
    [    0.138891] i2c-core: driver [max17135] using legacy resume method
    [    0.139409] SCSI subsystem initialized
    [    0.139620] libata version 3.00 loaded.
    [    0.139903] usbcore: registered new interface driver usbfs
    [    0.139963] usbcore: registered new interface driver hub
    [    0.140080] usbcore: registered new device driver usb
    [    0.140247] usbphy_nop1.10 supply vcc not found, using dummy regulator
    [    0.140348] usbphy_nop2.11 supply vcc not found, using dummy regulator
    [    0.141679] i2c i2c-0: client [ov5640_mipi] registered with bus id 0-003c
    [    0.141700] i2c i2c-0: IMX I2C adapter registered
    [    0.142625] pca953x 1-0026: failed reading register
    [    0.142644] pca953x: probe of 1-0026 failed with error -5
    [    0.142669] i2c i2c-1: client [pca9534] registered with bus id 1-0026
    [    0.142685] i2c i2c-1: IMX I2C adapter registered
    [    0.143307] i2c i2c-2: client [pfuze100] registered with bus id 2-0008
    [    0.143327] i2c i2c-2: IMX I2C adapter registered
    [    0.144025] i2c i2c-3: client [bmi160] registered with bus id 3-0068
    [    0.144612] tca8418_keypad 3-0034: tca8418_write_byte failed, reg: 1, val: 25, error: -5
    [    0.144635] i2c i2c-3: client [tca8418] registered with bus id 3-0034
    [    0.144651] i2c i2c-3: IMX I2C adapter registered
    [    0.144747] Linux video capture interface: v2.00
    [    0.144823] pps_core: LinuxPPS API ver. 1 registered
    [    0.144829] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.144849] PTP clock support registered
    [    0.160551] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
    [    0.161654] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
    [    0.161666] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
    [    0.161747] MIPI CSI2 driver module loaded
    [    0.161899] Advanced Linux Sound Architecture Driver Initialized.
    [    0.162961] Bluetooth: Core ver 2.18
    [    0.163005] NET: Registered protocol family 31
    [    0.163011] Bluetooth: HCI device and connection manager initialized
    [    0.163023] Bluetooth: HCI socket layer initialized
    [    0.163034] Bluetooth: L2CAP socket layer initialized
    [    0.163066] Bluetooth: SCO socket layer initialized
    [    0.163250] nfc: nfc_init: NFC Core ver 0.1
    [    0.163317] NET: Registered protocol family 39
    [    0.163572] Switched to clocksource mxc_timer1
    [    0.173760] NET: Registered protocol family 2
    [    0.174549] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.174595] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    [    0.174660] TCP: Hash tables configured (established 4096 bind 4096)
    [    0.174706] TCP: reno registered
    [    0.174717] UDP hash table entries: 256 (order: 1, 8192 bytes)
    [    0.174742] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    [    0.174958] NET: Registered protocol family 1
    [    0.175220] RPC: Registered named UNIX socket transport module.
    [    0.175227] RPC: Registered udp transport module.
    [    0.175231] RPC: Registered tcp transport module.
    [    0.175238] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.175677] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
    [    0.177458] Bus freq driver module loaded
    [    0.178576] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.185605] VFS: Disk quotas dquot_6.5.2
    [    0.185864] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.187716] NFS: Registering the id_resolver key type
    [    0.187767] Key type id_resolver registered
    [    0.187773] Key type id_legacy registered
    [    0.187807] jffs2: version 2.2. (NAND) \xffffffc2\xffffffa9 2001-2006 Red Hat, Inc.
    [    0.188528] fuse init (API version 7.22)
    [    0.188953] msgmni has been set to 985
    [    0.193110] io scheduler noop registered
    [    0.193119] io scheduler deadline registered
    [    0.193310] io scheduler cfq registered (default)
    [    0.193877] imx-weim 21b8000.weim: Driver registered.
    [    0.196047] MIPI DSI driver module loaded
    [    0.196702] mxc_sdc_fb fb.24: NO mxc display driver found!
    [    0.198250] imx-sdma 20ec000.sdma: no iram assigned, using external mem
    [    0.198407] imx-sdma 20ec000.sdma: no event needs to be remapped
    [    0.198569] imx-sdma 20ec000.sdma: loaded firmware 3.1
    [    0.201524] imx-sdma 20ec000.sdma: initialized
    [    0.203157] pfuze100-regulator 2-0008: Full layer: 2, Metal layer: 1
    [    0.203964] pfuze100-regulator 2-0008: FAB: 0, FIN: 0
    [    0.203975] pfuze100-regulator 2-0008: pfuze100 found.
    [    0.205889] SW1AB: 300 <--> 1875 mV at 1375 mV 
    [    0.207665] SW1C: 300 <--> 1875 mV at 1375 mV 
    [    0.208429] SW2: 800 <--> 3300 mV at 3300 mV 
    [    0.209207] SW3A: 400 <--> 1975 mV at 1500 mV 
    [    0.209961] SW3B: 400 <--> 1975 mV at 1500 mV 
    [    0.210740] SW4: 800 <--> 3300 mV at 3150 mV 
    [    0.211507] SWBST: 5000 <--> 5150 mV at 5000 mV 
    [    0.212257] VSNVS: 1000 <--> 3000 mV at 3000 mV 
    [    0.212421] VREFDDR: 750 mV 
    [    0.213171] VGEN1: 800 <--> 1550 mV at 1500 mV 
    [    0.213945] VGEN2: 800 <--> 1550 mV at 1500 mV 
    [    0.214737] VGEN3: 1800 <--> 3300 mV at 2500 mV 
    [    0.215507] VGEN4: 1800 <--> 3300 mV at 1800 mV 
    [    0.216272] VGEN5: 1800 <--> 3300 mV at 2800 mV 
    [    0.217037] VGEN6: 1800 <--> 3300 mV at 3300 mV 
    [    0.277308] Serial: IMX driver
    [    0.277645] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
    [    0.978292] console [ttymxc0] enabled
    [    0.981389] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
    [    0.989274] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
    [    0.997078] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
    [    1.004788] serial: Freescale lpuart driver
    [    1.007930] Buzzer_init
    [    1.009089] buzzer: Register character driver successfully
    [    1.014574] imx sema4 driver is registered.
    [    1.017715] [drm] Initialized drm 1.1.0 20060810
    [    1.021446] [drm] Initialized vivante 1.0.0 20120216 on minor 0
    [    1.033931] brd: module loaded
    [    1.039873] loop: module loaded
    [    1.045556] of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02008000' missing or ey
    [    1.057172] spi_imx 2008000.ecspi: cannot get the TX DMA channel!
    [    1.061976] spi_imx 2008000.ecspi: dma setup error,use pio instead
    [    1.067505] spi_drv_probe
    [    1.068841] lcd-us2066: spilcd_probe, start
    [    1.071906] lcd-us2066: spilcd_probe, LCD device created and added
    [    1.076840] lcd-us2066: spilcd_probe, LCD probed
    [    1.080177] spi_imx 2008000.ecspi: probed
    [    1.083120] of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02010000' missing or ey
    [    1.094752] spi_imx 2010000.ecspi: cannot get the TX DMA channel!
    [    1.099555] spi_imx 2010000.ecspi: dma setup error,use pio instead
    [    1.105246] imx6dl-pinctrl 20e0000.iomuxc: pin MX6DL_PAD_GPIO_18 already requested by 20e0000.iomuxc; cannot claim for spi2.0
    [    1.115330] imx6dl-pinctrl 20e0000.iomuxc: pin-135 (spi2.0) status -22
    [    1.120571] imx6dl-pinctrl 20e0000.iomuxc: could not request pin 135 (MX6DL_PAD_GPIO_18) from group trf7970-1  on device 20e0000.iomuxc
    [    1.131493] trf7970a spi2.0: Error applying setting, reverse things back
    [    1.136962] spi_drv_probe
    [    1.138299] trf7970a spi2.0: ##### TRF7970 Probe #####
    [    1.169808] spi_imx 2010000.ecspi: probed
    [    1.172799] of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02014000' missing or ey
    [    1.184429] spi_imx 2014000.ecspi: cannot get the TX DMA channel!
    [    1.189232] spi_imx 2014000.ecspi: dma setup error,use pio instead
    [    1.194696] spi_imx 2014000.ecspi: probed
    [    1.198014] CAN device driver interface
    [    1.202588] 2188000.ethernet supply phy not found, using dummy regulator
    [    1.223997] pps pps0: new PPS source ptp0
    [    1.226998] fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
    [    1.234731] fec 2188000.ethernet (unregistered net_device): Using random MAC address: e6:03:cd:94:e3:54
    [    1.246490] libphy: fec_enet_mii_bus: probed
    [    1.249978] fec 2188000.ethernet eth0: registered PHC device 0
    [    1.255300] PPP generic driver version 2.4.2
    [    1.258474] PPP BSD Compression module registered
    [    1.261886] PPP Deflate Compression module registered
    [    1.265694] hso: /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/externalsrc/kernel/drivers/net/usb/hso.c: Option Wireless
    [    1.275675] usbcore: registered new interface driver hso
    [    1.279698] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    1.284953] ehci-platform: EHCI generic platform driver
    [    1.289111] ehci-mxc: Freescale On-Chip EHCI Host driver
    [    1.293497] usbcore: registered new interface driver cdc_acm
    [    1.297910] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
    [    1.304722] usbcore: registered new interface driver usb-storage
    [    1.309479] usbcore: registered new interface driver usb_ehset_test
    [    1.315408] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
    [    1.330699] ci_hdrc ci_hdrc.1: doesn't support gadget
    [    1.334497] ci_hdrc ci_hdrc.1: EHCI Host Controller
    [    1.338103] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
    [    1.363610] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
    [    1.368507] hub 1-0:1.0: USB hub found
    [    1.370999] hub 1-0:1.0: 1 port detected
    [    1.375029] usbcore: registered new interface driver usbtouchscreen
    [    1.380718] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
    [    1.387925] i2c /dev entries driver
    [    1.390905] IR NEC protocol handler initialized
    [    1.394196] IR RC5(x) protocol handler initialized
    [    1.397691] IR RC6 protocol handler initialized
    [    1.400923] IR JVC protocol handler initialized
    [    1.404176] IR Sony protocol handler initialized
    [    1.407496] IR RC5 (streamzap) protocol handler initialized
    [    1.411770] IR SANYO protocol handler initialized
    [    1.415192] IR MCE Keyboard/mouse protocol handler initialized
    [    1.420963] i2c-core: driver [mag3110] using legacy suspend method
    [    1.425877] i2c-core: driver [mag3110] using legacy resume method
    [    1.431089] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
    [    1.438136] Bluetooth: HCI UART driver ver 2.2
    [    1.441289] Bluetooth: HCILL protocol initialized
    [    1.444911] hdev 86498000
    [    1.445440] HCI device registered (hdev 86498000)
    [    1.446029] sdhci: Secure Digital Host Controller Interface driver
    [    1.450918] sdhci: Copyright(c) Pierre Ossman
    [    1.454118] hci0 86498000
    [    1.454125] (stc): gdata/new_proto/recv or reg_complete_cb not ready
    [    1.459013] Bluetooth: st_register failed -22
    [    1.462356] usbcore: registered new interface driver ushc
    [    1.466485] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.471683] sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
    [    1.480726] mmc1: no vqmmc regulator found
    [    1.603654] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
    [    1.614390] sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
    [    1.622310] mmc2: no vqmmc regulator found
    [    1.643904] sdhci-esdhc-imx 2194000.usdhc: card claims to support voltages below defined range
    [    1.674664] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
    [    1.682267] mmc3: no vqmmc regulator found
    [    1.686205] mmc3: no vmmc regulator found
    [    1.694093] usb 1-1: new high-speed USB device number 2 using ci_hdrc
    [    1.734339] mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
    [    1.740854] galcore: clk_get vg clock failed, disable vg!
    [    1.754720] Galcore version 5.0.11.25762
    [    1.764975] PU: Power-on latency exceeded, new value 2117333 ns
    [    1.942175] cdc_acm 1-1:1.0: ttyACM0: USB ACM device
    [    2.013593] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
    [    2.026871] cdc_acm 1-1:1.2: ttyACM1: USB ACM device
    [    2.078059] cdc_acm 1-1:1.4: ttyACM2: USB ACM device
    [    2.105329] cdc_acm 1-1:1.6: ttyACM3: USB ACM device
    [    2.134316] cdc_acm 1-1:1.8: ttyACM4: USB ACM device
    [    2.214902] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
    [    2.228329] mxc_vpu 2040000.vpu: VPU initialized
    [    2.245713] mmc1: new high speed SDIO card at address 0001
    [    2.352638] mmc2: host does not support reading read-only switch. assuming write-enable.
    [    2.403588] mmc2: new high speed SDHC card at address 0007
    [    2.408246] mmcblk2: mmc2:0007 SD16G 14.4 GiB 
    [    2.470537]  mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4
    [    2.488704] caam 2100000.caam: Instantiated RNG4 SH0
    [    2.600137] mmc3: BKOPS_EN bit is not set
    [    2.686642] mmc3: new high speed DDR MMC card at address 0001
    [    2.693620] mmcblk3: mmc3:0001 M62704 3.56 GiB 
    [    2.703631] mmcblk3boot0: mmc3:0001 M62704 partition 1 2.00 MiB
    [    2.713614] mmcblk3boot1: mmc3:0001 M62704 partition 2 2.00 MiB
    [    2.723614] mmcblk3rpmb: mmc3:0001 M62704 partition 3 512 KiB
    [    2.740272] caam 2100000.caam: Instantiated RNG4 SH1
    [    2.747102] caam 2100000.caam: device ID = 0x0a160100 (Era 4)
    [    2.751658]  mmcblk3: unknown partition table
    [    2.754753] caam 2100000.caam: job rings = 2, qi = 0
    [    2.780438]  mmcblk3boot1: unknown partition table
    [    2.797023]  mmcblk3boot0: unknown partition table
    [    2.827507] caam algorithms registered in /proc/crypto
    [    2.835176] caam_jr 2101000.jr0: registering rng-caam
    [    2.839935] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
    [    2.847125] usbcore: registered new interface driver usbhid
    [    2.851406] usbhid: USB HID core driver
    [    2.854848] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    2.860172] [drm] No driver support for vblank timestamp query.
    [    2.865025] [drm] Initialized imx-drm 1.0.0 20120507 on minor 1
    [    2.870021] bmi160 3-0068: BMI160 i2c function probe entrance (new)
    [    2.875054] -------------BMI Probe Calling
    [    2.878518] bmi160 3-0068: Bosch Sensortec Device detected, HW IC name: BMI160C2
    [    2.884888] input: bmi160 as /devices/virtual/input/input0
    [    2.889290] bmi160 3-0068: bmi160 input register successfully, bmi160!
    [    2.894822] bmi160 3-0068: Invalid place parameter, use default value 0
    [    2.912554] BMI160 qpio number:175
    [    2.914712] bmi160 3-0068: BMI160 qpio number:175
    [    3.063873] bmi160 3-0068: sensor_time:65535, 65536
    [    3.067460] bmi160 3-0068: sensor bmi160 probed successfully
    [    3.071866] i2c-core: driver [bmi160] using legacy suspend method
    [    3.076686] i2c-core: driver [bmi160] using legacy resume method
    [    3.083752] fsl-asrc 2034000.asrc: driver registered
    [    3.091487] NET: Registered protocol family 26
    [    3.094722] Netfilter messages via NETLINK v0.30.
    [    3.098145] nfnl_acct: registering with nfnetlink.
    [    3.101813] ip_tables: (C) 2000-2006 Netfilter Core Team
    [    3.105883] TCP: cubic registered
    [    3.108467] NET: Registered protocol family 10
    [    3.112612] sit: IPv6 over IPv4 tunneling driver
    [    3.116714] NET: Registered protocol family 17
    [    3.119965] Bridge firewalling registered
    [    3.122687] can: controller area network core (rev 20120528 abi 9)
    [    3.127670] NET: Registered protocol family 29
    [    3.130821] can: raw protocol (rev 20120528)
    [    3.133813] can: broadcast manager protocol (rev 20120528 t)
    [    3.138187] can: netlink gateway (rev 20130117) max_hops=1
    [    3.142589] 8021q: 802.1Q VLAN Support v1.8
    [    3.145538] Key type dns_resolver registered
    [    3.149027] failed to disable 1.2 GHz OPP
    [    3.153525] SW4: disabling
    [    3.154987] usb_otg_vbus: disabling
    [    3.157193] regulator-dummy: disabling
    [    3.159965] imx mcc test is registered.
    [    3.163115] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
    [    3.181623] ALSA device list:
    [    3.183300]   No soundcards found.
    [    3.199581] EXT4-fs (mmcblk2p2): couldn't mount as ext3 due to feature incompatibilities
    [    3.213679] EXT4-fs (mmcblk2p2): couldn't mount as ext2 due to feature incompatibilities
    [    9.636675] EXT4-fs (mmcblk2p2): 1 orphan inode deleted
    [    9.640622] EXT4-fs (mmcblk2p2): recovery complete
    [    9.872562] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)
    [    9.879538] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    9.884543] devtmpfs: mounted
    [    9.886863] Freeing unused kernel memory: 336K (80d08000 - 80d5c000)
    [   10.921235] EXT4-fs (mmcblk2p7): warning: mounting fs with errors, running e2fsck is recommended
    [   10.952608] EXT4-fs (mmcblk2p7): recovery complete
    [   10.980868] EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
    [   10.995592] EXT4-fs (mmcblk2p8): VFS: Can't find ext4 filesystem
    [   12.339473] udevd[194]: starting version 182
    [   12.851019] random: nonblocking pool is initialized
    [   13.332300] evbug: Connected device: input0 (bmi160 at unknown)
    [   13.426709] cdc_ether 1-1:1.10 eth1: register 'cdc_ether' at usb-ci_hdrc.1-1, CDC Ethernet Device, 00:00:11:12:13:14
    [   13.454187] cdc_ether 1-1:1.12 eth2: register 'cdc_ether' at usb-ci_hdrc.1-1, CDC Ethernet Device, 00:00:11:12:13:16
    [   13.482298] usbcore: registered new interface driver cdc_ether
    [   13.693734] camera ov5640_mipi is found
    [   14.290842] EXT4-fs (mmcblk2p2): re-mounted. Opts: (null)
    [   16.692842] Loading modules backported from Linux version R8.7_SP1-0-g13c25bc
    [   16.701035] Backport generated by backports.git R8.7_SP1-0-gd4777ef
    [   18.377829] func->num issue 1 
    [   18.536778] wl18xx_driver wl18xx.0.auto: Direct firmware load failed with error -2
    [   18.543059] wl18xx_driver wl18xx.0.auto: Falling back to user helper
    [   18.834514] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
    [   18.879875] wlcore: loaded
    [   18.881308] wlcore: driver version: ol_r8.a9.22
    [   19.054358] fec 2188000.ethernet eth0: Freescale FEC PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=2188000.ethernet:02, irq=-1)
    [   19.065556] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [   22.268927] v4l2loopback driver version 0.10.0 loaded
    [   23.054253] libphy: 2188000.ethernet:02 - Link is Up - 1000/Full
    [   23.397440] wlcore: PHY firmware version: Rev 8.2.0.0.237
    [   23.992408] wlcore: firmware booted (Rev 8.9.0.0.70)
    [   24.509558] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
    [   24.526192] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [   24.871741] spi_drv_probe
    [   24.873077] zl380tw spi3.0: probing zl380tw spi device
    [   24.876039] SPI slave device found at bus::cs = 3::0
    [   24.879725] zl380tw spi3.0: zl380tw codec device created...
    [   24.898676] snd_microsemi_dac_probe :117 HERE...
    [   24.902060] clk_frequency = 66000000
    [   24.911184] zl380tw spi3.0: Probing zl380tw SoC CODEC driver
    [   24.920983] snd-microsemi-dac sound.23: zl380tw0-hifi <-> 2028000.ssi mapping ok
    [   25.044096] snd_soc_register_card success
    [   26.121273] status 0 of zl380tw_io_open
    [   26.274132] status 0 of zl380tw_io_open
    [   27.150734] status 0 of zl380tw_io_open
    [   27.154806] status 0 of zl380tw_io_open
    [   27.695759] status 0 of zl380tw_io_open
    [   27.705429] status 0 of zl380tw_io_open
    [   35.353694] ERROR: unrecognized std! 0 (PAL=ff, NTSC=b000
    [   44.822442] bmi_stepdetector_interrupt_handle
    [   44.879388] wiegand initialising
    [   44.881330] wiegand ready
    [   44.964771] Wiegand configuration 
    [   44.970547] Wiegandstatus 1 , index 0, bitcnt 26
    [   44.976289] Wiegand configuration 
    [   44.986571] Wiegandstatus 1 , index 0, bitcnt 26
    [   46.199359] FAT-fs (mmcblk2p4)
    

    45780 bytes read in 20 ms (2.2 MiB/s)
    ## Booting kernel from Legacy Image at 12000000 ...
       Image Name:   Linux-3.14.28_1.0.0_ga-eliuaccs
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    5868128 Bytes = 5.6 MiB
       Load Address: 10008000
       Entry Point:  10008000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 18000000
       Booting using the fdt blob at 0x18000000
       Loading Kernel Image ... OK
       Using Device Tree in place at 18000000, end 1800e2d3
    
    Starting kernel ...
    
    Uncompressing Linux... done, booting the kernel.
    Booting Linux on physical CPU 0x0
    Linux version 3.14.28_1.0.0_ga-eliuaccs (vvdnlt230@vvdnlt230-Latitude-3540) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Fri Sep 29 18:56:07 IST 7
    CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine model: Wandboard i.MX6 Dual Lite Board
    cma: CMA: reserved 320 MiB at 1c000000
    Memory policy: Data cache writeback
    CPU: All CPU(s) started in SVC mode.
    PERCPU: Embedded 8 pages/cpu @8bb33000 s8896 r8192 d15680 u32768
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 176748K/524288K available (7115K kernel code, 404K rwdata, 6192K rodata, 336K init, 431K bss, 347540K reserved, 0K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
        lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
        pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
        modules : 0x7f000000 - 0x7fe00000   (  14 MB)
          .text : 0x80008000 - 0x80d07150   (13309 kB)
          .init : 0x80d08000 - 0x80d5c2c0   ( 337 kB)
          .data : 0x80d5e000 - 0x80dc31a0   ( 405 kB)
           .bss : 0x80dc31fc - 0x80e2f1a4   ( 432 kB)
    SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    Preemptible hierarchical RCU implementation.
            RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS:16 nr_irqs:16 16
    L310 cache controller enabled
    l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32450000, Cache size: 512 kB
    failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22
    Switching to timer-based delay loop
    sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x106c4360 - 0x106c43b8
    CPU1: failed to boot: -38
    Brought up 1 CPUs
    SMP: Total of 1 processors activated.
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    pinctrl core: initialized pinctrl subsystem
    regulator-dummy: no parameters
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    cpuidle: using governor menu
    CPU identified as i.MX6DL, silicon rev 1.3
    Use WDOG1 as reset source
    syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
    vdd1p1: 800 <--> 1375 mV at 1100 mV 
    vdd3p0: 2800 <--> 3150 mV at 3000 mV 
    vdd2p5: 2000 <--> 2750 mV at 2400 mV 
    vddarm: 725 <--> 1450 mV at 1150 mV 
    vddpu: 725 <--> 1450 mV at 1150 mV 
    vddsoc: 725 <--> 1450 mV at 1175 mV 
    syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
    syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
    bio: create slab <bio-0> at 0
    mxs-dma 110000.dma-apbh: initialized
    wilink_wl_en: 1800 mV 
    1P8V: 1800 mV 
    2P5V: 2500 mV 
    3P3V: 3300 mV 
    usb_h1_vbus: 5000 mV 
    usb_otg_vbus: 5000 mV 
    i2c-core: driver [max17135] using legacy suspend method
    i2c-core: driver [max17135] using legacy resume method
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    usbphy_nop1.10 supply vcc not found, using dummy regulator
    usbphy_nop2.11 supply vcc not found, using dummy regulator
    i2c i2c-0: client [ov5640_mipi] registered with bus id 0-003c
    i2c i2c-0: IMX I2C adapter registered
    pca953x 1-0026: failed reading register
    pca953x: probe of 1-0026 failed with error -5
    i2c i2c-1: client [pca9534] registered with bus id 1-0026
    i2c i2c-1: IMX I2C adapter registered
    i2c i2c-2: client [pfuze100] registered with bus id 2-0008
    i2c i2c-2: IMX I2C adapter registered
    i2c i2c-3: client [bmi160] registered with bus id 3-0068
    tca8418_keypad 3-0034: tca8418_write_byte failed, reg: 1, val: 25, error: -5
    i2c i2c-3: client [tca8418] registered with bus id 3-0034
    i2c i2c-3: IMX I2C adapter registered
    Linux video capture interface: v2.00
    pps_core: LinuxPPS API ver. 1 registered
    pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    PTP clock support registered
    imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
    mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
    mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
    MIPI CSI2 driver module loaded
    Advanced Linux Sound Architecture Driver Initialized.
    Bluetooth: Core ver 2.18
    NET: Registered protocol family 31
    Bluetooth: HCI device and connection manager initialized
    Bluetooth: HCI socket layer initialized
    Bluetooth: L2CAP socket layer initialized
    Bluetooth: SCO socket layer initialized
    nfc: nfc_init: NFC Core ver 0.1
    NET: Registered protocol family 39
    Switched to clocksource mxc_timer1
    NET: Registered protocol family 2
    TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP: reno registered
    UDP hash table entries: 256 (order: 1, 8192 bytes)
    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    NET: Registered protocol family 1
    RPC: Registered named UNIX socket transport module.
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
    Bus freq driver module loaded
    futex hash table entries: 512 (order: 3, 32768 bytes)
    VFS: Disk quotas dquot_6.5.2
    Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    NFS: Registering the id_resolver key type
    Key type id_resolver registered
    Key type id_legacy registered
    jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    fuse init (API version 7.22)
    msgmni has been set to 985
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    imx-weim 21b8000.weim: Driver registered.
    MIPI DSI driver module loaded
    mxc_sdc_fb fb.24: NO mxc display driver found!
    imx-sdma 20ec000.sdma: no iram assigned, using external mem
    imx-sdma 20ec000.sdma: no event needs to be remapped
    imx-sdma 20ec000.sdma: loaded firmware 3.1
    imx-sdma 20ec000.sdma: initialized
    pfuze100-regulator 2-0008: Full layer: 2, Metal layer: 1
    pfuze100-regulator 2-0008: FAB: 0, FIN: 0
    pfuze100-regulator 2-0008: pfuze100 found.
    SW1AB: 300 <--> 1875 mV at 1375 mV 
    SW1C: 300 <--> 1875 mV at 1375 mV 
    SW2: 800 <--> 3300 mV at 3300 mV 
    SW3A: 400 <--> 1975 mV at 1500 mV 
    SW3B: 400 <--> 1975 mV at 1500 mV 
    SW4: 800 <--> 3300 mV at 3150 mV 
    SWBST: 5000 <--> 5150 mV at 5000 mV 
    VSNVS: 1000 <--> 3000 mV at 3000 mV 
    VREFDDR: 750 mV 
    VGEN1: 800 <--> 1550 mV at 1500 mV 
    VGEN2: 800 <--> 1550 mV at 1500 mV 
    VGEN3: 1800 <--> 3300 mV at 2500 mV 
    VGEN4: 1800 <--> 3300 mV at 1800 mV 
    VGEN5: 1800 <--> 3300 mV at 2800 mV 
    VGEN6: 1800 <--> 3300 mV at 3300 mV 
    Serial: IMX driver
    2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
    console [ttymxc0] enabled
    21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
    21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
    21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
    serial: Freescale lpuart driver
    Buzzer_init
    buzzer: Register character driver successfully
    imx sema4 driver is registered.
    [drm] Initialized drm 1.1.0 20060810
    [drm] Initialized vivante 1.0.0 20120216 on minor 0
    brd: module loaded
    loop: module loaded
    of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02008000' missing or empty
    spi_imx 2008000.ecspi: cannot get the TX DMA channel!
    spi_imx 2008000.ecspi: dma setup error,use pio instead
    spi_drv_probe
    lcd-us2066: spilcd_probe, start
    lcd-us2066: spilcd_probe, LCD device created and added
    lcd-us2066: spilcd_probe, LCD probed
    spi_imx 2008000.ecspi: probed
    of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02010000' missing or empty
    spi_imx 2010000.ecspi: cannot get the TX DMA channel!
    spi_imx 2010000.ecspi: dma setup error,use pio instead
    imx6dl-pinctrl 20e0000.iomuxc: pin MX6DL_PAD_GPIO_18 already requested by 20e0000.iomuxc; cannot claim for spi2.0
    imx6dl-pinctrl 20e0000.iomuxc: pin-135 (spi2.0) status -22
    imx6dl-pinctrl 20e0000.iomuxc: could not request pin 135 (MX6DL_PAD_GPIO_18) from group trf7970-1  on device 20e0000.iomuxc
    trf7970a spi2.0: Error applying setting, reverse things back
    spi_drv_probe
    trf7970a spi2.0: ##### TRF7970 Probe #####
    spi_imx 2010000.ecspi: probed
    of_dma_request_slave_channel: dma-names property of node '/soc/aips-bus@02000000/spba-bus@02000000/ecspi@02014000' missing or empty
    spi_imx 2014000.ecspi: cannot get the TX DMA channel!
    spi_imx 2014000.ecspi: dma setup error,use pio instead
    spi_imx 2014000.ecspi: probed
    CAN device driver interface
    2188000.ethernet supply phy not found, using dummy regulator
    pps pps0: new PPS source ptp0
    fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
    fec 2188000.ethernet (unregistered net_device): Using random MAC address: e6:03:cd:94:e3:54
    libphy: fec_enet_mii_bus: probed
    fec 2188000.ethernet eth0: registered PHC device 0
    PPP generic driver version 2.4.2
    PPP BSD Compression module registered
    PPP Deflate Compression module registered
    hso: /home/vvdnlt230/vvdn_all/ELIU_ACCS/eliu_accs/src/externalsrc/kernel/drivers/net/usb/hso.c: Option Wireless
    usbcore: registered new interface driver hso
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-platform: EHCI generic platform driver
    ehci-mxc: Freescale On-Chip EHCI Host driver
    usbcore: registered new interface driver cdc_acm
    cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
    usbcore: registered new interface driver usb-storage
    usbcore: registered new interface driver usb_ehset_test
    2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
    ci_hdrc ci_hdrc.1: doesn't support gadget
    ci_hdrc ci_hdrc.1: EHCI Host Controller
    ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    usbcore: registered new interface driver usbtouchscreen
    snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
    i2c /dev entries driver
    IR NEC protocol handler initialized
    IR RC5(x) protocol handler initialized
    IR RC6 protocol handler initialized
    IR JVC protocol handler initialized
    IR Sony protocol handler initialized
    IR RC5 (streamzap) protocol handler initialized
    IR SANYO protocol handler initialized
    IR MCE Keyboard/mouse protocol handler initialized
    i2c-core: driver [mag3110] using legacy suspend method
    i2c-core: driver [mag3110] using legacy resume method
    imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
    Bluetooth: HCI UART driver ver 2.2
    Bluetooth: HCILL protocol initialized
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    (stc): gdata/new_proto/recv or reg_complete_cb not ready
    Bluetooth: st_register failed -22
    usbcore: registered new interface driver ushc
    sdhci-pltfm: SDHCI platform and OF driver helper
    sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
    mmc1: no vqmmc regulator found
    mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
    sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
    mmc2: no vqmmc regulator found
    sdhci-esdhc-imx 2194000.usdhc: card claims to support voltages below defined range
    mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
    mmc3: no vqmmc regulator found
    mmc3: no vmmc regulator found
    usb 1-1: new high-speed USB device number 2 using ci_hdrc
    mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
    galcore: clk_get vg clock failed, disable vg!
    Galcore version 5.0.11.25762
    PU: Power-on latency exceeded, new value 2117333 ns
    cdc_acm 1-1:1.0: ttyACM0: USB ACM device
    mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
    cdc_acm 1-1:1.2: ttyACM1: USB ACM device
    cdc_acm 1-1:1.4: ttyACM2: USB ACM device
    cdc_acm 1-1:1.6: ttyACM3: USB ACM device
    cdc_acm 1-1:1.8: ttyACM4: USB ACM device
    mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
    mxc_vpu 2040000.vpu: VPU initialized
    mmc1: new high speed SDIO card at address 0001
    mmc2: host does not support reading read-only switch. assuming write-enable.
    mmc2: new high speed SDHC card at address 0007
    mmcblk2: mmc2:0007 SD16G 14.4 GiB 
     mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4
    caam 2100000.caam: Instantiated RNG4 SH0
    mmc3: BKOPS_EN bit is not set
    mmc3: new high speed DDR MMC card at address 0001
    mmcblk3: mmc3:0001 M62704 3.56 GiB 
    mmcblk3boot0: mmc3:0001 M62704 partition 1 2.00 MiB
    mmcblk3boot1: mmc3:0001 M62704 partition 2 2.00 MiB
    mmcblk3rpmb: mmc3:0001 M62704 partition 3 512 KiB
    caam 2100000.caam: Instantiated RNG4 SH1
    caam 2100000.caam: device ID = 0x0a160100 (Era 4)
     mmcblk3: unknown partition table
    caam 2100000.caam: job rings = 2, qi = 0
     mmcblk3boot1: unknown partition table
     mmcblk3boot0: unknown partition table
    caam algorithms registered in /proc/crypto
    caam_jr 2101000.jr0: registering rng-caam
    snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [drm] No driver support for vblank timestamp query.
    [drm] Initialized imx-drm 1.0.0 20120507 on minor 1
    bmi160 3-0068: BMI160 i2c function probe entrance (new)
    -------------BMI Probe Calling
    bmi160 3-0068: Bosch Sensortec Device detected, HW IC name: BMI160C2
    input: bmi160 as /devices/virtual/input/input0
    bmi160 3-0068: bmi160 input register successfully, bmi160!
    bmi160 3-0068: Invalid place parameter, use default value 0
    BMI160 qpio number:175
    bmi160 3-0068: BMI160 qpio number:175
    bmi160 3-0068: sensor_time:65535, 65536
    bmi160 3-0068: sensor bmi160 probed successfully
    i2c-core: driver [bmi160] using legacy suspend method
    i2c-core: driver [bmi160] using legacy resume method
    fsl-asrc 2034000.asrc: driver registered
    NET: Registered protocol family 26
    Netfilter messages via NETLINK v0.30.
    nfnl_acct: registering with nfnetlink.
    ip_tables: (C) 2000-2006 Netfilter Core Team
    TCP: cubic registered
    NET: Registered protocol family 10
    sit: IPv6 over IPv4 tunneling driver
    NET: Registered protocol family 17
    Bridge firewalling registered
    can: controller area network core (rev 20120528 abi 9)
    NET: Registered protocol family 29
    can: raw protocol (rev 20120528)
    can: broadcast manager protocol (rev 20120528 t)
    can: netlink gateway (rev 20130117) max_hops=1
    8021q: 802.1Q VLAN Support v1.8
    Key type dns_resolver registered
    failed to disable 1.2 GHz OPP
    SW4: disabling
    usb_otg_vbus: disabling
    regulator-dummy: disabling
    imx mcc test is registered.
    snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
    ALSA device list:
      No soundcards found.
    EXT4-fs (mmcblk2p2): couldn't mount as ext3 due to feature incompatibilities
    EXT4-fs (mmcblk2p2): couldn't mount as ext2 due to feature incompatibilities
    EXT4-fs (mmcblk2p2): 1 orphan inode deleted
    EXT4-fs (mmcblk2p2): recovery complete
    EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing unused kernel memory: 336K (80d08000 - 80d5c000)
    INIT: version 2.88 booting
    EXT4-fs (mmcblk2p7): warning: mounting fs with errors, running e2fsck is recommended
    EXT4-fs (mmcblk2p7): recovery complete
    EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
    EXT4-fs (mmcblk2p8): VFS: Can't find ext4 filesystem
    UIM SYSFS Node Not Found
    Starting udev
    udevd[194]: starting version 182
    random: nonblocking pool is initialized
    cdc_ether 1-1:1.10 eth1: register 'cdc_ether' at usb-ci_hdrc.1-1, CDC Ethernet Device, 00:00:11:12:13:14
    cdc_ether 1-1:1.12 eth2: register 'cdc_ether' at usb-ci_hdrc.1-1, CDC Ethernet Device, 00:00:11:12:13:16
    usbcore: registered new interface driver cdc_ether
    camera ov5640_mipi is found
    EXT4-fs (mmcblk2p2): re-mounted. Opts: (null)
    
    udevadm settle - timeout of 3 seconds reached, the event queue contains:
      /sys/devices/soc0/soc.0/2100000.aips-bus/2198000.usdhc/mmc_host/mmc2/mmc2:0007/block/mmcblk2/mmcblk2p8 (1765)
    ALSA: Restoring mixer settings...
    /usr/sbin/alsactl: load_state:1735: No soundcards found...
    Fri Sep 29 18:18:36 UTC 2017
    Loading modules backported from Linux version R8.7_SP1-0-g13c25bc
    Backport generated by backports.git R8.7_SP1-0-gd4777ef
    func->num issue 1 
    wl18xx_driver wl18xx.0.auto: Direct firmware load failed with error -2
    wl18xx_driver wl18xx.0.auto: Falling back to user helper
    INIT: Entering runlevel: 5
    Mac adreess of the device is 80:30:DC:05:4C:B3
    Configuring network interfaces... wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
    wlcore: loaded
    wlcore: driver version: ol_r8.a9.22
    fec 2188000.ethernet eth0: Freescale FEC PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=2188000.ethernet:02, irq=-1)
    IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    done.
    Starting system message bus: Starting Xserver
    open /dev/fb0: No such file or directory
    Unknown username "xuser" in message bus configuration file
    dbus.
    Starting Connection Manager
    Starting OpenBSD Secure Shell server: sshd
    done.
    Starting rpcbind daemon...done.
    Starting advanced power management daemon: No APM support in kernel
    (failed.)
    Starting syslogd/klogd: done
    v4l2loopback driver version 0.10.0 loaded
    Starting internet superserver: xinetd.
     * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon
    libphy: 2188000.ethernet:02 - Link is Up - 1000/Full
    wlcore: PHY firmware version: Rev 8.2.0.0.237
    wlcore: firmware booted (Rev 8.9.0.0.70)
    IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
    [ ok ]ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    Starting Telephony daemon
    Loading Modules
    spi_drv_probe
    SPI slave device found at bus::cs = 3::0
    snd_microsemi_dac_probe :117 HERE...
    clk_frequency = 66000000
    zl380tw spi3.0: Probing zl380tw SoC CODEC driver
    snd-microsemi-dac sound.23: zl380tw0-hifi <-> 2028000.ssi mapping ok
    snd_soc_register_card success
    Loaded Modules....
    Loading Modules... Done!
    Booting Codec
    device file =/dev/zl380tw.0
    Device reset completed successfully...
    
    :tw_ldfwcfg 0 /opt/zl40/zl40fwr.s3 /opt/zl40/zl40cfg.cr2
    device file =/dev/zl380tw.0
    1- Opening firmware file - done....
    -- Boot prepare - done....
    -- Firmware data transfer - done....
    3- Loading the config file into the device RAM
    a- Reading config file to host RAM - done....
    Device boot loading completed successfully...
    device file =/dev/zl380tw.0
    wr: addr 0x030a = 0x0068
    
    device file =/dev/zl380tw.0
    wr: addr 0x030c = 0x0f10
    
    Codec Booted... Done!
    Starting Linux NFC daemon
    Error resolving pool.ntp.org: Name or service not known (-2)
     1 Jan 00:00:25 ntpdate[491]: Can't find host pool.ntp.org: Name or service not known (-2)
     1 Jan 00:00:25 ntpdate[491]: no servers can be used, exiting
    [Access Service App] Queue created LCD=4
    [Access Service App] Q created mq=5
    [Access Service App] Initializing Access_control DB
    [Access Service App] Initializing database
    TABLE  = accessScheduleTable 
    TABLE  = bleAccessTable 
    TABLE  = cameraIPMappingTable 
    TABLE  = doorRelayMappingTable 
    TABLE  = keypadAccessTable 
    TABLE  = keypadAccessModeTable 
    TABLE  = nfcAccessTable 
    TABLE  = phoneAccessTable 
    TABLE  = rfidAccessTable 
    TABLE  = userStatusTable 
    TABLE  = contactProfileInfoTable 
    TABLE  = wiegandAccessTable 
    TABLE  = latchCodeTable 
    TABLE  = keypadAccessModeDeleteTrigger 
    TABLE  = keypadAccessModeInsertTrigger 
    TABLE  = keypadAccessModeUpdateTrigger 
    TABLE  = phoneAccessModeDeleteTrigger 
    TABLE  = phoneAccessModeInsertTrigger 
    TABLE  = phoneAccessModeUpdateTrigger 
    [Access Service App] Initialization of ACCESS CONTROL DB complete
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x763e0000
    Create Queue: [0]
    Queue ID: 0
    c Queue Created Successfully [CALL_TIMEOUT]
    Create Queue: [32769]
    Queue ID: 32769
    Create Queue: [65538]
    Queue ID: 65538
    Create Queue: [98307]
    Queue ID: 98307
    Create Queue: [131076]
    Queue ID: 131076
    Create Queue: [163845]
    Queue ID: 163845
    Create Queue: [196614]
    Queue ID: 196614
    Create Queue: [229383]
    Queue ID: 229383
    Create Queue: [262152]
    Queue ID: 262152
    Create Queue: [294921]
    Queue ID: 294921
    
    
    WDM Library : Register with WDM
    WDM Library : "493.access-service-app.20" Sent[Access Service App] Init Response Queue [From Baresip]
    
    [Access Service App] Received message on the response Queue From Baresip
    [AccessServiceApp] Offset in Seconds 0
    [Access Service App] Register with the Bare Sip Client
    [Access Service App] Printing the SIP Credentials
    [Access Service App] Sip Username : 
    [Access Service App] Sip Pasword : 
    [Access Service App] Sip Domain : 
    [AccessServiceApp] Setting Volume to : 2
    device file =/dev/zl380tw.0
    wr: addr 0x030a = 0x0002
    
    [AccessServiceApp] Setting Mic Sensitivity to : 2
    device file =/dev/zl380tw.0
    wr: addr 0x030c = 0x0210
    
    *****************************************************
    *********** Elika Access Systems Test Rel - 1.0.1.296************
    *****************************************************
    
    IO Manger is Started Successfully
    error 
    sh: line 0: echo: write error: No such device
    Queue ID: 65538
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x768b4000
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x76608000
    Memory attached: 0x76608000
    PID: 505
    VGA resolution set[INFO]        Product Info: i.MX6Q/D/S
    ERROR: unrecognized std! 0 (PAL=ff, NTSC=b000
    'video_main_pipeline' state changed from NULL to READY. 
    'video_main_pipeline' state changed from READY to PAUSED. 
    [INFO]  ringBufferEnable 0, chromaInterleave 0, mapType 0, linear2TiledEnable 0
    [WARN]  VPU iram is less than needed, some parts don't use iram
    'video_main_pipeline' state changed from PAUSED to PLAYING. 
    als init success
    LIVE555 Proxy Server
            (LIVE555 Streaming Media library version 2017.01.26; licensed under the GNU LGPL)
    
    (We handle incoming "REGISTER" requests on port 8000)
    
    (We use port 80 for optional RTSP-over-HTTP tunneling.)
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x7634f000
    Memory attached: 0x7634f000
    PID: 518
    vga resolution
    stream ready at rtsp://127.0.0.1:8554/primary
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x768c5000
    Memory attached: 0x768c5000
    PID: 522
    Executing Baresip Script.....
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x76954000
    buzzerControl-app[main]:Init succesfull 
    Queue ID: 294921
    buzzerControl-app[main]:BUZZER_CTRL_QUEUE initilised
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x76903000
    [KeypadManager] Openeing Queue is Success
    Queue ID: 294921
    Q created mq=5
    [KeypadManager] Can't open LCD
    Queue ID: 262152
    Queue ID: 32769
    mount: can't find /mnt/ota/ in /etc/fstab
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x76906000
    Queue ID: 262152
    Queue ID: 229383
    Queue ID: 294921
    bmi_stepdetector_interrupt_handle
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x7651c000
    Queue ID: 229383
    Queue ID: 262152
    Queue ID: 0
    
    
    WDM Library : Register with WDM
    wiegand initialising
    wiegand ready
    OTA Manager Version 1.0.4
    Create Queue: [393228]
    Queue ID: 393228
    Message ID: 393228
    Queue ID: 262152
    Q created mq=3
    >> OTAevent_msgId : 262152
    
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory AddrWiegand configuration 
    ess: 0x76953000
    Queue ID: 32769Wiegandstatus 1 , index 0, bitcnt 26
    
    
    
    WDM Library : Register wWiegand configuration 
    ith WDM
    WDM Library : "545.wiegand-manager-app.20" SentWiegand input 1 Thread created
    Wiegand iWiegandstatus 1 , index 0, bitcnt 26
    nput 2 Thread created
    Mac adreess of the device is 80:30:DC:05:4C:B3
    Starting autohdmi: 
    Q created mq=3
    Smart Access Manager - Version 1_0_3
    killall: SS1BTPM: no process killed
    
    Poky (Yocto Project Reference Distro) 1.8.1 eliuaccs-dual /dev/ttymxc0
    
    eliuaccs-dual login: FAT-fs (mmcblk2p4): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
     >> Inside Primary
    cat: can't open '/mnt/ota/ota_flag': No such file or directory
    cat: can't open '/mnt/ota/ota_flag': No such file or directory
    otaUpdateEventBuf.eventTime = 44 
    otaUpdateEventBuf.upgradeStatus = 1 
    otaUpdateEventBuf.swVersion = 1.0.1.296
     
    otaUpdateEventBuf.hwVersion = 1.0.1
     
     >> Sent data on EventQueue: 
    
    nfc-manager[main]:NFC initilised
    Start polling on nfc0 as initiator
    
    Shared memory size [4915200]
    Shared memory ID: [0]
    Shared Memory ID: 0
    Share Memory Address: 0x746fe000
    Memory attached: 0x746fe000
    PID: 523
    Moton detection disabled
    Queue ID: 32769
    Queue ID: 98307
    Initializing the Elika Bluetopia
    BTPM_Initialize() Success: 0.
    DEVM_RegisterEventCallback() Success: 5.
    echo 26 > /sys/class/gpio/export
    echo out > /sys/class/gpio/gpio26/direction
    echo 0 > /sys/class/gpio/gpio26/value
    echo 1 > /sys/class/gpio/gpio26/value
    echo 0 > /sys/class/gpio/gpio26/value
    echo 1 > /sys/class/gpio/gpio26/value
    
    Poky (Yocto Project Reference Distro) 1.8.1 eliuaccs-dual /dev/ttymxc0
    
    eliuaccs-dual login: