This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: Max Receive Power

Part Number: CC3200

Hi all,

We are working on an RF front end for the CC3200. I wanted to know what the MAX RF Input power is for the device. The data sheet states that it handles -4 dBm for 802.11b  and -10 dBm for 802.11g. I see that these values are the threshold for a 10% PER. 

I'm not really interested in performance for this question, just want to know the maximum power input that the CC3200 can handle before the components are damaged. 

Can the CC3200 handle 0 dBm without damaging the receiver? 10 dBm? 

Thanks in advance.

-Jason