This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220S-LAUNCHXL: How to connect a I2S MEMS microphone

Part Number: CC3220S-LAUNCHXL
Other Parts Discussed in Thread: CC3220S,

Hello,
I am currently working on a new design using the CC3220S.
One of the tasks I wish to implement is to measure sound volume levels of a single MEMS microphone.
The CC3220S datasheet documents there is a I2S peripheral interface,
and I was wondering if it can be used to interface with for instance a ICS-43434.
Which pins of the McASP/I2S pins should be connected ?
Are there some examples available ?

I also have a CC3220S-LAUNCHXL board which I would like use for testing...


Best regards,
Salvatore