Other Parts Discussed in Thread: WL18XX-BT-SP
Hi,
I am using TI firmware BTS 11.8.32 and the corresponding xml for BT initialization.
When I try to run the BT BER test as given in the section (BER Test - Between Two Wilink Devices) in the following link
using HCITester.
I get an error, expected 0x7 recieved 0x11
and unknown HCI command error.
Can you please let me know what I am doing wrong in BER test ?
17:53:51.594 ERROR - Packet Size. Got: 7 (0x07), Expected: 25 (0x19) |
17:53:51.604 ERROR - File: "D:\CE_Testing\bt_perf_test\Rx_mode.txt", Line: 15 |
17:53:51.604 ERROR - Status mismatch. Expected: 0x00, Got: 0x01 (Unknown HCI Command) |
17:53:51.604 ERRORed Line (15): Wait_HCI_Command_Complete_VS_DRP_Read_BER_Meter_Status_Event 5000, any, HCI_VS_DRP_Read_BER_Meter_Status, 0x00, &synched, &finished, any, &total_bits, &bit_errors, &packets |
17:53:51.604 --
|