Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120BOOST: SW2 and SW3 swapped in CC3120BOOST User's Guide (Table 1 in section 2.3.1)

Part Number: CC3120BOOST

It appears that the User's Guide for CC3120BOOST (document SWRU457) has the SW2 and SW3 functionality swapped in Table 1. It says SW2 will reset the device and SW3 will put the device to the boot loader mode for flashing the firmware. In reality these two descriptions are swapped. Also SW2 and SW3 markings on the silk screen image of the board shown on page 4 of the document do not match the silk screen on the real board, at least on Rev A of the real board.

  • Hi Oray,

    Thanks, we're currently making these changes. We previously had different revisions of the LaunchPads with alternate silk screens, and we're updating the User's Guides and demos accordingly for the released version.

    Best regards,
    Sarah