Part Number: WL1807MOD
Hello
Could you help me respond to my customer on issues during SI sign off process, were they found problems with the Pins (DS0 and DS1) configuration.
They tell me :-
Below are the WiFi SI simulation review feedback
- For Write mode, 12mA, slow drive strength is selected for Ultrascale FPGA and the series termination resistor value (R8 and RN21) needs to be changed to 47 ohms. With this change, we could able to pass the SI for the write mode.
- For Read mode, the below highlighted model (BQ18PROGFBPB_H10_PUPDOFF_1P8) is selected for the WL1807 Wifi Transceiver device. With this model, we could able to pass the SI for the Read mode.
In summary the Top Model highlighted in Blue Fails but the one Highlighted in Yellow Fails>
Customer believes this is due to DSO and DS1 signals so could we confirm this and let us know what are the differences between these models.
Thanks
Bob Bacon