This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: Is it possible to read file from CC3220SF external flash back to PC with UniFlash 4.2 CLI dslite?

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF, UNIFLASH, CC3200

Hello.

After file system is written to CC3220SF external flash with UniFlash 4.2, is it possible to read files from flash back to PC with UniFlash 4.2 command line "dslite"? We don't use security for file encryption. For the files listed in UniFlash GUI, I would expect to be able to read them back. However, I could not find the commands to do that. Can it be done?

I used to do that with UniFlash 3.4 with CC3200.

Thanks in advance,

Al