This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Probe issue of the wifi module wl1271

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: WL1271

Tool/software: Linux

I'm trying to integrate the wifi module WL1271L with am335x using TI processor SDK with its kernel version processor-sdk-linux-04.00.00

It appears to me that the required driver and firmware are already installed by TI SDK on the rootfs and I only have to configure the DTB, right?

I have configured the DTB as the following:

&mmc2 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mmc2_wifi_pins_default>;
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
max-frequency = <25000000>;
ti,needs-special-hs-handling;
cap-power-off-card;
keep-power-in-suspend;

#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@0 {
status = "okay";
compatible = "ti,wl1271";
reg = <1>;
interrupt-parent = <&gpio3>;
interrupts = <17 IRQ_TYPE_LEVEL_HIGH>;

};
};

But when I try to enable the wifi module, I got the following error from kernel (dynamic debug is enabled on some module):

[ 163.275106] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 163.319464] mmc1: new SDIO card at address 0001
[ 163.333269] driver_probe_device: bus: 'mmc': driver_probe_device: matched device mmc1:0001 with driver mmcblk
[ 163.353238] really_probe: bus: 'mmc': really_probe: probing driver mmcblk with device mmc1:0001
[ 163.378706] really_probe: mmcblk: probe of mmc1:0001 rejects match -19
[ 163.505993] driver_probe_device: bus: 'sdio': driver_probe_device: matched device mmc1:0001:1 with driver wl1271_sdio
[ 163.521800] really_probe: bus: 'sdio': really_probe: probing driver wl1271_sdio with device mmc1:0001:1
[ 163.537058] really_probe: wl1271_sdio: probe of mmc1:0001:1 rejects match -19
[ 163.544326] driver_probe_device: bus: 'sdio': driver_probe_device: matched device mmc1:0001:2 with driver wl1271_sdio
[ 163.559967] really_probe: bus: 'sdio': really_probe: probing driver wl1271_sdio with device mmc1:0001:2
[ 163.572050] really_probe: wl1271_sdio: probe of mmc1:0001:2 rejects match -19

In wlcore_probe_of probe function, of_match_node return null and doesn't much any device.

Any Help?

Thanks,