This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: Uniflash cannot find the device

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF, UNIFLASH

After some months I'm back again on a project based on CC3220SF. First, with the LP I can use both JTAG and serial (Uniflash).
Then I have my own custom board, already tested a couple of months ago. The only difference is I had to clean my PC and reinstall all again. Hence I guess my issue is related to some configuration.

The problem is Uniflash cannot connect to my board: it says timeout reading data or sometimes timeout while waiting ack.

I did the following:

  1. removed all jumpers from the LP
  2. connected the rx/tx from XDS (the two pins above the headers) to my board
  3. connected gnd, reset and also the JTAG pins (in fact I can debug my application)
  4. the SOP pins are: pull-down, pull-up, pull-down

To be sure I tried to swap the tx/rx lines.

What do you suggest to dig deeper in this issue?