Part Number: CC3220
Tool/software: Code Composer Studio
Q1. I am unable to install CC3220 SDK on 64-bit linux machine. Where can i get the SDK for 64-bit linux?
Q2. If, somehow, I install the CC3220 SDK on 32-bit linux, I won't be able to get the Code Composer studio (CCS) for 32-bit linux.
The following link provide CCS for 64-bit linux only: "http://software-dl.ti.com/ccs/esd/CCSv7/CCS_7_3_0/exports/CCS7.3.0.00019_linux-x64.tar.gz".
Also, refer the section "Deprecation notices" point 1 i.e "The 32-bit version of Code Composer Studio for Linux is discontinued in favor of a 64-bit version since CCSv6.2.0."
on the link http://processors.wiki.ti.com/index.php/Download_CCS
If this fact is true that CCS is not supported for 32-bit linux machine, then it is a blocking state for me.
Please provide CC3220 SDK as well as Code Composer Studio either for 32-bit linux or for 64-bit linux.
Q3. Is it possible to have two SDKs installed on the same machine i.e one is am355x SDK and other is CC3220 SDK.
I already have am355x SDK installed on my machine. will installing CC3220 SDK on the same machine will be affected/disturbed by the previously installed am355x SDK?