This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC3220MOD: Issue with File Operations on Serial Flash

Part Number: CC3220MOD
Other Parts Discussed in Thread: UNIFLASH

Tool/software: TI-RTOS

Hi,

  - We are using Code Composer Studio Version 7.1 or above and SDK - simplelink_cc32xx_sdk_1_50_00_06 

  - In Our Application We would like to store some (4 to 5) Files onto Serial Flash (CC3220MODSF) using sl_API's

  -  We would like to store the files in Secure or Redundant or FailSafe Mode. 

  - The example given with the SDK1.5 is working fine for us. 

  - Where as in our application we have written 2 files initially. Whenever there is an issue with file I/O operations after reloading the application using uniflash (Simplelink Image Creator), our files get erased and we have to create them again. Is there any possibility that we can program the chip without loosing those files?

  - If we do OTA update for the chip, will the Files present on Serial Flash still remain or get erased?

  - In our Application we will use these files at Multiple times for Read and Write Operations (Approx. 50 times per day). Our Application Includes TCP,UDP and HTTP protocols also. Now we need your suggestion on How good is it to go ahead with serial Flash for our requirement?.

     Please get back to us on this ASAP.

Thanks & Regards

Vivek