Part Number: cc3220
Hi
I would like to run the CC3220 in 1.85 V pre-regulated mode. The CC3220 data specifies the following as one of the requirements.
My concern is with the last requirement of the settling time under 4 us. My understanding is that that once the regulated load gets a step function from 0-500 mA, that transient recovery time to 1.85V should be less than 4 us. However, based on this I am having difficultly finding a regulator that meets this requirement from the TI's portfolio. A regulator such as TLV62568, which shows very fast transient and meets all the other reqirements,still seems insufficient. My question is then will this regulator work and is the interpretation of that requirement correct? Are there any recommendations from TI regarding the regulator for running 1.85V pre-regulated on the CC3220.
Thanks,