Other Parts Discussed in Thread: CC3200, , CC3100
I have a CC3200-LAUNCHXL Rev. 3.2 with a XC3200HZ chip mounted on it. In the CC3200 SimpleLink™ Wi-Fi®
SDK v1.3.0 Release Notes is written that it supports CC3200R1 chip (production chip) and CC3200-LAUNCHXL Rev. 3.2 onwards.
I have a similar situation also about CC3100 (CC3100-BOOST Rev. 3.3 mounting a XC3100HZ).
1. In my case I have no CC3200R1 mounted on it but the board is a Rev. 3.2 so I suppose 1.3.0 is not supporting my board right?
2. Is there any document describing the difference between CC3200R1 and XC3200HZ?
3. Does any patch/update exist for XC3200HZ chips to be supported by newest SimpleLink library releases or have I to live with 2 difference releases for the boards I already have in the field using XC3200HZ?
4. Last SimpleLink lib. rel for CC3200 is 1.3.0, instead for CC3100 is 1.2.0. Considering there are some bugs on 1.2.0 do you plan to update the CC3100 SimpleLink lib or is it possible to use the CC3200 lib (apart the devicelib related to the Cortex-M4 cpu that is not present in the CC3100)?
Kind regards,
Massimo