This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: Uniflash cannot get files from "www" folder

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH

Hello. I wrote a code that creates some files in the following path: "www/tracks/". The program works, saves and opens files correctly. Files are also available from a web browser. However, Uniflash shows that the folder "tracks/" is in the root of the file system. Also, when I try to download a file, I get the message: Operation failed: (155, 'FS_ERR_FILE_NOT_EXISTS'). What is the reason?