Tool/software: Linux
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Jun Yoshida said:I would like to create a SD card that builds kernel 4.4.32 using TI SDK (03.02.00.05)
From where you get this TI SDK for OMAP36x? In TI site, I am not able to find OMAP36x SDK.
The only info for OMAP36x I was able to find, is regarding TI Zoom board:


Regards,
Pavel
Jun,
The link you have provided is for 3rd party board, Gumstix Overo FireSTORM-Y Computer-On-Module. From the description of this board, I see it is with TI DM3730 device, not with OMAP36x device, see "Details" tab:
Texas Instruments DM3730 Applications Processor: 1GHz ARM Cortex-A8 DaVinci DM3730 high-performance microprocessor. Includes a 720p HD DSP imaging and video accelerator and PowerVR SGX graphics accelerator with Open GL ES 2.0 and OpenVG support. The DM3730 has been designed to provide best in class ARM and graphics performance while delivering low power consumption.
The latest TI SDK for DM37x boards is DVSDK v4.03, it comes with kernel 2.6.37:

This TI DVSDK by default support DM37x TI EVM (link below), thus you should port it for Gumstix board, if you need to use that TI DVSDK.

Another option is to use the Gumstix SW, which is based on kernel 3.17. You can find that SW in the "Software" tab inside the link you have provided.
From where to get Gumstix SW (which should run by default on this board, no need to port it), how to build that SW and how to create boot-able SD card with that SW, you should check with the Gumstix support team, refer to the below link:

Regards,
Pavel