Other Parts Discussed in Thread: WL1837MOD
Tool/software: Linux
Hi,
This inquiry was originally posted in the Sitara Processors Forum. It was recommended that I repost here.
Two related questions (Q1 and Q2 below)
Q1: Do any versions of ti-processor-sdk-linux-am335x-evm include WiLink 8.7 SP2? If so, which SDK version(s)?
(I've been told that WiLink is a separate add-on, but the all the SDK installers I've used included WiLink drivers, firmware and related utilities. So, it seems that some version of WiLink is always present with the standalone SDK. When I use SD cards created from those SDK installations (no special WiLink8 add-ons), my EVM w/ WL1837MOD works just fine.)
Although I'd love to leave well-enough alone, I do have a need for WiLink R8.7 SP2 for a certain project.
Q2: if WiLink R8.7 SP2 requires a special patch to an existing SDK installation, to which SDK version would you recommend I apply said patch?
Thanks in advance,
- Marc