This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1835MOD: Pairing to Windows PC to establish serial communication

Part Number: WL1835MOD
Other Parts Discussed in Thread: WL1835

Tool/software: Linux

Hello,

I'm using the BeagleBone Black Wireless which include the WL1835.
The OS is debian which is preloaded in the board.
I'm trying to establish a serial communication between the board and a Windows 10 PC. I was able to pair the bluetooth between the devices but no serial port was detected on the PC side.
Need the WL1835 a manual initialization/configuration to operate as UART? And to tell the PC to create a COM port trought the bluetooth device?

Thanks