Other Parts Discussed in Thread: CC3200
Tool/software: TI-RTOS
Hi,
I have a CC3200 with ServicePack_1.0.1.6-2.7.0.0 running on it. The CC3200 is connected in STA mode to my AP. Auto-Reconnect is enabled on the CC3200. I am running an application using TI-RTOS.
I get random disconnects from my wifi-router.
The CC3200 states reason code 6 which translates to: SL_CLASS_2_FRAME_RECEIVED_FROM_NONAUTHENTICATED_STATION
I ran a wireshark sniff on the wifi protocol, please see the attached. There you can see several disconnects, on at 14:44:08 CET and following.
The CC3200 is in good reach to the AP and not moving. The wifi has very few traffic/clients only.
It would be great if someone could have a look at the sniffer-logs to give a hint what could cause the seen behaviour.
Best,
Henry