This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: CC3220SF Custom Board Production Programming Flow

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF, , UNIFLASH, CC3120

We are designing a custom CC3220SF board based on the CC3220SF-LAUNCHXL LaunchPad.

Since each product that use a CC3220SF processor must also have a serial flash memory connected we will use the same use in the CC3220SF-LAUNCHXL LaunchPad

the MX25R3235FM1IL0 from Macronix.

My question is :

Once I get the bare populated PCB board manufactured what is the next step toward programming ?

I know the macronix serial flash has to be formatted and programmed at minimun with the Service Pack.

And the binary image running in the internal CC3220SF flash memory must be also programmed.

Can I do both using the Uniflash utility?

I have read the next documents , but I am still confused.

CC3220 Production Line Guide ( swra568.pdf )

Using Serial Flash On CC3120 and CC3220 ( swra515a.pdf)

CC3120 and CC3220 Embedded Programming (swpa230.pdf)

Thanks