Part Number: CC3220
I am considering using the CC3220MODA for my wifi application. I want to be able to send simple serial AT commands and allow the CC3220 to do all the heavy lifting for network requirements. It seems that this device has all that capability. I will have no need to program the CC3220 onboard MCU for my purposes. My question is does the onboard MCU in the CC3220 have the serial AT command applications/capability pre loaded (as purchased) or is it necessary to flash it. If flashing is required, is the basic SDK for AT command control available already from TI?