This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640R2F: Issue while pairing the phone with the launchpad

Part Number: CC2640R2F

Tool/software: TI-RTOS

I am using cc2640r2f launchpad with CCS7.2.  I have downloaded simplelink_cc2640r2_sdk_1_40_00_45 and  used the example ble5_multi_role_cc2640r2lp_app and ble5_multi_role_cc2640r2lp_stack_library.

The project is compiled and loaded successfully.I can get the Bluetooth signal from the launchpad but when I tried to pair my phone with the launchpad, it asks for the password and there are two options such as 0000 and 1234 while pairing. I tried both 0000 and 1234 but I couldn't able to pair with the launchpad.

Kindly suggest the right password.