This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120BOOST: CC3120BOOST not connecting to SSID

Part Number: CC3120BOOST
Other Parts Discussed in Thread: UNIFLASH, CC31XXEMUBOOST, CC3120

Hello,

I need help to send data from the CC3120BOOST card to a wifi network.

I bought CC3120BOOST and CC31XXEMUBOOST development kits. I installed simplelink_studio_cc31xx_sdk_1_00_00_05.exe and I compiled the network_terminal with Visual Studio. I managed to send TCP and UDP packet over WiFi. Next day I updated the serivce pack with sp_3.2.0.0_2.0.0.0_2.2.0.4.bin (file in the same archive as the network_terminal) with Uniflash 4.2.1.1562. Since then I can not connect to any ssid with network_terminal software; I get following message: "[line:202, error:-1] Network Error".
The scan command is working correctly.

One strange thing is that when I try to connect to a SSID just after programming the component with Uniflash, the wlanconnect command returns no message but It's still not connected.

How can I reset the kit to its original state? Can you give me the image file that is shipped with the development kit? Is it a better version of the software available?

Thanks.