Part Number: WL1837MOD
Hi,
MCP8.5_SP2 and NLCP8.7_SP3 have been released as a workaround against the WPA2 KRACK problem of WL18xx.
Is it necessary to update FW (wl18xx - fw.bin) as this workaround?
Is it possible to take measures only with the wpa_supplicant of the OS being used or the driver side?
There is a question as to what kind of workaround for minimal modification from customers already mass-produced.
There is our customer's request that they do not want to update the wl18xx firmware they are running now.
Best Regards,
Shigehiro Tsuda