I need to power the CC3100MOD from a single cell Li-Ion battery. Since the maximum power supply voltage of the module is 3.6V I need to reduce the battery voltage. What is the best way to do it in a mean of power efficiency:
1. Use an LDO to step down ot 3.6V and power the module?
or
2. Use a DC/DC converter to step down to 3.6V and power the module?
or
3. Use a DC/DC converter to step down to 2.3V and power the module?
The module has an internal DC/DC converter but there is no info about it's characteristics.