Other Parts Discussed in Thread: CC3220SF, UNIFLASH
Hi all,
I need some clarification about CC3220SF flash management:
1) SF version has an internal 1Mbit flash to run the code, but with the Uniflash tool I can write only on external flash (is this right). How does internal falsh work? Every time the system boot, the MCU bin file is copied from the external to the internal flash and run ?
2) What is the mean of "Fail-Safe" about files? I can't found informations on this aspect, how does it work?
3) During programmation , if I set the "Secure" flag about a file, this means that the file will be encrypted using the certificates previously loaded?
4) How does the factory image restore work? Have I flash an MCU bn image that I flag as "factory image"?
thanks!!
Riccardo