Tool/software: Code Composer Studio
I am trying to get the code building for AWS on cc3220. I have followed the steps on the Quick Start Guide up to building the project. When I build the subscribe_publish_sample I get 16 errors all seeming to be issues where a .h file cannot be seen so it brings up issues. From what I can tell every .h file needed is already in the include section that I can clearly see as part of the project. I have tried this with both gcc and ccs versions and get similar issues on both. The only thing I have thought of is when the quick start guide says install plugins I only have option of a .zip not .exe. It says CCS should recognize that I unzipped it in C:\ti\. Besides that I can not see anything that I haven't done and as I stated the files all seem to be in the include part of the project and when I look at properties all the linkers seem to be to point to right places.
any help would be awesome and if you could link me to a plugin version that is .exe instead of .zip that may help as well.
Thanks,
Jon