This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1835MOD: Issue in building WL18xx build scripts against linux kernel version 4.9.11

Part Number: WL1835MOD

Tool/software: Linux

Hi,

I am trying to integrate WL1835MODCOM8B Wi-Fi module with Sabre SD board. I tried to use the Wl18XX build scripts for the driver. I need to compile the driver against Linux kernel version 4.9.11 but the Wl18XX build scripts package supports only up to kernel version 4.4. So, I am now planning to use the wl18xx driver available in the Linux kernel. Will it cause any issues related to certification?