This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: Calibration Current

Part Number: CC3220

What are the implications of doing a one-time calibration on CC3220 that operates over a -40 to 85C industrial temperature range?

Would radio performance be degraded?

Any concerns with violating certifications?

Please advise.

Thanks,
Mark

  • Hi Mark,

    One-time calibration mode performs the calibration one time during the initialization and sticks to it, re-calibration will not occur.

    So if the init calibration occurs at 30C it will be calibrated for 30C operating conditions. Radio performance would degrade at other temperatures, especially the extremities, and it would most likely violate certs.

    One-time calibration mode is not recommended for use within a temperature changing environment, users should use normal mode.

    From section 3.8 "Calibrations" of SWRU455:

    "Normal calibration mode is used to achieve the best RF performance, or when the environment of the device is prone to changes (temperature changes)."

    Hope this helps,
    Kevin
  • Hi Kevin,

    The apps team committed to getting output power vs temperature data for one-time calibration.

    Thanks,
    Mark