This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: WL1807MOD antenna design

Part Number: WL1807MOD


hi, 

i have new design with WL1807MOD, so i have some question about antenna design with this module 

- any option for PCB antenna, cause on reference design of TI used CHIP antenna 

- With 2 pin antenna RF_ANT1 and RF_ANT2, we need to spear a lot space for placement 2 antenna (Chip antenna ) like TI reference: distance between them bigger than 62.5 and place in 90 degree, so with some small board that too difficult. so question, any idea if we can optimize placement as small as possible 

+ Put 2 antenna nearly asap

+ Option use only 1 antenna but our requirement need support 5Ghz and 2.4 GHz, please advise which port that can adapt like that ( from block diagram seem be RF_ANT2 can support , please verify