This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/CC3220: can it drive 3.3V for GPIO

Part Number: CC3220

Tool/software: WEBENCH® Design Tools

Hi,

we are considering CC3220SF and CC3220moda for one of our project. and we have the below 2 questions

1. CC3220moda:

   > Can the module CC3220moda  drive 3.3V for the GPIO pins, VBAT1(pin 37) and VBAT2(pin40) is connected to 2.8V (output of a buck converter)

   > Can the module interface a 1.8V GPS chip over a UART or should we need a level shifter.

2. CC3220SF

  >  Can CC3220SF  drive 3.3V for the GPIO pins when used in wide voltage mode. (Pin 10, 54, 44, 39, 37 set to 2.8V)

  >  We see that VDD pin 9 and 56 is powered from Pin 43 which is DCDC_DIG_SW. whats sets this voltage? is there an internal DC DC converter Buck/Boost? How is the digital IO voltage set?

  > Can the module interface a 1.8V GPS chip over a UART or should we need a level shifter.