I have a board that has a WL1837mod on it, and it is controlled by I.MX6UL. I would like to test the BLE functions on the module with the MT8852B Bluetooth test equipment. According to http://processors.wiki.ti.com/index.php/WL18xx_Bluetopia_PM_Bluetooth_RF_Testing#BLE_testing_2 , to have the module in the BT SIG RF mode, the device needs to powered up, loaded with the latest service pack and the DUT script. If the processor takes care of loading the driver for the bluetooth module, is there any way to have that automatically loaded to the chip without the processor? Also, it seems like there is no need of UART lines connections between the DUT and a computer on TI wiki which is required for the test equipment set up. I would appreciate any advice on this as well.
Thanks.