Other Parts Discussed in Thread: CC3220S-LAUNCHXL, , UNIFLASH, CC3220S, CC3220SF, CC3220MOD
Tool/software: TI-RTOS
Team,
I found that the WiFi signal strength is significantly less on CC3220MODA compared to CC3220S-LAUNCHXL despite running the same firmware on both devices.
Both device have been placed at the exact same location pointing the antenna portion in the same direction and my Wifi router is Ubiquiti UniFi AP Enterprise WiFi System Long Range. I experienced frequency disconnection on CC3220MODA and hence checked the WiFi strength using the Ubiquiti UniFi WiFi controller portal, which showed only 5% WiFi on CC3220MODA where as the launchpad gave 55% at the same location. Please note that I have just used a breakout board to connect CC3220MODA to the power supply and nothing else is changed. The CC3220MODA is also powered using a AC/DC power supply (5V) with a voltage regulator and filter giving steady 3.3V supply to the module.
Thanks
Zac