This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: CC3200 Mac address range

Part Number: CC3200

Hi,

Is there a specify mac address range that is used for CC3200 (number on part: cc3200R1 M2 4c3 ZFRR G4) chips?  Can I determine what the range would be from the number on the chip?  Right now, I have seen F4:B8:5E:xx:xx:xx and 58:7A:62:xx:xx:xx.   I would like to verify that the mac address falls within a known range or verify against a known sets of valid addresses for manufacturing tests.  

Thanks,

Kevin